Looking for specific product > ATS024T-W050

Hi,

I am looking for this power Adapter but with specific 4 prong end piece, I can only seem to find the barrel version everywhere. its a power adapter for Raritan DKX4-101 unite

Power adapter model # ATS024T-W050

picture of Specific 4 prong end piece:

And a picture of the female end it plugs into:

I am trying to find somehwere to buy this, I need 2 of them.

Cheers,

Your connector looks like it’s a Molex Microfit line, similar to this pre-made cable:

2451320405 Molex | Cable Assemblies | DigiKey

Unfortunately I’m not seeing that we have any power supplies available with a matching connector installed.

FYI I found a part on DIGIKEY to convert normal barrel 2.1mm adapter to the 4-pin i need!

That’s great! However, I would recommend that you verify that the pinout is what you need, as I don’t think there is a universal standard for this.

Here’s the pinout shown in the datasheet:

@duff_wm

I am in the same situation as you and have already bought a similar adapter to yours : https://teltonika-networks.com/products/accessories/powering-options/4-pin-to-barrel-socket-adapter-1

I would be very grateful if you are able to tell me if the adapter you bought worked for you to power the Raritan Dominion KDX IV-101 ?

Thank you very much.

For anyone else facing this same problem I found a working solution !!!

tl;dr : Cut the barrel adapter in the middle and switch the red and black wires around (so connect black from one part to the red of the other)

For anyone else facing the same issue I GOT IT TO WORK !!! I was pissed off and desperate enough to try this and just got lucky. I wish I had taken a photo of when I was trying things out.


With reference to this pic:

  1. The small barrel to molex adapter is
    1 x Teltonika PR2PD01B 4-Pin to Barrel Socket Adapter @ GBP 6.44 each (Bought from www.broadbandbuyer.com/products/47042-teltonika-pr2pd01b/)

  2. The power supply itself was from Amazon:
    www.amazon.co.uk/dp/B099F196YQ
    (5V 4A Power Supply Adapter - AC 100-240V to DC 5V/4A 20W Charger DC 5.5mm x 2.5mm Universal UK for Atomic Pi, Jetson Nano, USB Hub, WeBoost 850012 Connect RV 65 RV65, Odroid XU4 / XU4Q)


I had checked the specs of the barrel adapter and this power supply and they looke like they were compatible. I received these two things before receiving the Raritan KVM so I was able to check if the power supply itself by plugging it into an LED lamp which accepted that barrel adapter. The LED lamp turned on so the power supply test was successful.

When I got the Raritan KVM, I plugged in everything and the green light in the front of the unit did not come on to indicate power. So I cut the Teltonika adapter in half. It had two wires, red and black. I connected the red wired from one part to the black of the other and the black to red. Then tried connecting the frankenstein adapter to the KVM and it came to life !