Looking to source interconnect for current device

Hi all,

Looking to see if I can get help sourcing the mating connector for the following. Attributes below.

Thread Major Diameter - 8.82 mm / 0.347 in
Approximate Thread Height - ~3.85 mm / 0.152 in
Approximate Connector Height Height - ~8 mm / 0.315 in
Internal Diameter - 5.67 mm / 0.223 in
Signal Pin Diameter - ~0.50 mm / 0.020 in


Picture included. Thanks yall!

@cory.momntm

Would you have the item number for the device the connector you show is attached to?

SC1519-ND was found to look like the correct overall arrangement. However, if we can verify the specific connector used on the device you have in the images we can also select for the correct connector threading and size.

It’s on-board a TS20 from Interface Force Measurments. Link below.

They don’t have the mating part number on the documentation and supply their own harnesses so I doubt they would give me it if asked. Could still do but I know the folks here are super knowledgeable and could help out faster.

Hello Cory.momntm,

Thank you for the additional information, but the only documentation I was able to access on their website was this catalog. They do mention cable assemblies around page 493, and provide mating connectors, but I do not see the TS20 listed. Even looking at cable assemblies on their website, they do not provide any information. Unfortunately, I have been unable to find anything additional.