Mating connector for FTM-103-02-F-DV?

------Question for FTM-103-02-F-DV Please Put your question below------

What is the part number for the mating connector?

And why isn’t the information at the bottom of the product page like it is for almost any other connector?

Hello,

It looks like the mating part for this is 612-MLE-103-01-G-DV-ND. As for why this is not shown below, it is possible that our team has not added this in as a mating part yet.

I should have been more clear. I want a wired connector, as in I want to go from the board to a panel mounted connector. Is that available? For any 1mm pitch 2X3 pin header, I’m not fussy. I had boards made assuming this would be an easy part to find.

The original connector is meant for board to board. An option that might work for you is to solder wires onto a through hole connector, like the part below.

For a connector housing that has contacts that you can wire yourself, I was not able to find one in our system with a 1mm by 1mm pitch for 6 contacts.


 

Image

MFR PART # SFM210-LPSE-D03-ST-BK
DIGIKEY PART # S9384-ND
MANUFACTURER Sullins Connector Solutions
DESCRIPTION 6 Position Header Connector 0.039" (1.00mm) Through Hole Gold
DATASHEET Click Here