This is a connector pin that was soldered onto a circuit board for a thermal arc tig welder. I really appreciate any help!
To clarify, the connector was ripped off the board in an accident. Thats why the pins are pulled almost all of the way out of connector.
Hello vdubjim, welcome to the DigiKey TechForum.
I believe the connector in the pictures, is 455-BH2B-XH-2-ND.
We have these available, and the minimum order is 1 piece.
The spacing of the 2 pins is 2.5mm (Center to Center).
Thank you for the help David! I believe you are correct. I ordered a few based on your recommendations!