This is aftermarket nvidia sxm3 to pci adapter board. It says it needs 48v power connector, using micro-fit 8 pin. I have no idea where to get this. Anywhere on DigiKey?
Hello and welcome to the TechForum!
I was able to gather a few links that maybe what you are after. Feel free to ask follow up questions or clarify what you need for assistance.
Technical assistance was provided for MICRO-FIT
Cable options plug-plug and plug-wires
48V power supply
48V LED drivers
Thank you
Ryan
This is good, but the micro fit are all socket-to-socket. So how would I connect these to the power supply?
you would either need a power supply with a mating connection built into it from the manufacturer or you can add a connection to a power supply.
PCI type items like these are normally sold with the intent that they are going in the PC / Desktop case. Some can be send with a cord or set of cords to connect to the main board of the PC or the Main power supply for the whole case.
Ok this pcb came with no external connectors. I have looked and cannot find any power supply that has any micro-fit 8 pin.
So I was wondering if you all had any microfit 8-pin on one side, and on the other side something that connects to those generic power connectors. I don’t want to cut the cable apart if I can avoid it.
I currently am not seeing that we have one with the connections built in.
The below link is an example power supply that may have that type of connection.
This looks awesome, but I think this is regular molex, not micro fit molex.
Connector housings such as the 0430250808 are available to make a cable of the sort desired. Scroll down that product page for the related contacts, sold separately.