I am considering how to install the Opto diode AXUV100G and removing the heat efficiently.
I am installing it at an X-Ray beamline at a synchrotron facility, thus the optodiode will measure an X-Ray beam with the following characteristics:
• a power of 70W and density of about 16 W/mm2
• energy is 25-1500 eV
My actual question is: how much energy do I need to remove from the diode to avoid overheating?
This leads to the following question: How much of the energy does the diode and casing absorp from the beam? If the answer to this question is a very low %, I guess we do not have to continue answering the next questions. But if the absorption is significant, we have to answer:
-
What is the diode material and thickness?
-
What is the casing material and thickness?
-
How is the diode attached to the casing?
With this information I can evaluate how much heat I must remove to avoid overheating (I suppose the maximum design temperature should be 80 degC as per the datasheet since the diode will be installed in vacuum (e-9 mbar), can you confirm this? what is damaged if overheated beyond 80 degC?)
Thanks