Outside dimensions of the 3 pin male header: 10mm long by 6.7mm wide by 7.3 or 7.4mm high
2mm pitch.
Maybe WM18921-ND
You can double check measurements on the datasheet. https://www.molex.com/pdm_docs/sd/353620350_sd.pdf
-Robert
Doesn’t appear to match to me.
From WM18921-ND:
Actual top-down view:
Do you know the pitch? Measurement between pins.
-Robert
2mm pin pitch
Hi Thanks for contacting Digi-Key. Is it possible to send additional photos and measurements , including the pitch of the contacts.
Thanks
-Original Message–
Here’s some more photos.
3-pin Male header outside length: 10mm
3-pin Male header outside width: 6.7mm as measured at the base
3-pin Male header insulation height: 7.5mm
3-pin Male header pin pitch: 2mm
3-pin Male header inside length: 8.7mm
3-pin Male header inside width: 4.5mm
I am trying to modify a product as a hobby project. This board also contains an Elan 8-bit MCU (which has an English datasheet but is not found on digikey) and an A308 lithium charger IC that I can only find information on from Alibaba. This suggests to me that their supply-chain is based out of Asia and compatible connectors may not be found through Molex or other North American suppliers.
That Latch is what I couldn’t find in our catalog. The 5023510300 looks very similar in profile, but the latch is just a touch off.
My search space was here: https://www.digikey.com/short/00r5rcp9