I have a pot that the shaft come out of the the end of the pot. I have reach out to the manufacturer for the information on this along with a part number RV9110NS-KQ15A6.0-B103-0000S-P01A. I would like to replace this but the manufacturer only sells in large quantities. The brand is sanni. I am needing this for a plate amplifier I currently use. I was wondering if you have a part to fix or something close?
Would you have images of the item you have on hand?
The 693-14921F0GJSX13103KA-ND was found based on the information I was able to find for the item.
However I am not certain on the style of potentiometer your original is.
I see that the part you sent me is a 6 pin mine is a 5pin.
Hi, is the one you said would work be and option? I did see that it’s a 6pin and mine is a 5 pin but is this just 2 grounds? is this something that I could solder a jumper wire? Not sure but needing to figure this out but don’t have a lot of knowledge about this. So, any advice would be much apricated. I have also included a few more photos to hopefully help with this issue.
Thanks Chad
okay, I am so sorry. I finally looked at the drawings closer and figured out you basically can build you own? That’s if I understand right? So, is the part number 14921F0GJSX13103KA the exact one I need to order? If not, could you assist me in identifying the exact one needed?
Hello @chadshaw1
Thank you for the photos and drawing for that part.
Using the information you have provided part number PTR901-2015K-B103 would be a good replacement for that potentiometer and according to the datasheet it has the 5-pin layout you are looking for.