Power supply Query - MPS-1800S-60-30

I am Vinay from iwave systems and technologies, Bangalore, India. We contacted the manufacturer directly to verify the power supply, and the image provided by them differs from the one displayed on the DigiKey website. We are interested in purchasing this product through DigiKey. Could you please confirm whether the same power supply will be delivered if we place an order?"

When you mention the image provided by the manufacturer, do you mean the reference photos here?

From what I can see, their photo is exactly the same as ours, with the exception that the digital display shows a different set of values. The specifications across the board are the same for the MPS-1800S series apart from the max voltage/current outputs, so the reference photo would not be a good way to determine which supply is which part number.

Our listing for MPS-1800S-60-30 is the 60VDC max voltage output, 30A max current output version of this power supply; if that is the one you want, then this is the correct part number: 4321-MPS-1800S-60-30-ND

Hi Chris Groom,

We discovered that the output and input voltage connections at the back of the power supply have different types of terminations. While the part numbers and other specifications are identical, the termination type varies. We require the termination to match exactly as shown in the manufacturer’s provided image.

After inquiring, the manufacturer confirmed that the image on the DigiKey website is outdated, and the image they shared accurately reflects what they supply. Therefore, we are double-checking this with DigiKey.

Regards,
Vinay
Ph - 7483271950