Problem finding correct LTW locking mechanism

I ordered a BD-088BFFA-QL8MP0 plug to repair the mic cord on a Icom M801 SSB transceiver. It fits but the locking mechanism is incorrect. I need one that locks with a quarter turn to the right. The ordered part has a spring mechanism where you turn it to the left insert the plug then let it return to the right. It will not mate with the jack when in the unlock position. I also had ordered a panel jack for the remote mic for an ICOM VHF radio and found that while everything else was correct, it had a threaded locking mechanism rather than a turn to the right bayonet mechanism. I have not figured out how to order the right locking mechanisms.

Hello,

Unfortunately this one does not come in a bayonet lock type connection.

Curious which part number that you ordered for the ICOM VHF remote mic?

@tjfurst

If the one in the image(which I hope I managed to fix to make it visible) is the one he was trying to use.

It looks like the AU-08PMMP-QC8001. However They would need to confirm.
AU-08PMMP-QC8001 Amphenol LTW | Connectors, Interconnects | DigiKey

I ended up not having the plug lock to the radio. I was able to get a board mounted jack that would lock to the plug I installed on the mic cable, but chickened out on changing the jack, and since the SSB is seldom used on the boat, I just plug in the microphone without locking it. I am actually on the boat now but have the details of what I ordered at home. BTW, I understand that it is possible to use the later version of the ICOM mic with the 802 SSB with loss of button function. While I like to be able to get on the SSB to use as a Ham radio, my friend (the boat owner) avoids SSB as much a possible and we now have Starlink for general data and communications. The mic is onboard and will work if needed. Wish I had a great solution.
Jack