この記事では、C SDKを使って Raspberry Pico 2 W を無線アクセスポイント(LANホットスポット)(2.4GHz IEEE 802.11n規格)としてセットアップする方法を説明します。このデバイスはDHCP(Dynamic Host Control Protocol)サーバを使用して、直接接続するクライアントに対して(WiFi LANルータのように)IPアドレスを割り当てます。
この記事では、C SDKがパソコンに正しくインストールされていることを前提としています。
まず最初に、以下に示すC言語のソースコードをビルドします。
/**
* Copyright (c) 2022 Raspberry Pi (Trading) Ltd.
*
* SPDX-License-Identifier: BSD-3-Clause
*/
#include <string.h>
#include "pico/cyw43_arch.h"
#include "pico/stdlib.h"
#include "lwip/pbuf.h"
#include "lwip/tcp.h"
#include "dhcpserver.h"
#include "dnsserver.h"
#define TCP_PORT 80
#define DEBUG_printf printf
#define POLL_TIME_S 5
#define HTTP_GET "GET"
#define HTTP_RESPONSE_HEADERS "HTTP/1.1 %d OK\nContent-Length: %d\nContent-Type: text/html; charset=utf-8\nConnection: close\n\n"
#define LED_TEST_BODY "<html><body><h1>Hello from Pico.</h1><p>Led is %s</p><p><a href=\"?led=%d\">Turn led %s</a></body></html>"
#define LED_PARAM "led=%d"
#define LED_TEST "/ledtest"
#define LED_GPIO 0
#define HTTP_RESPONSE_REDIRECT "HTTP/1.1 302 Redirect\nLocation: http://%s" LED_TEST "\n\n"
typedef struct TCP_SERVER_T_ {
struct tcp_pcb *server_pcb;
bool complete;
ip_addr_t gw;
} TCP_SERVER_T;
typedef struct TCP_CONNECT_STATE_T_ {
struct tcp_pcb *pcb;
int sent_len;
char headers[128];
char result[256];
int header_len;
int result_len;
ip_addr_t *gw;
} TCP_CONNECT_STATE_T;
static err_t tcp_close_client_connection(TCP_CONNECT_STATE_T *con_state, struct tcp_pcb *client_pcb, err_t close_err) {
if (client_pcb) {
assert(con_state && con_state->pcb == client_pcb);
tcp_arg(client_pcb, NULL);
tcp_poll(client_pcb, NULL, 0);
tcp_sent(client_pcb, NULL);
tcp_recv(client_pcb, NULL);
tcp_err(client_pcb, NULL);
err_t err = tcp_close(client_pcb);
if (err != ERR_OK) {
DEBUG_printf("close failed %d, calling abort\n", err);
tcp_abort(client_pcb);
close_err = ERR_ABRT;
}
if (con_state) {
free(con_state);
}
}
return close_err;
}
static void tcp_server_close(TCP_SERVER_T *state) {
if (state->server_pcb) {
tcp_arg(state->server_pcb, NULL);
tcp_close(state->server_pcb);
state->server_pcb = NULL;
}
}
static err_t tcp_server_sent(void *arg, struct tcp_pcb *pcb, u16_t len) {
TCP_CONNECT_STATE_T *con_state = (TCP_CONNECT_STATE_T*)arg;
DEBUG_printf("tcp_server_sent %u\n", len);
con_state->sent_len += len;
if (con_state->sent_len >= con_state->header_len + con_state->result_len) {
DEBUG_printf("all done\n");
return tcp_close_client_connection(con_state, pcb, ERR_OK);
}
return ERR_OK;
}
static int test_server_content(const char *request, const char *params, char *result, size_t max_result_len) {
int len = 0;
if (strncmp(request, LED_TEST, sizeof(LED_TEST) - 1) == 0) {
// Get the state of the led
bool value;
cyw43_gpio_get(&cyw43_state, LED_GPIO, &value);
int led_state = value;
// See if the user changed it
if (params) {
int led_param = sscanf(params, LED_PARAM, &led_state);
if (led_param == 1) {
if (led_state) {
// Turn led on
cyw43_gpio_set(&cyw43_state, LED_GPIO, true);
} else {
// Turn led off
cyw43_gpio_set(&cyw43_state, LED_GPIO, false);
}
}
}
// Generate result
if (led_state) {
len = snprintf(result, max_result_len, LED_TEST_BODY, "ON", 0, "OFF");
} else {
len = snprintf(result, max_result_len, LED_TEST_BODY, "OFF", 1, "ON");
}
}
return len;
}
err_t tcp_server_recv(void *arg, struct tcp_pcb *pcb, struct pbuf *p, err_t err) {
TCP_CONNECT_STATE_T *con_state = (TCP_CONNECT_STATE_T*)arg;
if (!p) {
DEBUG_printf("connection closed\n");
return tcp_close_client_connection(con_state, pcb, ERR_OK);
}
assert(con_state && con_state->pcb == pcb);
if (p->tot_len > 0) {
DEBUG_printf("tcp_server_recv %d err %d\n", p->tot_len, err);
#if 0
for (struct pbuf *q = p; q != NULL; q = q->next) {
DEBUG_printf("in: %.*s\n", q->len, q->payload);
}
#endif
// Copy the request into the buffer
pbuf_copy_partial(p, con_state->headers, p->tot_len > sizeof(con_state->headers) - 1 ? sizeof(con_state->headers) - 1 : p->tot_len, 0);
// Handle GET request
if (strncmp(HTTP_GET, con_state->headers, sizeof(HTTP_GET) - 1) == 0) {
char *request = con_state->headers + sizeof(HTTP_GET); // + space
char *params = strchr(request, '?');
if (params) {
if (*params) {
char *space = strchr(request, ' ');
*params++ = 0;
if (space) {
*space = 0;
}
} else {
params = NULL;
}
}
// Generate content
con_state->result_len = test_server_content(request, params, con_state->result, sizeof(con_state->result));
DEBUG_printf("Request: %s?%s\n", request, params);
DEBUG_printf("Result: %d\n", con_state->result_len);
// Check we had enough buffer space
if (con_state->result_len > sizeof(con_state->result) - 1) {
DEBUG_printf("Too much result data %d\n", con_state->result_len);
return tcp_close_client_connection(con_state, pcb, ERR_CLSD);
}
// Generate web page
if (con_state->result_len > 0) {
con_state->header_len = snprintf(con_state->headers, sizeof(con_state->headers), HTTP_RESPONSE_HEADERS,
200, con_state->result_len);
if (con_state->header_len > sizeof(con_state->headers) - 1) {
DEBUG_printf("Too much header data %d\n", con_state->header_len);
return tcp_close_client_connection(con_state, pcb, ERR_CLSD);
}
} else {
// Send redirect
con_state->header_len = snprintf(con_state->headers, sizeof(con_state->headers), HTTP_RESPONSE_REDIRECT,
ipaddr_ntoa(con_state->gw));
DEBUG_printf("Sending redirect %s", con_state->headers);
}
// Send the headers to the client
con_state->sent_len = 0;
err_t err = tcp_write(pcb, con_state->headers, con_state->header_len, 0);
if (err != ERR_OK) {
DEBUG_printf("failed to write header data %d\n", err);
return tcp_close_client_connection(con_state, pcb, err);
}
// Send the body to the client
if (con_state->result_len) {
err = tcp_write(pcb, con_state->result, con_state->result_len, 0);
if (err != ERR_OK) {
DEBUG_printf("failed to write result data %d\n", err);
return tcp_close_client_connection(con_state, pcb, err);
}
}
}
tcp_recved(pcb, p->tot_len);
}
pbuf_free(p);
return ERR_OK;
}
static err_t tcp_server_poll(void *arg, struct tcp_pcb *pcb) {
TCP_CONNECT_STATE_T *con_state = (TCP_CONNECT_STATE_T*)arg;
DEBUG_printf("tcp_server_poll_fn\n");
return tcp_close_client_connection(con_state, pcb, ERR_OK); // Just disconnect clent?
}
static void tcp_server_err(void *arg, err_t err) {
TCP_CONNECT_STATE_T *con_state = (TCP_CONNECT_STATE_T*)arg;
if (err != ERR_ABRT) {
DEBUG_printf("tcp_client_err_fn %d\n", err);
tcp_close_client_connection(con_state, con_state->pcb, err);
}
}
static err_t tcp_server_accept(void *arg, struct tcp_pcb *client_pcb, err_t err) {
TCP_SERVER_T *state = (TCP_SERVER_T*)arg;
if (err != ERR_OK || client_pcb == NULL) {
DEBUG_printf("failure in accept\n");
return ERR_VAL;
}
DEBUG_printf("client connected\n");
// Create the state for the connection
TCP_CONNECT_STATE_T *con_state = calloc(1, sizeof(TCP_CONNECT_STATE_T));
if (!con_state) {
DEBUG_printf("failed to allocate connect state\n");
return ERR_MEM;
}
con_state->pcb = client_pcb; // for checking
con_state->gw = &state->gw;
// setup connection to client
tcp_arg(client_pcb, con_state);
tcp_sent(client_pcb, tcp_server_sent);
tcp_recv(client_pcb, tcp_server_recv);
tcp_poll(client_pcb, tcp_server_poll, POLL_TIME_S * 2);
tcp_err(client_pcb, tcp_server_err);
return ERR_OK;
}
static bool tcp_server_open(void *arg, const char *ap_name) {
TCP_SERVER_T *state = (TCP_SERVER_T*)arg;
DEBUG_printf("starting server on port %d\n", TCP_PORT);
struct tcp_pcb *pcb = tcp_new_ip_type(IPADDR_TYPE_ANY);
if (!pcb) {
DEBUG_printf("failed to create pcb\n");
return false;
}
err_t err = tcp_bind(pcb, IP_ANY_TYPE, TCP_PORT);
if (err) {
DEBUG_printf("failed to bind to port %d\n",TCP_PORT);
return false;
}
state->server_pcb = tcp_listen_with_backlog(pcb, 1);
if (!state->server_pcb) {
DEBUG_printf("failed to listen\n");
if (pcb) {
tcp_close(pcb);
}
return false;
}
tcp_arg(state->server_pcb, state);
tcp_accept(state->server_pcb, tcp_server_accept);
printf("Try connecting to '%s' (press 'd' to disable access point)\n", ap_name);
return true;
}
void key_pressed_func(void *param) {
assert(param);
TCP_SERVER_T *state = (TCP_SERVER_T*)param;
int key = getchar_timeout_us(0); // get any pending key press but don't wait
if (key == 'd' || key == 'D') {
cyw43_arch_lwip_begin();
cyw43_arch_disable_ap_mode();
cyw43_arch_lwip_end();
state->complete = true;
}
}
int main() {
stdio_init_all();
TCP_SERVER_T *state = calloc(1, sizeof(TCP_SERVER_T));
if (!state) {
DEBUG_printf("failed to allocate state\n");
return 1;
}
if (cyw43_arch_init()) {
DEBUG_printf("failed to initialise\n");
return 1;
}
// Get notified if the user presses a key
stdio_set_chars_available_callback(key_pressed_func, state);
const char *ap_name = "picow_test";
#if 1
const char *password = "password";
#else
const char *password = NULL;
#endif
cyw43_arch_enable_ap_mode(ap_name, password, CYW43_AUTH_WPA2_AES_PSK);
#if LWIP_IPV6
#define IP(x) ((x).u_addr.ip4)
#else
#define IP(x) (x)
#endif
ip4_addr_t mask;
IP(state->gw).addr = PP_HTONL(CYW43_DEFAULT_IP_AP_ADDRESS);
IP(mask).addr = PP_HTONL(CYW43_DEFAULT_IP_MASK);
#undef IP
// Start the dhcp server
dhcp_server_t dhcp_server;
dhcp_server_init(&dhcp_server, &state->gw, &mask);
// Start the dns server
dns_server_t dns_server;
dns_server_init(&dns_server, &state->gw);
if (!tcp_server_open(state, ap_name)) {
DEBUG_printf("failed to open server\n");
return 1;
}
state->complete = false;
while(!state->complete) {
// the following #ifdef is only here so this same example can be used in multiple modes;
// you do not need it in your code
#if PICO_CYW43_ARCH_POLL
// if you are using pico_cyw43_arch_poll, then you must poll periodically from your
// main loop (not from a timer interrupt) to check for Wi-Fi driver or lwIP work that needs to be done.
cyw43_arch_poll();
// you can poll as often as you like, however if you have nothing else to do you can
// choose to sleep until either a specified time, or cyw43_arch_poll() has work to do:
cyw43_arch_wait_for_work_until(make_timeout_time_ms(1000));
#else
// if you are not using pico_cyw43_arch_poll, then Wi-FI driver and lwIP work
// is done via interrupt in the background. This sleep is just an example of some (blocking)
// work you might be doing.
sleep_ms(1000);
#endif
}
tcp_server_close(state);
dns_server_deinit(&dns_server);
dhcp_server_deinit(&dhcp_server);
cyw43_arch_deinit();
printf("Test complete\n");
return 0;
}
これにより、クライアントにIPアドレスを割り当てるDHCPサーバと、ユーザーが Raspberry Pico 2 W ボード上の緑色LEDを制御できるHTTPサーバ(TCPコネクション型プロトコルを使用)が作成されます。無線アクセスポイントのプロジェクトをビルドした後、ファームウェアをロードします(説明のため、以下に添付しています)。
picow_access_point_background.uf2(675 KB)
Raspberry Pico 2 W ボードに対し、以下のように書き込みます。
digikey_coffee_cup # picotool load picow_access_point_background.uf2
Raspberry Pico 2 W ボードにこのファームウェアをロードしたあと、パソコン、ノートパソコン、または携帯電話から、以下の認証情報を使ってpicow_testと呼ばれるWiFi「ホットスポット」を経由して接続します。
login: picow_test
password: password
接続が確立したら、ブラウザを開きます。
このウェブサイトサーバは Raspberry Pico 2 W ボードによって生成され、ユーザーはボード上のLEDの状態(ONまたはOFF)を確認し、制御することも可能です。Turn led ONリンクを押してLEDの状態を変更すると、少し遅れてボード上の緑色のLEDが点灯し、ウェブサーバがLEDの状態を以下に示すように更新します。
これを必要な回数だけ繰り返すと、TCPコネクション型プロトコルを使ってHTTPクライアントブラウザから独自の無線アクセスポイント(ルータに似ています)を経由して Raspberry Pico 2 W の緑色LEDを制御する方法がわかります。 一般的なルータを使わなくても、この無線アクセスポイントを経由して別の Raspberry Pico 2 W デバイスを接続することができます。 この場合、HTTPクライアントはWiFi経由で Raspberry Pico 2 W に直接接続されます。また、必要に応じて名前とパスワードを変更するだけで、他の無線アクセスポイントを作成することもできます。
const char *ap_name = "picow_test1";
const char *password = "password";
Raspberry Pico 2 W はDigiKeyからお求めいただけます。どうぞ良い一日を!
この記事はスペイン語でこちらからご覧いただけます。
Este artículo está disponible en español aquí.