Recommendation wanted: 12V-to-5V Buck Converter

I’m installing a Qi2/MagSafe car charger and want to hardwire it because I despise wires, and I like to solder. I see a lot of no-name converters on Amazon and ebay and I want to make sure I get something quality that wont fry the devices. I’d prefer the kind that has pads to solder wires on as opposed to a USB cord/port, as I didn’t see any with a female USB-C port. I’d rather use a USB-C breakout board than a USB adapter.

Is there a converter you recommend for this scenario?

TIA!

Hello @Kwazii !

It’s going to depend on the specification on the charger you’re installing, I don’t believe there will be a one size fits all solution for the converter. Do you have some more information on the charger you’re using?

Sorry if it wasn’t clear, the phone charger connects to power via USB-C (and wirelessly to the phone), so I just need a converter with 5V 3A out.

The charger I intend to use is something like this or this