I’m trying to figure out which type of wire to board connector this is. It is part of a home appliance and carries low voltage signals for LED and push buttons.
Header:
Receptacle:
Description:
- Most likely a 1.0mm pitch (measured on the header)
- 2 row, 7 positions per row
- Header width (including side latches) is 15mm
- Male header is “U Shaped”, i.e there is a U shaped gap between each row
- Male header has side latches that need to be pushed to remove the connection
The closest I could find that matches the pictures is a JST SHLD but SHLD doesn’t come in 14 pins