Similar to 1841800000 but not right angle

Hello,

We’re going to be replacing boards using Weidmuller1841800000. We need something similar but pins have to be straight and not in right angle. Tried looking for one through parametric search but to no avail. It doesn’t to be Weidmuller brand.

Hoping for your kind assistance.

Hello @analogcay

Welcome to the TechForum

I found 2 similar terminal blocks to part number 1841800000 but with straight pins. those parts are part number 1842480000 and part number 1621810000

Thank you for this. As per checking both items aren’t in stock? are there other alternatives? or ways to get them earlier? lead time is a bit long

Hi analogcay,

The only stocking terminal block header I found which is 19-pin, 3.5mm pitch, and 180° (vertical) mating is the 1-2342071-9. The part is rather pricey, so if you don’t mind using an open sided variation, I would recommend the following two headers placed side-by-side:

1604890000 Weidmüller 14-Pin 3.50mm Open Sidewall Omnimate SL series vertical header

1604800000 Weidmüller 15-Pin 3.50mm Open Sidewall Omnimate SL series vertical header

These can be placed side-by-side and fit the same 19-pin hole pattern because of the lack of sidewalls. Because of this, a single 19-pin plug can still be used, if desired.

We’ll check this out. Thank you.

In case it doesn’t fit, can you also recommend an alternative similar to 1841800000 but just with longer pins. Say, where the connector can extend forward farther?

Hello @analogcay

I did not find an alternative part similar to part number 1841800000 but with longer pins.