Sourcing 9mm Audio Potentiometers

I currently have a customer’s high end multi-channel Audio Amplifier on the bench in pieces, The Volume pots have simply worn out and have become noisy.

The pots in question are 9mm vertical mount with a sleeve shaft collar. There are no markings other than B503 on the bottom so there are obviously 50K linear but of unknown manufacture. I can find numerous suppliers with the collarless versions but with no other mechanical support for the shaft I doubt they would last very long. I am having real trouble sourcing suitable replacements.

I am looking for;

  • Bourns : PTV09A-1030F-503
  • Alpha : RV09ACF-40-30F-B50K
  • Same Sky : PT01-A130D-B503
  • Alps Alpine : RK09D1130-F30-C0-B503

Can you help me with any of these parts?

Welcome to the TechForum william.walters! Do you have any pictures of the originals? I am not sure what is meant by “no mechanical support for the shaft.” Do you mean something with a bushing?

I’ve got similar hits to some of those parts:
1: PTV09A-4030F-B503
3: PT01-D130D-B503

These don’t appear to have bushings, though. Here is a list of options that are similar to the ones above that do have bushings for mechanical supports:

50K Options With Different Size Bushings

Hi Kaleb,

Thanks for your response. The image below on the left shows the part I need. The image on the right is the collarless version which is of no use to me and I’m sure you can see the difference. It has to be a direct replacement for the existing pots in the amplifier. The collarless version will not have the mechanical robustness to do the job and nothing else will fit.

I have received a response from Bourns who where very helpful but say that they have never actually made this particular part but could if I ordered 1000. I only need 3!!

Unfortunately, the OEM, Acus amplifiers, Italy, are being most unhelpful. They haven’t even had the courtesy to reply to my enquiry about sourcing replacements.

Regards,

John Walters

I don’t see any images attached. If I had to guess, ACUS probably had a specific collar/bushing that isn’t “standard.” Not too uncommon for OEMS, unfortunately. Is there any way you could retrofit it?

Without Collar (ignore different shaft for now)

With Collar, This is the form I need.

Hello william.walters,

The closest match I found for 50K, and with a sleeve, is part number 2223-PT01-D225D-A503-ND. If you need a longer shaft, but best option is part number PTV09A-4225F-A503-ND, which does not have a collar. Both have a 10mm wide body.
Please check the datasheets to verify compatibility to your application.