Hope this category/forum is appropriate for this query.
I am after a female spade connector and nylon housing for my domestic oven. Refer to the attached images at the bottom of this post to see the existing terminal crimp and housing to be replaced.
Assuming these will need to be high temp rated, provided that some of the wiring is for power (10~20A max) and therefore nickel plated steel is reqruied, rather than brass/tin? Below specs have been found to be potential candidates, however, I’d like to seek advice from those who have the knowledge since I am playing guesswork.
Any assistance/comments would be appreciated.
EXISTING SPEC
locking female spade terminal
6.35 x 0.8mmwire diameter aprox 1.8mm
6.35 x 0.8mm
wire diameter aprox 1.8mm
9mm housing/tab
PROPOSED SPEC
Terminal options:
RS#: 205-5288
RS#: 905-3390
Housing options:
RS#: 680-2962
RS#: 688-1029