Hello everyone,
I need to generate a square wave at 600kHz with the TLC555. On the datasheet (7.3.2 Astable Operation) TI advise us to use there calculation tool for the frequencies above 100kHz. So I download it and I introduce the value in the tool for the calculation : Vcc = 5V , C1 = 0.1n , Freq = 600kHz , Duty Cycle = 50% , and I check the box “Use Diode?” (for the ~50% duty cycle)
After that I introduce the value calculated in a Spice simulation (I use “PSpice for TI” and it should had the best spice model for the simulation (the encrypted one))

And the problem is that the result of the simulation don’t match with the calculation design tool ! and I don’t understand why … Is my simulation wrong ? is the TI tool’s wrong ? is the model of TI wrong ?
So if someone can help me I will be very grateful ! 'cause I can’t find the answer ![]()
Thank you very much !!