コンデンサはもともと蓄電器として知られ、エネルギーを集めて蓄えることができるアナログ部品です。その多くはバッテリのようにプラスとマイナスの端子が付いていますが、機能は大きく異なります。コンデンサは、ほとんど瞬時に放電することができますが、長期的なエネルギー貯蔵には向いていません。通常、2枚のプレート(導電体)で構成され、その間に誘電体があります。この誘電体は、ガラス、セラミック、プラスチックフィルム、紙、あるいは空気で構成されます。コンデンサは、入ってくるエネルギーを取り込み、静電界に蓄え、回路設計によってエネルギーが流れるようにします。コンデンサは静電容量によって分類されます。静電容量とは、コンデンサが蓄えることのできる総エネルギーのことで、単位はファラッドです。