#920061308

Hi Not sure if you can help.

But we have a Pionner F-X99ZL FM / AM Digital box as part of a Hifi unit and require a cable to extend to the main stereo.

The cable slots into the main Hifi system for sound etc. But require a cable extend this by 12 - 15 inches so we can move the radio box to sit alongside the main box, instead of sitting on top the main Hifi unit.

Hope that makes sense.

Mant thanks
JIm

Hello,

What type of cable do you need?

Hi Karl, it is a Pionner cable, check picture. This goes into the back of the hifi system, so I need one that clicks into this and then this connector to go back into the HiFi box. If that makes sense SO I can extend by 12-15 inches..Thanks Jim

Hello,

Unfortunately, we do not carry one like this.

Hi jimgiddins,

I’m fairly sure that is a proprietary cable for Pioneer, and I doubt that they ever made what would essentially be an extension cable for it.

It’s conceivable that perhaps longer ones were made at one time and you could find one on e-bay or similar, but I’d be a bit surprised.

I’m sure you’d probably rather not do it, but I’d recommend cutting it somewhere in the middle and adding some sort of readily-available connectors on each cut end and then make an extension cable using mates to those same connectors.

As an example, you could use the following cable assembly and mating connectors:

  • 1939-1887-ND Cable assembly, L = 1m (3.28ft), with Molex Micro-Fit 3.0 connectors

  • WM2764-ND mating Micro-Fit 3.0 connector housing (to be mounted on cut ends of your cable)

Contacts for the WM2764-ND (choose based on wire gauge of your cable):