Help me, I can't find this FFC anywhere

I have been searching for months. I need An FFC Cable for one of my 3D printers, the issue is the length I need. Most max out at 400mm in length

24Pin | 0.5 Pitch | 600mm Length | Reversed FFC. From memory, it was about 24-25mm wide.

Any help would be greatly appreciated

Hi @D3FCON ,
Could not find one either. You could consider having an extender to join two shorter ones or one 600mm type A (non-reversed) and one short type B.

Cheers, heke

@D3FCON

I also found the FJH-24-R-60.00-4-ND.
This one is 1524mm long.
However it looks like we may be able to special order on that would meet your exact length.
If that one would otherwise work we can look at submitting that request to have the correct length quoted to you.

If that is something that you would like to do you can direct message me you details and can start working on that.

Hi,
Welcome to the DigiKey TechForum. Take a look at DigiKey part WM16396-ND to see if this option will work for you.

I have thought of that but it wont work in my case as the rail has no space for a connector fitment unless I create a hole to run the cable in and out of the inside of the rail, see image

It looks like Steve may have an options a post up from this one that I am going to look into, This particular 3D Printer is rare and is more of a prototype release. It actually came with spare cables but there faulty now also so I think i am going to need a bunch over the span of it’s life :slight_smile: “Atomstack Cambrian Pro”