Hello,
I have the below connector where I beleive is a kind of molex connector but I can’t find it anywhere in your site. Do you know what is the name of it?
I am not seeing this one either. To me it looks more like a terminal block. Though I went through all the options and was not able to find anything. Sorry. Generally others view this and can help also. Hoefully they will find something.
Hi oktabitt,
I suspect it’s the Samtec IPBS-115-01-T-D-GP. Note that the image on our website is a bit different from the actual part, in particular, on the ends.
Here’s an image from their datasheet:
As a note, the key to finding this part was figuring out the pitch (space from pin-center to pin-center) and then searching by this pitch length within the category "Rectangular Connectors → Headers, Receptacles, Female Sockets. I used your image and read length from first pin to last pin, and divided that length by one less than the number of pins (so, 14) to get a pitch of 4.167mm. Looking withing the above-mentioned category, I found that the nearest pitch was 4.20mm or 0.165 inches, so I selected that, and then filtered “30” for “Number of Positions” to narrow it down.
Mating Pitch and Number of Positions:
Many thanks. This was the right connector.