Voltage sensor and current sensor

I need a voltage sensor and a current sensor.

  1. Voltage sensor, input voltage around 250V AC and output voltage around 5V AC.
  2. Current sensor, input current 50A-315A and output current is 40mA.
    Kindly suggest me few of them with part number.

Hello,

I am not having any luck finding the voltage sensor. I found this link: Current/Voltage Transducer Monitors | Monitors | Electronic Components Distributor DigiKey

The input is DC though. Maybe someone else can offer suggestions.

I found these options that would list the current you need. Though the voltages for the output are listed as ratiometric. This would mean I would say the voltage would be ratiometric to your inout voltage. I did not see anything on the list I found that would have the input voltage of 40 volts. Here is what I found:

I hope someone else can find better parts than what I did. Hopefully someone can find closer to what you need.

I’ve located the voltage transducer. Here’s the datasheet link—See if it’s what you need.