Adjusting the Voltage of an Output Module for the NEVO+ Series

How to adjust the voltage of an output module fitted to a NEVO+600 or NEVO+1200 industrial and medical power supply:

When setting the voltage of the output modules, the input power connector must be attached, and the unit must be powered up.

Be careful not to make contact with the input side of the unit from now on as the unit is live. The input side of the unit should be isolated to ensure safe configuration.

Set the voltage set points using a calibrated multi meter and potentiometer.

The use of shielded test leads with clips, prevents accidental shorting of the module terminals and insures a good connection.

Once these are clipped into place begin adjusting the output module 1 to the desired voltage. Turning the potentiometer anticlockwise decreases the voltage. Turning it clockwise increases the voltage. Repeat the process to configure the remaining modules to the desired voltage using your multimeter as a reference.

For an example, view the demonstration video to see how we set a module to 5VDC.