BMW Connector

I’m trying to locate any parts for a connector from my 2015 BMW i3. I bought a used module on eBay trying to salvage the connector but I’m still having a hard time trying to find the pins.

Any pointers would be greatly appreciated.



On the top picture, the symbol above the number is for the manufacture TE Connectivity. The part number 3-967415-1 comes up, but it only says the part is restricted. So it is a proprietary part, made specifically for BMW, and you will not be able to buy it through regular distributors. The part number from the second picture 3-965775-1 comes up also, and is listed as an Active part (no restrictions listed), but it does not list an pins or other information. You should try contact the manufacture to see if the contacts are available. Their website says they offer 24/7 support, and has a live chat option. You can also call them at 1-800-522-6752.

2 Likes

Hello. I’m not sure if you got a sufficient answer to this question, but your question came up when I was searching for something in a similar domain, so I thought to add my information to your question either for you or for others in the future…

From what I have seen, BMW connectors that look like this from TE Connectivity are based on the “Micro Quadlock System” (small square pins), “Micro Power Quadlock” (small 2.6mm tabs and sockets), and “Power Quadlock” (larger 5.2mm tabs and sockets).

You can usually find MQS pin pigtails from BMW Parts departments (search google shopping for ‘BMW Pin Contact MQS with Cable’), but I think you are looking for the socket side, not the pin side (search google for ’ BMW MQS Bushing Contact w/ Wire Lead’). I recently ordered some of these MQS sockets (which I think would be good for your case): https://www.digikey.com/en/products/detail/te-connectivity-amp-connectors/5-968221-6/10467605

I like the flexibility of being able to use my own wires and do the crimp. There are lots of variations on the MQS/MPQ/PQ connectors (wire gauge, materials, etc.) - just search on the Digikey site under Rectangular Connectors with filters for “Micro Quadlock”, “Micro Power Quadlock”, and “Power Quadlock”: https://www.digikey.com/short/p0m1qr1q

I found those specific terms via the BMW TIS (technical information systems) website which has all the wiring diagrams/repair instructions for BMWs (it’s paywalled, but only $30 for a day to grab all your info).

1 Like

Thank you for the input, this is helpful.