Need help in identifying correct female connector. I only have photos of male connector. It is 22 pin connector but i need only one female connector to go into male connector. I am installing trailer harness on mazda cx 50 turbo. Connector goes on to battery jumper harness cable.
We can take a look for an option.
Would you be able to attach the images to a reply?
Yes i attached some photos. Can only upload 3 photos.
While I take a look.
Would you be able to measure the center to center distances from one contact to another?
Both in row and row to row.
I am not having luck finding a matching housing to then also look for a possible matching contact for the housing.
Yes nathan , i will measure and send you soon distance.
Hi nathan i only need connector terminal and not housing.
It is something like this digi key part number id
900-2163012212-ND. I purchased from somewhere same part with 14-16 awg. But it is not going in.
When identifying a terminal/contact it maybe possible(but mostly uncommon) to be able to track the item by just the image of the contact or even additional dimensional reference to the contact as a fair many a look very similar and in some cases may even kind of work.
If one can ID the housing the contact is meant to go into one can then look at the contacts that housing is meant to use to find the target item.
With the center to center (inter row and row to row) measurements(pitch) this can help narrow the option we have to look at.
Also, come housings have enough marking on them that too (with the pitch) can help even more to find a contact that can be use to replace or add in to the on hand housings
Hi nathan sorry for late reply.
Inter row distanace is 3 mm and row to row is 5 mm. I tool scale to measure as best as i can do. Thanks.
Sorry, I did not have luck IDing the housing that is shown.