What is this part? I need help identifying the part in the picture. 14 pin D-type converter monitor?
I believe pin one is in the upper left corner. it appears to be a voltage monitor/regulator/converter with connections to an MCU. MCU connections may be for ADC, I2C, or GPIO?
2nd image shows pins 2, 3, 4 connected to system voltages. Pins 5, 6, and 7 go to the MCU.
I am sorry I cannot identify the part.
Can anyone say what that package type is properly/formally called? The 3x4 pin distribution should have a unique identifier, shouldn’t it?
Yes, this has become a real challenge. I expect the part may be replaced by a newer version/design.
Hello @james.kennedy
Saw this on a USB controller so not the same part but they are calling out a QWFN14 package and it appears to be laid out similarly to your ic.

-Robert
Hey! That helps. Thank you, all, for your efforts on this difficult part.
What company made that USB part?
OnSemi -
Here is a link to the datasheet.
-Robert
1 Like
Thank you, Robert.
I keep
hoping that someday, someone will recognize this unique part.
James
It’s interesting how the package marked QSAB JTH has little stubs sticking out of the WQFN14-like package. I wonder if that pre-dated the clipped stubs (the “N”?) of the WQFN14?
Looks like TI calls a very similar looking package a 14-UQFN also. It’s 2.5mm square. For example, the LMH6554LEE/NOPB has this package type. Part markings are different, so this is not it either, but this gives you an additional package type to search for.