Help with choosing the correct hardware for harness

Howdy. I’m trying to find the correct part connectors and pins and crimping tools to build the harness my newest drone. The connector that works with the flight controller is DF1B-18DP-2.5DS.
I need the male connector correct pins for same. This will spider out to 3 modules using a JST-GH-6P, SH1.0-4P and the third I need some help with. The pins are 2.5 with 6 pins, however I only need to engage 4 of them and they’re inline with each other. It would also be helpful for it to be a 90 degree connector for the sake of cleanliness. The other connector is a 3 pin for the 18 awg motor wires.
Also the correct crimper and wire cutter to handle the silicone wires.
Thank you

Hello, welcome to the TechForum!

For connector DF1B-18DP-2.5DS, I was able to find H3817-ND in our system as the housing, H3828-ND as an option for the contacts, and H9936-ND as the crimp tool for these. For JST-GH-6P I was able to find 455-1596-ND, 455-1606-1-ND, and 455-2883-ND as the housing, contacts, and crimp tool. Unfortunately the largest wire gauge I could find for your first connector is 20AWG, and the second connector is 26AWG. I was unable to find options for 18AWG

Thank you so far Mr Johnson. Will the JRready crimping tool also work? I’ve used them before and they’re in a satisfactory price range. It doesn’t have to be a rectangle connector. I’m just trying to do as little soldering as possible.