Differential-input amplifier topologies like the difference amplifier and current-sense amplifier are highly effective for amplifying differential signals in various applications, particularly when dealing with very high common-mode voltages.
However, for applications requiring amplification of extremely small signals with exceptional precision, especially in the presence of substantial common-mode voltages and noise, even more precise amplifiers are necessary. This is where instrumentation amplifiers (in-amps) come into play, as they are specifically designed to meet these stringent requirements.
Limitations of Difference Amplifiers
When comparing a difference amplifier to an instrumentation amplifier, one key drawback of the difference amplifier is its relatively low input impedance. Another issue is that the impedance at each amplifier input isn’t equal. These limitations become significant in applications like amplifying a differential signal (V2 – V1) from a Wheatstone bridge (Figure 11) , which is commonly used in various sensor systems.
A first concern is that many wheatstone bridges have significant output impedance, which has to drive the low input impedance of the difference amplifier. For example, if the bridge has an output impedance of 4 kΩ and the amplifier has an input impedance of 200 kΩ, 2% of the sensor’s signal would be lost due to voltage drop across the bridge. This loss is unacceptable in precision measurements.
Another issue is that the unequal input impedances of the difference amplifier cause uneven voltage drops across the two sides of the bridge, introducing errors in the measured differential voltage.
To solve these issues, it is necessary to use an amplifier that has a much higher input impedance, presents a balanced load on the bridge outputs, and has excellent CMRR. These are the key features and advantages of an instrumentation amplifier.
Instrumentation Amplifier
The classic 3-op-amp instrumentation amplifier (Figure 12a) consists of two main stages. The first stage, (preamp stage), includes two operational amplifiers (A1 and A2), while the second stage, (subtractor stage), uses a third op-amp (A3). The subtractor stage follows the familiar difference amplifier topology.
In this design, A1 and A2 provide extremely high and balanced input impedance. They also amplify the differential input voltage and pass the common-mode voltage through without amplification. The subtractor stage (A3) then removes the common-mode voltage and outputs the amplified differential signal.
One key advantage of this topology is that the gain can be easily set using a single external resistor (RG), eliminating the need to match discrete resistor ratios. This makes it particularly well-suited for amplifying very small signals while rejecting high levels of common-mode voltage. The transfer function of this instrumentation amplifier is:
VOUT = G × VDIFF + VREF
Here, VDIFF represents the difference in input voltages (V+IN – V–IN), G is the gain of the amplifier, and VREF is the reference voltage that adjusts the output level.
Integrated instrumentation amplifiers (Figure 12b) offer additional benefits due to possessing precisely matched resistors on the same monolithic chip. Whereas common-mode rejection of an integrated difference amplifier might be in the range of 90 dB to 100 dB, many in-amps have a CMRR specification of 130 dB to 140 dB or more.
Returning to the earlier Wheatstone bridge example, with a source resistance of 4 kΩ and an instrumentation amplifier like ADI’s AD8422 (which has an input resistance of 200 GΩ), the signal loss is minuscule—just 0.000002% (0.02 ppm).
Another advantage of instrumentation amplifiers is their lower input bias current compared to difference amplifiers. This results in less voltage error caused by bias currents flowing through the source resistance, further enhancing precision.
Related Articles
The Role of Difference Amplifiers in Precision Sensor Systems
Current-Sense Amplifiers and Their Distinction from Difference Amplifiers
Understanding Single-Ended Operational Amplifier Topology for Precision Sensor Applications
Applicable Part Numbers
| DigiKey Part Number | Manufacturer Part Number |
|---|---|
| MCP6N11-001E/SN-ND | MCP6N11-001E/SN |
| MCP6N11T-001E/MNYTR-ND,MCP6N11T-001E/MNYCT-ND,MCP6N11T-001E/MNYDKR-ND | MCP6N11T-001E/MNY |
| MCP6N11T-010E/SNTR-ND,MCP6N11T-010E/SNCT-ND,MCP6N11T-010E/SNDKR-ND | MCP6N11T-010E/SN |
| 296-INA823DRTR-ND,296-INA823DRCT-ND,296-INA823DRDKR-ND | INA823DR |
| 296-30588-2-ND,296-30588-1-ND,296-30588-6-ND | INA827AIDGKR |
| MCP6N16T-010E/MSTR-ND,MCP6N16T-010E/MSCT-ND,MCP6N16T-010E/MSDKR-ND | MCP6N16T-010E/MS |
| MCP6N16-100E/MS-ND | MCP6N16-100E/MS |
| 296-19951-2-ND,296-19951-1-ND,296-19951-6-ND | INA321EA/2K5 |
| 296-36596-2-ND,296-36596-1-ND,296-36596-6-ND | INA826AIDRGR |
| 296-30238-2-ND,296-30238-1-ND,296-30238-6-ND | INA826AIDR |
| 296-29663-2-ND,296-29663-1-ND,296-29663-6-ND | INA826AIDGKR |
| 296-INA823DTTR-ND,296-INA823DTCT-ND,296-INA823DTDKR-ND | INA823DT |
| 296-31643-2-ND,296-31643-1-ND,296-31643-6-ND | INA126UA/2K5 |
| 296-30347-2-ND,296-30347-1-ND,296-30347-6-ND | INA826AIDRGT |
| 296-33294-5-ND | INA826AID |
| 296-41257-2-ND,296-41257-1-ND,296-41257-6-ND | INA126EA/2K5 |
| INA126UA-ND | INA126UA |
| 296-38946-2-ND,296-38946-1-ND,296-38946-6-ND | INA126U/2K5 |
| 296-23564-2-ND,296-23564-1-ND,296-23564-6-ND | INA333AIDGKR |
| AD8237ARMZ-R7TR-ND,AD8237ARMZ-R7CT-ND,AD8237ARMZ-R7DKR-ND | AD8237ARMZ-R7 |
| 505-AD8237ARMZ-ND | AD8237ARMZ |
| 296-48550-2-ND,296-48550-1-ND,296-48550-6-ND | INA2132UA/2K5 |
| INA326EA/2K5TR-ND,INA326EA/2K5CT-ND,INA326EA/2K5DKR-ND | INA326EA/2K5 |
| 296-41266-2-ND,296-41266-1-ND,296-41266-6-ND | INA333AIDRGR |
| 296-INA333QDGKRQ1TR-ND,296-INA333QDGKRQ1CT-ND,296-INA333QDGKRQ1DKR-ND | INA333QDGKRQ1 |
| 505-AD8227ARMZ-ND | AD8227ARMZ |
| 505-AD8236ARMZ-R7TR-ND,505-AD8236ARMZ-R7CT-ND,505-AD8236ARMZ-R7DKR-ND | AD8236ARMZ-R7 |
| AD8227ARMZ-R7TR-ND,AD8227ARMZ-R7CT-ND,AD8227ARMZ-R7DKR-ND | AD8227ARMZ-R7 |
| 505-AD8223ARZ-ND | AD8223ARZ |
| AD8226ARZ-R7TR-ND,AD8226ARZ-R7CT-ND,AD8226ARZ-R7DKR-ND | AD8226ARZ-R7 |
| AD8226ARMZ-R7TR-ND,AD8226ARMZ-R7CT-ND,AD8226ARMZ-R7DKR-ND | AD8226ARMZ-R7 |
| 296-INA821IDRTR-ND,296-INA821IDRCT-ND,296-INA821IDRDKR-ND | INA821IDR |
| 296-INA821IDRGRTR-ND,296-INA821IDRGRCT-ND,296-INA821IDRGRDKR-ND | INA821IDRGR |
| 296-INA819IDRTR-ND,296-INA819IDRCT-ND,296-INA819IDRDKR-ND | INA819IDR |
| 296-INA819IDGKRTR-ND,296-INA819IDGKRCT-ND,296-INA819IDGKRDKR-ND | INA819IDGKR |
| 296-INA818IDRTR-ND,296-INA818IDRCT-ND,296-INA818IDRDKR-ND | INA818IDR |
| INA2132UA-ND | INA2132UA |
| 296-13453-2-ND,296-13453-1-ND,296-13453-6-ND | INA337AIDGKT |
| 296-15312-2-ND,296-15312-1-ND,296-15312-6-ND | INA326EA/250 |
| 296-24575-2-ND,296-24575-1-ND,296-24575-6-ND | INA333AIDRGT |
| 296-23565-2-ND,296-23565-1-ND,296-23565-6-ND | INA333AIDGKT |
| AD8553ARMZ-REELTR-ND,AD8553ARMZ-REELCT-ND,AD8553ARMZ-REELDKR-ND | AD8553ARMZ-REEL |
| 296-INA821IDGKTTR-ND,296-INA821IDGKTCT-ND,296-INA821IDGKTDKR-ND | INA821IDGKT |
| 296-38945-2-ND,296-38945-1-ND,296-38945-6-ND | INA122UA/2K5 |
| 505-AD8223BRZ-R7TR-ND,505-AD8223BRZ-R7CT-ND,505-AD8223BRZ-R7DKR-ND | AD8223BRZ-R7 |
| 296-INA819IDGKTTR-ND,296-INA819IDGKTCT-ND,296-INA819IDGKTDKR-ND | INA819IDGKT |
| 296-INA818ID-ND | INA818ID |
| 296-38944-2-ND,296-38944-1-ND,296-38944-6-ND | INA121UA/2K5 |
| 296-INA217AIDWRTR-ND,296-INA217AIDWRCT-ND,296-INA217AIDWRDKR-ND | INA217AIDWR |
| 505-AD8235ACBZ-P7-ND | AD8235ACBZ-P7 |
| MAX4208AUA+TTR-ND,MAX4208AUA+TCT-ND,MAX4208AUA+TDKR-ND | MAX4208AUA+T |
| 505-AD8231ACPZ-R7TR-ND,505-AD8231ACPZ-R7CT-ND,505-AD8231ACPZ-R7DKR-ND | AD8231ACPZ-R7 |
| AD8226BRMZ-R7TR-ND,AD8226BRMZ-R7CT-ND,AD8226BRMZ-R7DKR-ND | AD8226BRMZ-R7 |
| 296-13645-2-ND,296-13645-1-ND,296-13645-6-ND | INA217AIDWT |
| 296-INA851RGTR-ND,296-INA851RGTRCT-ND,296-INA851RGTRDKR-ND | INA851RGTR |
| INA163UA-ND | INA163UA |
| 296-48911-2-ND,296-48911-1-ND,296-48911-6-ND | INA122U/2K5 |
| AD623ARMZ-REELTR-ND,AD623ARMZ-REELCT-ND,AD623ARMZ-REELDKR-ND | AD623ARMZ-REEL |
| 505-AD623ARMZ-ND | AD623ARMZ |
| AD623ARZ-RLTR-ND,AD623ARZ-RLCT-ND,AD623ARZ-RLDKR-ND | AD623ARZ-RL |
| 505-AD623ARZ-ND | AD623ARZ |
| AD623ARZ-R7TR-ND,AD623ARZ-R7CT-ND,AD623ARZ-R7DKR-ND | AD623ARZ-R7 |
| 296-26058-2-ND,296-26058-1-ND,296-26058-6-ND | INA129UA/2K5 |
| 2156-INA125P-ND,INA125P-ND | INA125P |
| 505-AD8422ARMZ-R7TR-ND,505-AD8422ARMZ-R7CT-ND,505-AD8422ARMZ-R7DKR-ND | AD8422ARMZ-R7 |
| 505-AD8422ARMZ-ND | AD8422ARMZ |
| 296-26057-2-ND,296-26057-1-ND,296-26057-6-ND | INA128UA/2K5 |
| 505-AD8426ACPZ-R7TR-ND,505-AD8426ACPZ-R7CT-ND,505-AD8426ACPZ-R7DKR-ND | AD8426ACPZ-R7 |
| 296-41256-2-ND,296-41256-1-ND,296-41256-6-ND | INA121U/2K5 |
| LT1789CS8-1#PBF-ND | LT1789CS8-1#PBF |
| 296-26059-2-ND,296-26059-1-ND,296-26059-6-ND | INA129U/2K5 |
| 296-INA849DRTR-ND,296-INA849DRCT-ND,296-INA849DRDKR-ND | INA849DR |
| 296-INA849DGKRTR-ND,296-INA849DGKRCT-ND,296-INA849DGKRDKR-ND | INA849DGKR |
| 505-AD8421ARMZ-RLTR-ND,505-AD8421ARMZ-RLCT-ND,505-AD8421ARMZ-RLDKR-ND | AD8421ARMZ-RL |
| 505-AD8422ARZ-R7TR-ND,505-AD8422ARZ-R7CT-ND,505-AD8422ARZ-R7DKR-ND | AD8422ARZ-R7 |
| 505-AD8277BRZ-ND | AD8277BRZ |
| 296-41258-2-ND,296-41258-1-ND,296-41258-6-ND | INA141UA/2K5 |
| 505-AD8421ACPZ-R7TR-ND,505-AD8421ACPZ-R7CT-ND,505-AD8421ACPZ-R7DKR-ND | AD8421ACPZ-R7 |
| INA129PA-ND | INA129PA |
| 505-AD8221ARMZ-ND | AD8221ARMZ |
| AD8221ARMZ-R7TR-ND,AD8221ARMZ-R7CT-ND,AD8221ARMZ-R7DKR-ND | AD8221ARMZ-R7 |
| AD8221ARMZ-RLTR-ND,AD8221ARMZ-RLCT-ND,AD8221ARMZ-RLDKR-ND | AD8221ARMZ-RL |
| MAX4194ESA+TR-ND,MAX4194ESA+CT-ND,MAX4194ESA+DKR-ND | MAX4194ESA+T |
| LTC6915CDE#PBF-ND | LTC6915CDE#PBF |
| INA121U-ND | INA121U |
| AD8220ARMZ-R7TR-ND,AD8220ARMZ-R7CT-ND,AD8220ARMZ-R7DKR-ND | AD8220ARMZ-R7 |
| 505-AD8220ARMZ-ND | AD8220ARMZ |
| AD623ANZ-ND | AD623ANZ |
| LTC6915IGN#PBF-ND | LTC6915IGN#PBF |
| 505-LTC6915IDE#PBF-ND | LTC6915IDE#PBF |
| AD8221ARZ-R7TR-ND,AD8221ARZ-R7CT-ND,AD8221ARZ-R7DKR-ND | AD8221ARZ-R7 |
| 505-AD8221ARZ-ND | AD8221ARZ |
| AD8421ARZ-R7TR-ND,AD8421ARZ-R7CT-ND,AD8421ARZ-R7DKR-ND | AD8421ARZ-R7 |
| 505-AD8421ARZ-ND | AD8421ARZ |
| 296-46091-2-ND,296-46091-1-ND,296-46091-6-ND | INA114AU/1K |
| 505-AD8295ACPZ-R7TR-ND,505-AD8295ACPZ-R7CT-ND,505-AD8295ACPZ-R7DKR-ND | AD8295ACPZ-R7 |
| INA128UA-ND | INA128UA |
| INA129U-ND | INA129U |
| 505-AD8220WARMZ-R7TR-ND,505-AD8220WARMZ-R7CT-ND,505-AD8220WARMZ-R7DKR-ND | AD8220WARMZ-R7 |
| 505-AD8220WARMZ-ND | AD8220WARMZ |
| 505-LTC6915HGN#PBF-ND | LTC6915HGN#PBF |
| LT1789CS8-1#TRPBFTR-ND,LT1789CS8-1#TRPBFCT-ND,LT1789CS8-1#TRPBFDKR-ND | LT1789CS8-1#TRPBF |
| 2156-INA128PA-ND,INA128PA-ND | INA128PA |
| 505-AD8228ARZ-R7TR-ND,505-AD8228ARZ-R7CT-ND,505-AD8228ARZ-R7DKR-ND | AD8228ARZ-R7 |
| AD622ARZ-ND | AD622ARZ |
| 505-AD622ARZ-R7TR-ND,505-AD622ARZ-R7CT-ND,505-AD622ARZ-R7DKR-ND | AD622ARZ-R7 |
| 505-AD622ARZ-RLTR-ND,505-AD622ARZ-RLCT-ND,505-AD622ARZ-RLDKR-ND | AD622ARZ-RL |
| 505-AD5751ACPZ-REEL7TR-ND,505-AD5751ACPZ-REEL7CT-ND,505-AD5751ACPZ-REEL7DKR-ND | AD5751ACPZ-REEL7 |
| 505-AD8426BCPZ-R7TR-ND,505-AD8426BCPZ-R7CT-ND,505-AD8426BCPZ-R7DKR-ND | AD8426BCPZ-R7 |
| INA114AP-ND | INA114AP |
| AD627ARZ-RLTR-ND,AD627ARZ-RLCT-ND,AD627ARZ-RLDKR-ND | AD627ARZ-RL |
| 505-AD627ARZ-R7TR-ND,505-AD627ARZ-R7CT-ND,505-AD627ARZ-R7DKR-ND | AD627ARZ-R7 |
| 505-AD627ARZ-ND | AD627ARZ |
| LT1789IS8-1#TRPBFTR-ND,LT1789IS8-1#TRPBFCT-ND,LT1789IS8-1#TRPBFDKR-ND | LT1789IS8-1#TRPBF |
| 505-AD8429ARZ-R7TR-ND,505-AD8429ARZ-R7CT-ND,505-AD8429ARZ-R7DKR-ND | AD8429ARZ-R7 |
| 505-AD8429ARZ-ND | AD8429ARZ |
| 505-AD8422BRMZ-ND | AD8422BRMZ |
| 505-AD622ANZ-ND | AD622ANZ |
| 505-LT1167CS8#PBF-ND | LT1167CS8#PBF |
| LT1167CS8#TRPBFTR-ND,LT1167CS8#TRPBFCT-ND,LT1167CS8#TRPBFDKR-ND | LT1167CS8#TRPBF |
| LT1168CS8#TRPBFTR-ND,LT1168CS8#TRPBFCT-ND,LT1168CS8#TRPBFDKR-ND | LT1168CS8#TRPBF |
| 505-LT1168CS8#PBF-ND | LT1168CS8#PBF |
| 505-LT1920IS8#PBF-ND | LT1920IS8#PBF |
| AD8225ARZ-ND | AD8225ARZ |
| AD623BRZ-R7TR-ND,AD623BRZ-R7CT-ND,AD623BRZ-R7DKR-ND | AD623BRZ-R7 |
| 296-INA2128UA/1KTR-ND,296-INA2128UA/1KCT-ND,296-INA2128UA/1KDKR-ND | INA2128UA/1K |
| 505-AD8222ACPZ-R7TR-ND,505-AD8222ACPZ-R7CT-ND,505-AD8222ACPZ-R7DKR-ND | AD8222ACPZ-R7 |
| 296-35901-2-ND,296-35901-1-ND,296-35901-6-ND | INA128U/2K5 |
| AD8220BRMZ-RLTR-ND,AD8220BRMZ-RLCT-ND,AD8220BRMZ-RLDKR-ND | AD8220BRMZ-RL |
| AD8220BRMZ-R7TR-ND,AD8220BRMZ-R7CT-ND,AD8220BRMZ-R7DKR-ND | AD8220BRMZ-R7 |
| 505-AD8220BRMZ-ND | AD8220BRMZ |
| 505-AD8224ACPZ-R7TR-ND,505-AD8224ACPZ-R7CT-ND,505-AD8224ACPZ-R7DKR-ND | AD8224ACPZ-R7 |
| AD627ANZ-ND | AD627ANZ |
| 505-LT1167IS8#PBF-ND | LT1167IS8#PBF |
| LT1167IS8#TRPBFTR-ND,LT1167IS8#TRPBFCT-ND,LT1167IS8#TRPBFDKR-ND | LT1167IS8#TRPBF |
| 505-AD8421BRMZ-ND | AD8421BRMZ |
| AD8421BRMZ-R7TR-ND,AD8421BRMZ-R7CT-ND,AD8421BRMZ-R7DKR-ND | AD8421BRMZ-R7 |
| AD8421BRMZ-RLTR-ND,AD8421BRMZ-RLCT-ND,AD8421BRMZ-RLDKR-ND | AD8421BRMZ-RL |
| AD620ARZ-REEL7TR-ND,AD620ARZ-REEL7CT-ND,AD620ARZ-REEL7DKR-ND | AD620ARZ-REEL7 |
| 505-AD620ARZ-ND | AD620ARZ |
| 505-AD620ARZ-REELTR-ND,505-AD620ARZ-REELCT-ND,505-AD620ARZ-REELDKR-ND | AD620ARZ-REEL |
| 296-44818-2-ND,296-44818-1-ND,296-44818-6-ND | INA141U/2K5 |
| 505-AD8221BRZ-ND | AD8221BRZ |
| AD8221BRZ-R7TR-ND,AD8221BRZ-R7CT-ND,AD8221BRZ-R7DKR-ND | AD8221BRZ-R7 |
| 296-26056-2-ND,296-26056-1-ND,296-26056-6-ND | INA118U/2K5 |
| 505-AD8421BRZ-ND | AD8421BRZ |
| AD8421BRZ-R7TR-ND,AD8421BRZ-R7CT-ND,AD8421BRZ-R7DKR-ND | AD8421BRZ-R7 |
| INA2128UA-ND | INA2128UA |
| INA114BP-ND | INA114BP |
| 505-AD627BRZ-R7TR-ND,505-AD627BRZ-R7CT-ND,505-AD627BRZ-R7DKR-ND | AD627BRZ-R7 |
| AD627BRZ-RLTR-ND,AD627BRZ-RLCT-ND,AD627BRZ-RLDKR-ND | AD627BRZ-RL |
| INA128U-ND | INA128U |
| 505-AD627BRZ-ND | AD627BRZ |
| 505-AD8253ARMZ-RLTR-ND,505-AD8253ARMZ-RLCT-ND,505-AD8253ARMZ-RLDKR-ND | AD8253ARMZ-RL |
| 505-AD8253ARMZ-R7TR-ND,505-AD8253ARMZ-R7CT-ND,505-AD8253ARMZ-R7DKR-ND | AD8253ARMZ-R7 |
| 505-AD8253ARMZ-ND | AD8253ARMZ |
| LT1101CN8#PBF-ND | LT1101CN8#PBF |
| INA114BU-ND | INA114BU |
| 2156-INA115BU-ND,INA115BU-ND | INA115BU |
| AD8250ARMZ-R7TR-ND,AD8250ARMZ-R7CT-ND,AD8250ARMZ-R7DKR-ND | AD8250ARMZ-R7 |
| 505-AD8251ARMZ-ND | AD8251ARMZ |
| 505-AD8250ARMZ-ND | AD8250ARMZ |
| AD8251ARMZ-R7TR-ND,AD8251ARMZ-R7CT-ND,AD8251ARMZ-R7DKR-ND | AD8251ARMZ-R7 |
| INA128P-ND | INA128P |
| INA141U-ND | INA141U |
| INA118P-ND | INA118P |
| 296-PGA204AU/1KTR-ND,296-PGA204AU/1KCT-ND,296-PGA204AU/1KDKR-ND | PGA204AU/1K |
| INA118U-ND | INA118U |
| AD8429BRZ-R7TR-ND,AD8429BRZ-R7CT-ND,AD8429BRZ-R7DKR-ND | AD8429BRZ-R7 |
| 505-AD8429BRZ-ND | AD8429BRZ |
| 505-AD620ANZ-ND | AD620ANZ |
| AD621ARZ-R7TR-ND,AD621ARZ-R7CT-ND,AD621ARZ-R7DKR-ND | AD621ARZ-R7 |
| 505-AD621ARZ-ND | AD621ARZ |
| 505-LT1101SW#PBF-ND | LT1101SW#PBF |
| LT1167ACS8#TRPBFTR-ND,LT1167ACS8#TRPBFCT-ND,LT1167ACS8#TRPBFDKR-ND | LT1167ACS8#TRPBF |
| 505-LT1167ACS8#PBF-ND | LT1167ACS8#PBF |
| 296-25555-2-ND,296-25555-1-ND,296-25555-6-ND | INA129MDREP |
| 2156-INA110KU-ND,INA110KU-ND | INA110KU |
| AD8224BCPZ-R7TR-ND,AD8224BCPZ-R7CT-ND,AD8224BCPZ-R7DKR-ND | AD8224BCPZ-R7 |
| INA111BU-ND | INA111BU |
| AD8224HBCPZ-R7TR-ND,AD8224HBCPZ-R7CT-ND,AD8224HBCPZ-R7DKR-ND | AD8224HBCPZ-R7 |
| 505-AD8222BCPZ-R7TR-ND,505-AD8222BCPZ-R7CT-ND,505-AD8222BCPZ-R7DKR-ND | AD8222BCPZ-R7 |
| 505-AD620BRZ-ND | AD620BRZ |
| AD620BRZ-R7TR-ND,AD620BRZ-R7CT-ND,AD620BRZ-R7DKR-ND | AD620BRZ-R7 |
| PGA204AU-ND | PGA204AU |
| 505-AD8421TRMZ-EP-ND | AD8421TRMZ-EP |
| 296-49183-2-ND,296-49183-1-ND,296-49183-6-ND | INA118UB/2K5 |
| 505-LT1167AIS8#PBF-ND | LT1167AIS8#PBF |
| AMP02FSZ-RLTR-ND,AMP02FSZ-RLCT-ND,AMP02FSZ-RLDKR-ND | AMP02FSZ-RL |
| AMP04FSZ-R7TR-ND,AMP04FSZ-R7CT-ND,AMP04FSZ-R7DKR-ND | AMP04FSZ-R7 |
| AMP04FSZ-ND | AMP04FSZ |
| 2156-INA2128U-ND,INA2128U-ND | INA2128U |
| PGA204BU-ND | PGA204BU |
| INA118UB-ND | INA118UB |
| LT1101AIN8#PBF-ND | LT1101AIN8#PBF |
| AD620BNZ-ND | AD620BNZ |
| 505-AD621BRZ-R7TR-ND,505-AD621BRZ-R7CT-ND,505-AD621BRZ-R7DKR-ND | AD621BRZ-R7 |
| 505-AD621BRZ-ND | AD621BRZ |
| PGA205BU-ND | PGA205BU |
| 505-AD524ARZ-16-ND | AD524ARZ-16 |
| 505-AD8428BRZ-ND | AD8428BRZ |
| AMP02FPZ-ND | AMP02FPZ |
| AMP04FPZ-ND | AMP04FPZ |
| AMP04ESZ-ND | AMP04ESZ |
| 2156-PGA206UA-ND,PGA206UA-ND | PGA206UA |
| 2156-PGA207UA-ND,296-15093-5-ND | PGA207UA |
| AMP02EPZ-ND | AMP02EPZ |
| AD524ADZ-ND | AD524ADZ |
| AD524BDZ-ND | AD524BDZ |
| 296-INA350ABSIDDFRTR-ND,296-INA350ABSIDDFRCT-ND,296-INA350ABSIDDFRDKR-ND | INA350ABSIDDFR |
| 296-INA350CDSIDDFRTR-ND,296-INA350CDSIDDFRCT-ND,296-INA350CDSIDDFRDKR-ND | INA350CDSIDDFR |
| 296-INA350ABSIDSGRTR-ND,296-INA350ABSIDSGRCT-ND,296-INA350ABSIDSGRDKR-ND | INA350ABSIDSGR |
| 296-INA350CDSIDSGRTR-ND,296-INA350CDSIDSGRCT-ND,296-INA350CDSIDSGRDKR-ND | INA350CDSIDSGR |
| 296-INA351ABSIDSGRTR-ND,296-INA351ABSIDSGRCT-ND,296-INA351ABSIDSGRDKR-ND | INA351ABSIDSGR |
| 296-INA351CDSIDSGRTR-ND,296-INA351CDSIDSGRCT-ND,296-INA351CDSIDSGRDKR-ND | INA351CDSIDSGR |
| 296-41265-2-ND,296-41265-1-ND,296-41265-6-ND | INA332AIDGKR |
| MCP6N11T-010E/MNYTR-ND,MCP6N11T-010E/MNYCT-ND,MCP6N11T-010E/MNYDKR-ND | MCP6N11T-010E/MNY |
| MCP6N11T-100E/MNYTR-ND,MCP6N11T-100E/MNYCT-ND,MCP6N11T-100E/MNYDKR-ND | MCP6N11T-100E/MNY |
| MCP6N11-010E/SN-ND | MCP6N11-010E/SN |
| MCP6N11-100E/SN-ND | MCP6N11-100E/SN |
| 296-12204-2-ND,296-12204-1-ND,296-12204-6-ND | INA332AIDGKT |
| 296-41264-2-ND,296-41264-1-ND,296-41264-6-ND | INA2332AIPWR |
| 296-INA823DGKRTR-ND,296-INA823DGKRCT-ND,296-INA823DGKRDKR-ND | INA823DGKR |
| 296-12202-2-ND,296-12202-1-ND,296-12202-6-ND | INA331AIDGKT |
| MCP6N16-100E/MF-ND | MCP6N16-100E/MF |
| INA322EATR-ND,INA322EACT-ND,INA322EADKR-ND,2156-INA322EA/250-ND | INA322EA/250 |
| 296-44980-2-ND,296-44980-1-ND,296-44980-6-ND | INA2331AIPWR |
| 296-INA823DGKTTR-ND,296-INA823DGKTCT-ND,296-INA823DGKTDKR-ND | INA823DGKT |
| 296-46101-2-ND,296-46101-1-ND,296-46101-6-ND | INA331IDGKR |
| 505-AD8293G80ARJZ-R7TR-ND,505-AD8293G80ARJZ-R7CT-ND,505-AD8293G80ARJZ-R7DKR-ND | AD8293G80ARJZ-R7 |
| 505-AD8293G160ARJZ-R7TR-ND,505-AD8293G160ARJZ-R7CT-ND,505-AD8293G160ARJZ-R7DKR-ND | AD8293G160ARJZ-R7 |
| INA155UA-ND | INA155UA |
| INA321EATR-ND,INA321EACT-ND,INA321EADKR-ND | INA321EA/250 |
| 296-50344-2-ND,296-50344-1-ND,296-50344-6-ND | INA826SIDRCR |
| 296-29687-5-ND | INA826AIDGK |
| 505-MAX41400ANL±ND | MAX41400ANL+ |
| 296-14586-2-ND,296-14586-1-ND,296-14586-6-ND,2156-INA321E/2K5-ND | INA321E/2K5 |
| INA321ETR-ND,INA321ECT-ND,INA321EDKR-ND,2156-INA321E/250-ND | INA321E/250 |
| AD8237ARMZ-RLTR-ND,AD8237ARMZ-RLCT-ND,AD8237ARMZ-RLDKR-ND | AD8237ARMZ-RL |
| 175-MAX41400ANL+TTR-ND,175-MAX41400ANL+TCT-ND,175-MAX41400ANL+TDKR-ND | MAX41400ANL+T |
| 505-AD8420ARMZ-R7TR-ND,505-AD8420ARMZ-R7CT-ND,505-AD8420ARMZ-R7DKR-ND | AD8420ARMZ-R7 |
| INA126U-ND | INA126U |
| 505-AD8236ARMZ-ND | AD8236ARMZ |
| AD8227ARZ-R7TR-ND,AD8227ARZ-R7CT-ND,AD8227ARZ-R7DKR-ND | AD8227ARZ-R7 |
| 505-AD8227ARZ-ND | AD8227ARZ |
| 505-AD8223ARZ-RLTR-ND,505-AD8223ARZ-RLCT-ND,505-AD8223ARZ-RLDKR-ND | AD8223ARZ-RL |
| AD8223ARZ-R7TR-ND,AD8223ARZ-R7CT-ND,AD8223ARZ-R7DKR-ND | AD8223ARZ-R7 |
| 505-AD8226ARMZ-ND | AD8226ARMZ |
| AD8226ARMZ-RLTR-ND,AD8226ARMZ-RLCT-ND,AD8226ARMZ-RLDKR-ND | AD8226ARMZ-RL |
| 505-AD8226ARZ-RLTR-ND,505-AD8226ARZ-RLCT-ND,505-AD8226ARZ-RLDKR-ND | AD8226ARZ-RL |
| 505-AD8226ARZ-ND | AD8226ARZ |
| 296-INA819IDRGRTR-ND,296-INA819IDRGRCT-ND,296-INA819IDRGRDKR-ND | INA819IDRGR |
| INA2126UA-ND | INA2126UA |
| 296-15953-2-ND,296-15953-1-ND,296-15953-6-ND,2156-INA327EA/250-ND | INA327EA/250 |
| 296-50343-2-ND,296-50343-1-ND,296-50343-6-ND | INA125UA/2K5 |
| 296-44950-2-ND,296-44950-1-ND,296-44950-6-ND | INA2132U/2K5 |
| 296-44408-5-ND | INA2126U |
| 505-AD8553ARMZ-ND | AD8553ARMZ |
| 296-53404-ND | INA821ID |
| AD8223BRZ-ND | AD8223BRZ |
| 296-53403-ND | INA819ID |
| MAX4460ESA±ND | MAX4460ESA+ |
| 296-INA125U/2K5TR-ND,296-INA125U/2K5CT-ND,296-INA125U/2K5DKR-ND | INA125U/2K5 |
| MAX4208AUA±ND | MAX4208AUA+ |
| LTC6800HMS8#TRPBFTR-ND,LTC6800HMS8#TRPBFCT-ND,LTC6800HMS8#TRPBFDKR-ND | LTC6800HMS8#TRPBF |
| AD5748ACPZ-ND | AD5748ACPZ |
| LTC6800HMS8#PBF-ND | LTC6800HMS8#PBF |
| 505-AD8277ARZ-R7TR-ND,505-AD8277ARZ-R7CT-ND,505-AD8277ARZ-R7DKR-ND | AD8277ARZ-R7 |
| 505-AD8277ARZ-ND | AD8277ARZ |
| AD8231ACPZ-RLTR-ND,AD8231ACPZ-RLCT-ND,AD8231ACPZ-RLDKR-ND | AD8231ACPZ-RL |
| 2156-INA125PA-ND,INA125PA-ND | INA125PA |
| AD8227BRZ-R7TR-ND,AD8227BRZ-R7CT-ND,AD8227BRZ-R7DKR-ND | AD8227BRZ-R7 |
| 505-AD8227BRMZ-ND | AD8227BRMZ |
| INA2126ETR-ND,INA2126ECT-ND,INA2126EDKR-ND | INA2126E/250 |
| INA121UA-ND | INA121UA |
| INA125UA-ND | INA125UA |
| 505-AD8226BRMZ-ND | AD8226BRMZ |
| 2156-INA122PA-ND,INA122PA-ND | INA122PA |
| AD623ARMZ-REEL7TR-ND,AD623ARMZ-REEL7CT-ND,AD623ARMZ-REEL7DKR-ND | AD623ARMZ-REEL7 |
| 505-AD8422ACPZ-R7TR-ND,505-AD8422ACPZ-R7CT-ND,505-AD8422ACPZ-R7DKR-ND | AD8422ACPZ-R7 |
| AD8426ACPZ-WP-ND | AD8426ACPZ-WP |
| 505-AD8421ARMZ-ND | AD8421ARMZ |
| 161-LT6370IMS8#PBF-ND | LT6370IMS8#PBF |
| AD8421ARMZ-R7TR-ND,AD8421ARMZ-R7CT-ND,AD8421ARMZ-R7DKR-ND | AD8421ARMZ-R7 |
| 505-AD8422ARZ-ND | AD8422ARZ |
| MAX4194ESA±ND | MAX4194ESA+ |
| 505-LTC6915CGN#PBF-ND | LTC6915CGN#PBF |
| INA129UA-ND | INA129UA |
| 505-AD8221ARZ-RLTR-ND,505-AD8221ARZ-RLCT-ND,505-AD8221ARZ-RLDKR-ND | AD8221ARZ-RL |
| INA129P-ND | INA129P |
| 296-INA849DGKTTR-ND,296-INA849DGKTCT-ND,296-INA849DGKTDKR-ND | INA849DGKT |
| LT1789CS8-10#PBF-ND | LT1789CS8-10#PBF |
| 505-LT6370IS8E#PBF-ND | LT6370IS8E#PBF |
| AD5750-2BCPZ-ND | AD5750-2BCPZ |
| 296-INA851RGTTTR-ND,296-INA851RGTTCT-ND,296-INA851RGTTDKR-ND | INA851RGTT |
| AD5750BCPZ-ND | AD5750BCPZ |
| 161-LT6370HS8E#PBF-ND | LT6370HS8E#PBF |
| LT1920CN8#PBF-ND | LT1920CN8#PBF |
| LT1920CS8#PBF-ND | LT1920CS8#PBF |
| 505-LT1920CS8#TRPBFTR-ND,505-LT1920CS8#TRPBFCT-ND,505-LT1920CS8#TRPBFDKR-ND | LT1920CS8#TRPBF |
| 505-LT1789IS8-1#PBF-ND | LT1789IS8-1#PBF |
| LT1167CS8-1#PBF-ND | LT1167CS8-1#PBF |
| 505-LT6370AHS8E#PBF-ND | LT6370AHS8E#PBF |
| 505-AD623BRZ-ND | AD623BRZ |
| 505-AD8422BRZ-ND | AD8422BRZ |
| INA103KP-ND | INA103KP |
| 505-LTC6373IDFM#PBF-ND | LTC6373IDFM#PBF |
| LT1167IS8-1#PBF-ND | LT1167IS8-1#PBF |
| INA103KU-ND | INA103KU |
| 505-AD8295BCPZ-R7TR-ND,505-AD8295BCPZ-R7CT-ND,505-AD8295BCPZ-R7DKR-ND | AD8295BCPZ-R7 |
| INA111AP-ND | INA111AP |
| AD8228BRMZ-R7TR-ND,AD8228BRMZ-R7CT-ND,AD8228BRMZ-R7DKR-ND | AD8228BRMZ-R7 |
| 505-AD8228BRZ-R7TR-ND,505-AD8228BRZ-R7CT-ND,505-AD8228BRZ-R7DKR-ND | AD8228BRZ-R7 |
| LT1102CN8#PBF-ND | LT1102CN8#PBF |
| LT1168AIS8#PBF-ND | LT1168AIS8#PBF |
| 505-LT1167ACN8#PBF-ND | LT1167ACN8#PBF |
| LT1101IN8#PBF-ND | LT1101IN8#PBF |
| AD8222HBCPZ-R7TR-ND,AD8222HBCPZ-R7CT-ND,AD8222HBCPZ-R7DKR-ND | AD8222HBCPZ-R7 |
| 505-AD8428ARZ-ND | AD8428ARZ |
| LT1102ACN8#PBF-ND | LT1102ACN8#PBF |
| AD620BRZ-RLTR-ND,AD620BRZ-RLCT-ND,AD620BRZ-RLDKR-ND | AD620BRZ-RL |
| AD8224HBCPZ-WP-ND | AD8224HBCPZ-WP |
| LT1167AIS8-1#PBF-ND | LT1167AIS8-1#PBF |
| INA2141U-ND | INA2141U |
| 505-LT1101ISW#PBF-ND | LT1101ISW#PBF |
| 505-AMP02FSZ-ND | AMP02FSZ |
| PGA202KP-ND | PGA202KP |
| AD621ANZ-ND | AD621ANZ |
| INA110KP-ND | INA110KP |
| AD621BNZ-ND | AD621BNZ |
| AMP01GSZ-ND | AMP01GSZ |
| AD625KNZ-ND | AD625KNZ |
| MCP6N11-005E/SN-ND | MCP6N11-005E/SN |
| 296-46100-2-ND,296-46100-1-ND,296-46100-6-ND | INA331AIDGKR |
| MCP6N16-001E/MS-ND | MCP6N16-001E/MS |
| MCP6N16-001E/MF-ND | MCP6N16-001E/MF |
| 296-32100-2-ND,296-32100-1-ND,296-32100-6-ND | INA2332AIPWT |
| 296-38962-ND | INA827AIDGK |
| INA155EATR-ND,INA155EACT-ND,INA155EADKR-ND | INA155EA/250 |
| 296-12203-2-ND,296-12203-1-ND,296-12203-6-ND | INA331IDGKT |
| INA156EATR-ND,INA156EACT-ND,INA156EADKR-ND,2156-INA156EA/250-ND | INA156EA/250 |
| 296-17647-2-ND,296-17647-1-ND,296-17647-6-ND | INA2331AIPWT |
| 296-49650-2-ND,296-49650-1-ND,296-49650-6-ND | INA826SIDRCT |
| INA126EATR-ND,INA126EACT-ND,INA126EADKR-ND | INA126EA/250 |
| 296-41261-2-ND,296-41261-1-ND,296-41261-6-ND | INA2126UA/2K5 |
| 296-INA126E/2K5TR-ND,296-INA126E/2K5CT-ND,296-INA126E/2K5DKR-ND | INA126E/2K5 |
| 505-AD8420ARMZ-ND | AD8420ARMZ |
| INA126ETR-ND,INA126ECT-ND,INA126EDKR-ND | INA126E/250 |
| INA2321EATR-ND,INA2321EACT-ND,INA2321EADKR-ND | INA2321EA/250 |
| 505-AD8293G160BRJZ-R7TR-ND,505-AD8293G160BRJZ-R7CT-ND,505-AD8293G160BRJZ-R7DKR-ND | AD8293G160BRJZ-R7 |
| INA2126EATR-ND,INA2126EACT-ND,INA2126EADKR-ND | INA2126EA/250 |
| AD8223ARMZ-R7TR-ND,AD8223ARMZ-R7CT-ND,AD8223ARMZ-R7DKR-ND | AD8223ARMZ-R7 |
| 505-AD8223ARMZ-ND | AD8223ARMZ |
| MAX4209HAUA±ND | MAX4209HAUA+ |
| MAX4462HETT+TTR-ND,MAX4462HETT+TCT-ND,MAX4462HETT+TDKR-ND | MAX4462HETT+T |
| 296-INA821IDRGTTR-ND,296-INA821IDRGTCT-ND,296-INA821IDRGTDKR-ND | INA821IDRGT |
| 296-INA819IDRGTTR-ND,296-INA819IDRGTCT-ND,296-INA819IDRGTDKR-ND | INA819IDRGT |
| 296-13454-2-ND,296-13454-1-ND,296-13454-6-ND | INA338AIDGST |
| AD8223BRMZ-ND | AD8223BRMZ |
| INA2132U-ND | INA2132U |
| 505-AD8227BRMZ-R7TR-ND,505-AD8227BRMZ-R7CT-ND,505-AD8227BRMZ-R7DKR-ND | AD8227BRMZ-R7 |
| 505-AD8227BRZ-ND | AD8227BRZ |
| 505-AD8231ACPZ-WP-ND | AD8231ACPZ-WP |
| 505-AD8226BRZ-R7TR-ND,505-AD8226BRZ-R7CT-ND,505-AD8226BRZ-R7DKR-ND | AD8226BRZ-R7 |
| MAX4461TESA±ND | MAX4461TESA+ |
| 505-AD5749ACPZ-ND | AD5749ACPZ |
| MAX4462HESA±ND | MAX4462HESA+ |
| 175-MAX4460EUT+TTR-ND,175-MAX4460EUT+TCT-ND,175-MAX4460EUT+TDKR-ND | MAX4460EUT+T |
| MAX4196ESA±ND | MAX4196ESA+ |
| 505-AD5750-1BCPZ-ND | AD5750-1BCPZ |
| AD5750ACPZ-ND | AD5750ACPZ |
| 505-AD5750-1ACPZ-ND | AD5750-1ACPZ |
| MAX4197ESA±ND | MAX4197ESA+ |
| MAX4195ESA±ND | MAX4195ESA+ |
| AD8295ACPZ-WP-ND | AD8295ACPZ-WP |
| AD8228ARMZ-R7TR-ND,AD8228ARMZ-R7CT-ND,AD8228ARMZ-R7DKR-ND | AD8228ARMZ-R7 |
| 505-AD8228ARZ-ND | AD8228ARZ |
| 161-LT6370HDD#PBF-ND | LT6370HDD#PBF |
| 161-LT6370HMS8#PBF-ND | LT6370HMS8#PBF |
| AD5751ACPZ-ND | AD5751ACPZ |
| AD8426BCPZ-WP-ND | AD8426BCPZ-WP |
| 505-LT6370AIS8E#PBF-ND | LT6370AIS8E#PBF |
| 161-LT6372IMSE-0.2#PBF-ND | LT6372IMSE-0.2#PBF |
| 161-LT6372IUDC-0.2#PBF-ND | LT6372IUDC-0.2#PBF |
| 505-LT6372IMSE-1#PBF-ND | LT6372IMSE-1#PBF |
| LT1789IS8-10#PBF-ND | LT1789IS8-10#PBF |
| AD8222HACPZ-R7TR-ND,AD8222HACPZ-R7CT-ND,AD8222HACPZ-R7DKR-ND | AD8222HACPZ-R7 |
| LT1168IS8#PBF-ND | LT1168IS8#PBF |
| 505-LT6372HMSE-0.2#PBF-ND | LT6372HMSE-0.2#PBF |
| 505-LT6372HMSE-1#PBF-ND | LT6372HMSE-1#PBF |
| 2156-INA115AU-ND,INA115AU-ND | INA115AU |
| AD8224HACPZ-R7TR-ND,AD8224HACPZ-R7CT-ND,AD8224HACPZ-R7DKR-ND | AD8224HACPZ-R7 |
| AD8295BCPZ-WP-ND | AD8295BCPZ-WP |
| 505-AD8221TRMZ-EP-R7TR-ND,505-AD8221TRMZ-EP-R7CT-ND,505-AD8221TRMZ-EP-R7DKR-ND | AD8221TRMZ-EP-R7 |
| AD8228BRMZ-ND | AD8228BRMZ |
| AD5751BCPZ-ND | AD5751BCPZ |
| AD8231TCPZ-EP-R7TR-ND,AD8231TCPZ-EP-R7CT-ND,AD8231TCPZ-EP-R7DKR-ND | AD8231TCPZ-EP-R7 |
| 2156-AD627BNZ-ND,AD627BNZ-ND | AD627BNZ |
| LT1168ACN8#PBF-ND | LT1168ACN8#PBF |
| 505-LT1168ACS8#PBF-ND | LT1168ACS8#PBF |
| 296-PGA205AU/1KTR-ND,296-PGA205AU/1KCT-ND,296-PGA205AU/1KDKR-ND | PGA205AU/1K |
| LT1167ACS8-1#PBF-ND | LT1167ACS8-1#PBF |
| 161-LT1102IN8#PBF-ND | LT1102IN8#PBF |
| 505-AD8224BCPZ-WP-ND | AD8224BCPZ-WP |
| LT1101ACN8#PBF-ND | LT1101ACN8#PBF |
| AD8222BCPZ-WP-ND | AD8222BCPZ-WP |
| LT1167AIN8#PBF-ND | LT1167AIN8#PBF |
| INA118PB-ND | INA118PB |
| AMP04ESZ-R7TR-ND,AMP04ESZ-R7CT-ND,AMP04ESZ-R7DKR-ND | AMP04ESZ-R7 |
| 505-AD8236ARMZ-RLTR-ND,505-AD8236ARMZ-RLCT-ND,505-AD8236ARMZ-RLDKR-ND | AD8236ARMZ-RL |
| 505-AD8293G80BRJZ-R7TR-ND,505-AD8293G80BRJZ-R7CT-ND,505-AD8293G80BRJZ-R7DKR-ND | AD8293G80BRJZ-R7 |
| MAX4462TETT+TR-ND,MAX4462TETT+CT-ND,MAX4462TETT+DKR-ND | MAX4462TETT+T |
| AD8223BRMZ-R7TR-ND,AD8223BRMZ-R7CT-ND,AD8223BRMZ-R7DKR-ND | AD8223BRMZ-R7 |
| LTC6800HDD#PBF-ND | LTC6800HDD#PBF |
| AD5750-1BCPZ-REEL7TR-ND,AD5750-1BCPZ-REEL7CT-ND,AD5750-1BCPZ-REEL7DKR-ND | AD5750-1BCPZ-REEL7 |
| 161-LT6372IUDC-1#PBF-ND | LT6372IUDC-1#PBF |
| AD8222ACPZ-RLTR-ND,AD8222ACPZ-RLCT-ND,AD8222ACPZ-RLDKR-ND | AD8222ACPZ-RL |
| AD8422BRZ-R7TR-ND,AD8422BRZ-R7CT-ND,AD8422BRZ-R7DKR-ND | AD8422BRZ-R7 |
| 161-LT6372HUDC-1#PBF-ND | LT6372HUDC-1#PBF |
| 161-LT6372HUDC-0.2#PBF-ND | LT6372HUDC-0.2#PBF |
| AD8251ARMZ-RLTR-ND,AD8251ARMZ-RLCT-ND,AD8251ARMZ-RLDKR-ND | AD8251ARMZ-RL |
| 505-AD8250ARMZ-RLTR-ND,505-AD8250ARMZ-RLCT-ND,505-AD8250ARMZ-RLDKR-ND | AD8250ARMZ-RL |
| AD621ARZ-RLTR-ND,AD621ARZ-RLCT-ND,AD621ARZ-RLDKR-ND | AD621ARZ-RL |
| 505-AD524ARZ-16-REEL7TR-ND,505-AD524ARZ-16-REEL7CT-ND,505-AD524ARZ-16-REEL7DKR-ND | AD524ARZ-16-REEL7 |
| 2156-PGA206PA-ND,296-33537-5-ND | PGA206PA |
| 2156-AD625ADZ-ND,AD625ADZ-ND | AD625ADZ |
| 505-AD8229HRZ-ND | AD8229HRZ |
| MCP6N11T-005E/MNYTR-ND,MCP6N11T-005E/MNYCT-ND,MCP6N11T-005E/MNYDKR-ND | MCP6N11T-005E/MNY |
| 296-INA155EA/2K5TR-ND,296-INA155EA/2K5CT-ND,296-INA155EA/2K5DKR-ND | INA155EA/2K5 |
| INA155ETR-ND,INA155ECT-ND,INA155EDKR-ND | INA155E/250 |
| 175-MAX4460ETT+TTR-ND,175-MAX4460ETT+TCT-ND,175-MAX4460ETT+TDKR-ND | MAX4460ETT+T |
| 175-MAX4462HEUT+TTR-ND,175-MAX4462HEUT+TCT-ND,175-MAX4462HEUT+TDKR-ND | MAX4462HEUT+T |
| 175-MAX4209HAUA+TTR-ND,175-MAX4209HAUA+TCT-ND,175-MAX4209HAUA+TDKR-ND | MAX4209HAUA+T |
| 505-LT6370IDD#TRPBFTR-ND,505-LT6370IDD#TRPBFCT-ND,505-LT6370IDD#TRPBFDKR-ND | LT6370IDD#TRPBF |
| 505-AD8277BRZ-R7TR-ND,505-AD8277BRZ-R7CT-ND,505-AD8277BRZ-R7DKR-ND | AD8277BRZ-R7 |
| 175-MAX4195ESA+TTR-ND,175-MAX4195ESA+TCT-ND,175-MAX4195ESA+TDKR-ND | MAX4195ESA+T |
| 505-LT6370IS8E#TRPBFTR-ND,505-LT6370IS8E#TRPBFCT-ND,505-LT6370IS8E#TRPBFDKR-ND | LT6370IS8E#TRPBF |
| 505-LT6370HDD#TRPBFTR-ND,505-LT6370HDD#TRPBFCT-ND,505-LT6370HDD#TRPBFDKR-ND | LT6370HDD#TRPBF |
| 505-LT6370HMS8#TRPBFTR-ND,505-LT6370HMS8#TRPBFCT-ND,505-LT6370HMS8#TRPBFDKR-ND | LT6370HMS8#TRPBF |
| 505-LTC6373SDFM#PBF-ND | LTC6373SDFM#PBF |
| 505-LT1168AIN8#PBF-ND | LT1168AIN8#PBF |
| 2156-MAX4461UEUT-ND | MAX4461UEUT |
| 2156-MAX4462HEUT-ND | MAX4462HEUT |
| MCP6N11T-002E/MNYTR-ND,MCP6N11T-002E/MNYCT-ND,MCP6N11T-002E/MNYDKR-ND | MCP6N11T-002E/MNY |
| 2156-MAX4461TEUT-ND | MAX4461TEUT |
| INA155U/2K5-ND,2156-INA155U/2K5-ND | INA155U/2K5 |
| 2156-MAX4461UEUT+T-ND | MAX4461UEUT+T |
| 296-INA322EA/2K5TR-ND,296-INA322EA/2K5CT-ND,296-INA322EA/2K5DKR-ND,2156-INA322EA/2K5-ND | INA322EA/2K5 |
| 296-INA156EA/2K5TR-ND,296-INA156EA/2K5CT-ND,296-INA156EA/2K5DKR-ND,2156-INA156EA/2K5-ND | INA156EA/2K5 |
| 2156-OP06FZ-ND | OP06FZ |
| 505-AD8231WACPZ-RLTR-ND | AD8231WACPZ-RL |
| 2156-ADOP37FQ-ND | ADOP37FQ |
| AD5750ACPZ-REEL7TR-ND | AD5750ACPZ-REEL7 |
| 2156-OP05BICJ-ND | OP05BICJ |
| 2156-OP06GZ-ND | OP06GZ |
| 2156-INA115AU-1-ND | INA115AU-1 |
| INA327EA/2K5TR-ND,INA327EA/2K5CT-ND,INA327EA/2K5DKR-ND,2156-INA327EA/2K5-ND | INA327EA/2K5 |
| AD8220WARMZ-RLTR-ND | AD8220WARMZ-RL |
| 2156-OP05EP-ND | OP05EP |
| 2156-OP06EZ-ND | OP06EZ |
| 505-LT1920IS8#TRPBFTR-ND | LT1920IS8#TRPBF |
| 2156-INA141UA-ND | INA141UA |
| INA166UATR-ND,2156-INA166UA/2K5-ND | INA166UA/2K5 |
| INA115AU/1K-ND,2156-INA115AU/1K-ND | INA115AU/1K |
| 505-AD8422ARMZ-RLTR-ND,505-AD8422ARMZ-RLCT-ND | AD8422ARMZ-RL |
| INA2141UA/1K-ND,2156-INA2141UA/1K-ND | INA2141UA/1K |
| 2156-OP05Z-ND | OP05Z |
| 505-LT1168ACS8#TRPBFTR-ND | LT1168ACS8#TRPBF |
| 505-LT1101SW#TRPBFTR-ND | LT1101SW#TRPBF |
| 2156-INA2141UA-ND | INA2141UA |
| INA101KU/1K-ND,2156-INA101KU/1K-ND | INA101KU/1K |
| 505-LT1789CS8-10#TRPBFTR-ND,505-LT1789CS8-10#TRPBFCT-ND,505-LT1789CS8-10#TRPBFDKR-ND | LT1789CS8-10#TRPBF |
| 505-LT1167AIS8#TRPBFTR-ND | LT1167AIS8#TRPBF |
| 505-AD8225ARZ-R7TR-ND,505-AD8225ARZ-R7CT-ND | AD8225ARZ-R7 |
| 2156-INA111BU-296-ND | INA111BU |
| 505-AD623BRZ-RLTR-ND,505-AD623BRZ-RLCT-ND | AD623BRZ-RL |
| 2156-OP05Z/883C-ND | OP05Z/883C |
| 2156-PGA205AU-ND | PGA205AU |
| 2156-OP06CZ/883C-ND | OP06CZ/883C |
| 2156-PGA204AP-ND,PGA204AP-ND | PGA204AP |
| 505-AD8221BRZ-RLTR-ND,505-AD8221BRZ-RLCT-ND | AD8221BRZ-RL |
| 2156-PGA207UA-2-ND | PGA207UA-2 |
| 2156-OP06BJ-ND | OP06BJ |
| 2156-PGA205BP-ND,PGA205BP-ND | PGA205BP |
| 2156-AD625AE-ND | AD625AE |
| 505-AD8421TRMZ-EP-R7TR-ND,505-AD8421TRMZ-EP-R7CT-ND | AD8421TRMZ-EP-R7 |
| 2156-PGA205AP-ND,PGA205AP-ND | PGA205AP |
| PGA207UA/1K-ND,2156-PGA207UA/1K-ND | PGA207UA/1K |
| 2156-PGA204BP-ND,PGA204BP-ND | PGA204BP |
| 2156-AD624AD/±ND | AD624AD/+ |
| 2156-OP06AJ-ND | OP06AJ |
| 2156-INA101AG-ND,INA101AG-ND | INA101AG |
| 2156-AMP01EX-ND,AMP01EX-ND | AMP01EX |
| 2156-AD524CE-ND | AD524CE |
| 2156-INA101SM-ND,296-41554-5-ND | INA101SM |
| 2156-AMP01BX-ND,AMP01BX-ND | AMP01BX |
| 2156-AD625BDZ-ND,AD625BDZ-ND | AD625BDZ |
| 2156-AD624SD-505-ND | AD624SD |
| 2156-AD625SD-ND,AD625SD-ND | AD625SD |
| 2156-AD524BE-ND,AD524BE-ND | AD524BE |