Introduction
Precision sensors are essential for accurately measuring physical phenomena in a wide range of applications. As the variety and quantity of precision-measurement applications increases, engineers are called upon to design systems that can sense ever-smaller amplitude signals in the presence of interferers, while maintaining signal fidelity.
Achieving this requires more than just selecting the right sensor; it involves comprehensive design of the entire signal path—from the sensor to the data converter that digitizes the analog measurements. One critical element in this signal chain is the amplifier circuit, which plays a pivotal role in amplifying the signal while maintaining its fidelity.
This series of articles explore the process of selecting the right precision amplifier topology for sensor applications, focusing on key types such as operational amplifiers, difference amplifiers, current-sense amplifiers, instrumentation amplifiers, and fully differential amplifiers.
This article specifically covers the Single-Ended Operational Amplifier Topology. For information on other topologies, please refer to the linked articles below.
When choosing an amplifier topology, the first step is to check whether the sensor output signal is single-ended or differential. Some topologies work with single-ended inputs, while others are designed for differential inputs. The choice also depends on whether you need the amplifier to provide a single-ended or differential output.
Single-Ended Operational Amplifier Topology
The operational amplifier (or ‘op amp’ in common parlance) is an extremely versatile amplifier that can be configured for many different operations, hence the name. For circuits with single-ended input and output signals, a basic op-amp circuit with feedback from a pair of resistors is commonly used.
When using a single-ended op amp circuit to amplify a high precision signal, the choice of which topology to use usually comes down to deciding between a non-inverting amplifier and an inverting amplifier (Figure 1). Both circuits utilize a single feedback resistor and single gain resistor.
A simple single-ended input, single-ended output application is shown in Figure 2.
Analog Devices’ TMP35 temperature sensor outputs a voltage that is proportional to temperature at a sensitivity of 10 mV/°C. That signal is then connected to a single-ended, non-inverting amplifier circuit, which has a transfer function of VOUT = G × VIN, where G is the closed-loop gain of the circuit which is equal to 1 + (R2/R1). To sense a temperature range of, for example, 0°C to 50°C, the sensor’s full-scale output range would be 10 mV/°C × 50°C = 500 mV. If the sensor output were to drive, for example, an analog-to-digital converter (ADC) with a 5 V full-scale input range, the signal would need to be amplified by a gain of 10 V/V in order to utilize the ADC’s full input dynamic range. This is achieved with the non-inverting operational amplifier circuit, where G = 1 + (9 kΩ/1 kΩ) = 10 V/V.
Common-Mode Rejection in Amplifier Topology Selection
When selecting an amplifier topology, a crucial factor to assess is the amplifier circuit’s capability to effectively reject common-mode input voltage—preventing the signal voltages that are common to both inputs from manifestation at the output—while amplifying the differential input voltage.
The common-mode rejection ratio (CMRR) serves as a quantitative measure of an amplifier circuit’s proficiency in this regard. The higher the CMRR, the less error at the output. CMRR is normally represented as the ratio between two gains: the gain of the differential voltage (ADIFF) relative to the gain of the common-mode voltage (ACM) with units in dB.
![]()
An ideal op amp creates a “virtual short” between its inputs, meaning the voltage at the positive input (+IN) is mirrored at the negative input (–IN). This common voltage is called the common-mode voltage.
Modern op amps often have high common-mode rejection ratio (CMRR) values, ranging from 120 dB to 140 dB or more, which helps minimize common-mode errors and ensures accurate output. For instance, with a CMRR of 140 dB, then only 0.00001% (or 0.1 ppm) of the common-mode voltage at the op amp inputs will show up on the output (VOUT).
For a low voltage op amp with a maximum input range of 5 V, the maximum common-mode error at that output would only be 0.5 µV. But using an op amp with a high input-voltage range—for example 50 V—would result in an error of 5 µV on the output. Whether this is an issue or not depends on the system design requirements. If the common-mode error exceeds the acceptable limit for a specific system design, it would be necessary to use a circuit that minimizes that error contribution.
In a non-inverting amplifier, the inputs (+IN and –IN) are equal to the signal voltage (VIN), so an increase in the input signal also increases the common-mode voltage and the associated error at the output. On the other hand, an inverting amplifier ties the +IN input (and consequently –IN) to ground, making the input common-mode voltage 0 V. This setup eliminates common-mode voltage at the input and prevents common-mode errors at the output.
Conclusion
Selecting the right amplifier topology is crucial for designing precise signal chains, especially when working with highly sensitive sensors. Single-ended operational amplifiers, like non-inverting and inverting amplifiers, are flexible solutions that can amplify sensor signals without compromising accuracy. One key factor to consider is the common-mode rejection ratio (CMRR), which helps reduce errors and maintain signal integrity.
Picking the right amplifier can significantly improve the overall performance and accuracy of your system, making it a vital component in the design of high-precision circuits. For additional details on other amplifier types, like difference amplifiers and instrumentation amplifiers, please refer to the linked articles.
Related Articles:
The Role of Difference Amplifiers in Precision Sensor Systems
Current-Sense Amplifiers and Their Distinction from Difference Amplifiers
Applicable Part Numbers
| DigiKey Part Number | Manufacturer Part Number |
|---|---|
| 497-LMC7101ILTTR-ND,497-LMC7101ILTCT-ND,497-LMC7101ILTDKR-ND | LMC7101ILT |
| 296-38954-2-ND,296-38954-1-ND,296-38954-6-ND | INA210AIDCKR |
| 296-38956-2-ND,296-38956-1-ND,296-38956-6-ND | INA214AIDCKR |
| 296-26072-2-ND,296-26072-1-ND,296-26072-6-ND | INA213AIDCKR |
| MC33072DR2GOSTR-ND,MC33072DR2GOSCT-ND,MC33072DR2GOSDKR-ND | MC33072DR2G |
| MC34072DR2GOSTR-ND,MC34072DR2GOSCT-ND,MC34072DR2GOSDKR-ND | MC34072DR2G |
| 296-48553-2-ND,296-48553-1-ND,296-48553-6-ND | INA214CIDCKR |
| 296-23586-2-ND,296-23586-1-ND,296-23586-6-ND,2156-INA212AIDCKT-ND | INA212AIDCKT |
| MC34072VDR2GOSTR-ND,MC34072VDR2GOSCT-ND,MC34072VDR2GOSDKR-ND | MC34072VDR2G |
| 296-23422-2-ND,296-23422-1-ND,296-23422-6-ND | INA214AIDCKT |
| MC34072ADR2GOSTR-ND,MC34072ADR2GOSCT-ND,MC34072ADR2GOSDKR-ND | MC34072ADR2G |
| MC34074ADR2GOSTR-ND,MC34074ADR2GOSCT-ND,MC34074ADR2GOSDKR-ND | MC34074ADR2G |
| MC33074DR2GOSTR-ND,MC33074DR2GOSCT-ND,MC33074DR2GOSDKR-ND | MC33074DR2G |
| 296-39130-2-ND,296-39130-1-ND,296-39130-6-ND | OPA376AIDBVR |
| 296-35916-2-ND,296-35916-1-ND,296-35916-6-ND | OPA376AIDCKR |
| MC33074ADTBR2GOSTR-ND,MC33074ADTBR2GOSCT-ND,MC33074ADTBR2GOSDKR-ND | MC33074ADTBR2G |
| 296-36701-2-ND,296-36701-1-ND,296-36701-6-ND | OPA376AQDBVRQ1 |
| 296-22191-2-ND,296-22191-1-ND,296-22191-6-ND | OPA376AIDCKT |
| 296-21982-2-ND,296-21982-1-ND,296-21982-6-ND | OPA376AIDBVT |
| 296-22564-2-ND,296-22564-1-ND,296-22564-6-ND | OPA2376AIDR |
| 296-22630-2-ND,296-22630-1-ND,296-22630-6-ND | OPA2376AIDGKR |
| 296-39119-2-ND,296-39119-1-ND,296-39119-6-ND | OPA2376AIYZDR |
| 296-INA310B3IDGKRTR-ND,296-INA310B3IDGKRCT-ND,296-INA310B3IDGKRDKR-ND | INA310B3IDGKR |
| 296-26268-2-ND,296-26268-1-ND,296-26268-6-ND | OPA277UA/2K5 |
| 296-22565-2-ND,296-22565-1-ND,296-22565-6-ND | OPA4376AIPWR |
| OPA277UA-ND | OPA277UA |
| MAX4238ASA+TR-ND,MAX4238ASA+CT-ND,MAX4238ASA+DKR-ND | MAX4238ASA+T |
| MAX4238AUT+TTR-ND,MAX4238AUT+TCT-ND,MAX4238AUT+TDKR-ND | MAX4238AUT+T |
| AD8274ARMZ-R7TR-ND,AD8274ARMZ-R7CT-ND,AD8274ARMZ-R7DKR-ND | AD8274ARMZ-R7 |
| AD8273ARZ-ND | AD8273ARZ |
| 296-OPA3S328YBJRTR-ND,296-OPA3S328YBJRCT-ND,296-OPA3S328YBJRDKR-ND | OPA3S328YBJR |
| OP221GSZ-REEL7TR-ND,OP221GSZ-REEL7CT-ND,OP221GSZ-REEL7DKR-ND | OP221GSZ-REEL7 |
| 296-OPA2828IDGNRTR-ND,296-OPA2828IDGNRCT-ND,296-OPA2828IDGNRDKR-ND | OPA2828IDGNR |
| 296-OPA2828IDGNTTR-ND,296-OPA2828IDGNTCT-ND,296-OPA2828IDGNTDKR-ND | OPA2828IDGNT |
| 5503-LMV321B-TR-ND,5503-LMV321B-TRCT-ND,5503-LMV321B-TRDKR-ND | LMV321B-TR |
| 497-1561-2-ND,497-1561-1-ND,497-1561-6-ND | LM2904DT |
| 5503-LM321AW-S5TR-ND,5503-LM321AW-S5TRCT-ND,5503-LM321AW-S5TRDKR-ND | LM321AW-S5TR |
| 5503-LM358A-SRTR-ND,5503-LM358A-SRCT-ND,5503-LM358A-SRDKR-ND | LM358A-SR |
| 497-4046-2-ND,497-4046-1-ND,497-4046-6-ND | LM2904PT |
| 5503-LM324A-SRTR-ND,5503-LM324A-SRCT-ND,5503-LM324A-SRDKR-ND | LM324A-SR |
| 497-13049-2-ND,497-13049-1-ND,497-13049-6-ND | LM2904AYPT |
| 296-INA500AIDBVRTR-ND,296-INA500AIDBVRCT-ND,296-INA500AIDBVRDKR-ND | INA500AIDBVR |
| 296-INA500AIDCKRTR-ND,296-INA500AIDCKRCT-ND,296-INA500AIDCKRDKR-ND | INA500AIDCKR |
| 5503-TPH2502-SRTR-ND,5503-TPH2502-SRCT-ND,5503-TPH2502-SRDKR-ND | TPH2502-SR |
| 497-12965-2-ND,497-12965-1-ND,497-12965-6-ND | LM2904Q2T |
| 497-7816-2-ND,497-7816-1-ND,497-7816-6-ND | LM2904ST |
| 296-INA351CDSIDSGRTR-ND,296-INA351CDSIDSGRCT-ND,296-INA351CDSIDSGRDKR-ND | INA351CDSIDSGR |
| 296-40124-2-ND,296-40124-1-ND,296-40124-6-ND | INA210BIDCKR |
| 296-40131-2-ND,296-40131-1-ND,296-40131-6-ND | INA214BIDCKR |
| 296-OPA323IDCKRTR-ND,296-OPA323IDCKRCT-ND,296-OPA323IDCKRDKR-ND | OPA323IDCKR |
| 296-TLV9361QDBVRQ1TR-ND,296-TLV9361QDBVRQ1CT-ND,296-TLV9361QDBVRQ1DKR-ND | TLV9361QDBVRQ1 |
| 296-44266-2-ND,296-44266-1-ND,296-44266-6-ND | INA213BQDCKRQ1 |
| 296-TLV365QDBVRQ1TR-ND,296-TLV365QDBVRQ1CT-ND,296-TLV365QDBVRQ1DKR-ND | TLV365QDBVRQ1 |
| 296-24493-2-ND,296-24493-1-ND,296-24493-6-ND | INA213AQDCKRQ1 |
| 296-40129-2-ND,296-40129-1-ND,296-40129-6-ND | INA213BIDCKR |
| 296-48548-2-ND,296-48548-1-ND,296-48548-6-ND | INA210CIDCKR |
| 296-41418-2-ND,296-41418-1-ND,296-41418-6-ND,2156-INA212AIDCKR-ND | INA212AIDCKR |
| 296-27745-2-ND,296-27745-1-ND,296-27745-6-ND | INA214AQDCKRQ1 |
| MC33072ADR2GOSTR-ND,MC33072ADR2GOSCT-ND,MC33072ADR2GOSDKR-ND,2832-MC33072ADR2G-ND | MC33072ADR2G |
| 296-46095-2-ND,296-46095-1-ND,296-46095-6-ND | INA215AIDCKR |
| 296-48294-2-ND,296-48294-1-ND,296-48294-6-ND | INA213CIDCKR |
| NCV33072DR2GOSTR-ND,NCV33072DR2GOSCT-ND,NCV33072DR2GOSDKR-ND | NCV33072DR2G |
| 296-51141-2-ND,296-51141-1-ND,296-51141-6-ND | INA210CQDCKRQ1 |
| 150-MCP60711T-E/OTTR-ND,150-MCP60711T-E/OTCT-ND,150-MCP60711T-E/OTDKR-ND | MCP60711T-E/OT |
| 296-41417-2-ND,296-41417-1-ND,296-41417-6-ND | INA211AIDCKR |
| MC34071DR2GOSTR-ND,MC34071DR2GOSCT-ND,MC34071DR2GOSDKR-ND | MC34071DR2G |
| 5503-TPA191A4-SC6RTR-ND,5503-TPA191A4-SC6RCT-ND,5503-TPA191A4-SC6RDKR-ND | TPA191A4-SC6R |
| MC34074DR2GOSTR-ND,MC34074DR2GOSCT-ND,MC34074DR2GOSDKR-ND | MC34074DR2G |
| MC33071DR2GOSTR-ND,MC33071DR2GOSCT-ND | MC33071DR2G |
| MC33074ADR2GOSTR-ND,MC33074ADR2GOSCT-ND,MC33074ADR2GOSDKR-ND | MC33074ADR2G |
| NCV33072ADR2GOSTR-ND,NCV33072ADR2GOSCT-ND,NCV33072ADR2GOSDKR-ND | NCV33072ADR2G |
| 5503-TPA191A2-SC6RTR-ND,5503-TPA191A2-SC6RCT-ND,5503-TPA191A2-SC6RDKR-ND | TPA191A2-SC6R |
| 296-23420-2-ND,296-23420-1-ND,296-23420-6-ND | INA210AIDCKT |
| 296-38955-2-ND,296-38955-1-ND,296-38955-6-ND | INA213BIDCKT |
| 296-23421-2-ND,296-23421-1-ND,296-23421-6-ND | INA213AIDCKT |
| 296-TLV9161QDBVRQ1TR-ND,296-TLV9161QDBVRQ1CT-ND,296-TLV9161QDBVRQ1DKR-ND | TLV9161QDBVRQ1 |
| 296-OPA2323IDRTR-ND,296-OPA2323IDRCT-ND,296-OPA2323IDRDKR-ND | OPA2323IDR |
| 296-41368-2-ND,296-41368-1-ND,296-41368-6-ND | OPA376AIDR |
| 296-TLV2387DRTR-ND,296-TLV2387DRCT-ND,296-TLV2387DRDKR-ND | TLV2387DR |
| 296-TLV2387DGKRTR-ND,296-TLV2387DGKRCT-ND,296-TLV2387DGKRDKR-ND | TLV2387DGKR |
| MC33074DTBR2GOSTR-ND,MC33074DTBR2GOSCT-ND,MC33074DTBR2GOSDKR-ND | MC33074DTBR2G |
| MC34074VDR2GOSTR-ND,MC34074VDR2GOSCT-ND,MC34074VDR2GOSDKR-ND | MC34074VDR2G |
| 296-22190-5-ND | OPA376AID |
| MC33071ADR2GOSTR-ND,MC33071ADR2GOSCT-ND,MC33071ADR2GOSDKR-ND | MC33071ADR2G |
| 296-OPA992QDBVRQ1TR-ND,296-OPA992QDBVRQ1CT-ND,296-OPA992QDBVRQ1DKR-ND | OPA992QDBVRQ1 |
| 296-OPA2994IDGKRTR-ND,296-OPA2994IDGKRCT-ND,296-OPA2994IDGKRDKR-ND | OPA2994IDGKR |
| 488-NCS21671SQ025T2GTR-ND,488-NCS21671SQ025T2GCT-ND,488-NCS21671SQ025T2GDKR-ND | NCS21671SQ025T2G |
| 296-OPA4323IPWRTR-ND,296-OPA4323IPWRCT-ND,296-OPA4323IPWRDKR-ND | OPA4323IPWR |
| 296-TLV4387PWRTR-ND,296-TLV4387PWRCT-ND,296-TLV4387PWRDKR-ND | TLV4387PWR |
| 296-INA310B2IDGKRTR-ND,296-INA310B2IDGKRCT-ND,296-INA310B2IDGKRDKR-ND | INA310B2IDGKR |
| 296-INA310B1IDGKRTR-ND,296-INA310B1IDGKRCT-ND,296-INA310B1IDGKRDKR-ND | INA310B1IDGKR |
| 296-44296-2-ND,296-44296-1-ND,296-44296-6-ND | OPA2376QDGKRQ1 |
| 296-43771-2-ND,296-43771-1-ND,296-43771-6-ND | OPA2376AQDRQ1 |
| 296-26264-2-ND,296-26264-1-ND,296-26264-6-ND | OPA2376AIDGKT |
| 296-23919-2-ND,296-23919-1-ND,296-23919-6-ND | OPA2376AIYZDT |
| 296-26263-5-ND | OPA2376AID |
| 296-OPA328DBVRTR-ND,296-OPA328DBVRCT-ND,296-OPA328DBVRDKR-ND | OPA328DBVR |
| 296-INA310A3IDGKRTR-ND,296-INA310A3IDGKRCT-ND,296-INA310A3IDGKRDKR-ND | INA310A3IDGKR |
| 296-INA310A2IDGKRTR-ND,296-INA310A2IDGKRCT-ND,296-INA310A2IDGKRDKR-ND | INA310A2IDGKR |
| 296-INA310A1IDGKRTR-ND,296-INA310A1IDGKRCT-ND,296-INA310A1IDGKRDKR-ND | INA310A1IDGKR |
| 497-19618-ND | LM2904D |
| 296-INA241A1IDRTR-ND,296-INA241A1IDRCT-ND,296-INA241A1IDRDKR-ND | INA241A1IDR |
| 296-INA241A4IDRTR-ND,296-INA241A4IDRCT-ND,296-INA241A4IDRDKR-ND | INA241A4IDR |
| 296-INA241A2IDRTR-ND,296-INA241A2IDRCT-ND,296-INA241A2IDRDKR-ND | INA241A2IDR |
| 296-INA296A3IDGKRTR-ND,296-INA296A3IDGKRCT-ND,296-INA296A3IDGKRDKR-ND | INA296A3IDGKR |
| 296-INA296A4IDRTR-ND,296-INA296A4IDRCT-ND,296-INA296A4IDRDKR-ND | INA296A4IDR |
| 296-INA241A1IDGKRTR-ND,296-INA241A1IDGKRCT-ND,296-INA241A1IDGKRDKR-ND | INA241A1IDGKR |
| 296-INA296A4IDGKRTR-ND,296-INA296A4IDGKRCT-ND,296-INA296A4IDGKRDKR-ND | INA296A4IDGKR |
| 296-INA241A3IDRTR-ND,296-INA241A3IDRCT-ND,296-INA241A3IDRDKR-ND | INA241A3IDR |
| 296-INA296A2IDGKRTR-ND,296-INA296A2IDGKRCT-ND,296-INA296A2IDGKRDKR-ND | INA296A2IDGKR |
| 296-OPA2328DRTR-ND,296-OPA2328DRCT-ND,296-OPA2328DRDKR-ND | OPA2328DR |
| 296-OPA2387DRTR-ND,296-OPA2387DRCT-ND,296-OPA2387DRDKR-ND | OPA2387DR |
| 296-INA296A5QDDFRQ1TR-ND,296-INA296A5QDDFRQ1CT-ND,296-INA296A5QDDFRQ1DKR-ND | INA296A5QDDFRQ1 |
| 296-INA296A3QDGKRQ1TR-ND,296-INA296A3QDGKRQ1CT-ND,296-INA296A3QDGKRQ1DKR-ND | INA296A3QDGKRQ1 |
| 296-INA241A3QDDFRQ1TR-ND,296-INA241A3QDDFRQ1CT-ND,296-INA241A3QDDFRQ1DKR-ND | INA241A3QDDFRQ1 |
| 296-46973-2-ND,296-46973-1-ND,296-46973-6-ND | OPA4376AQPWRQ1 |
| 296-26288-5-ND | OPA4376AIPW |
| 296-51513-2-ND,296-51513-1-ND,296-51513-6-ND | OPA859IDSGR |
| 175-MAX49925XATB+TTR-ND,175-MAX49925XATB+TCT-ND,175-MAX49925XATB+TDKR-ND | MAX49925XATB+T |
| MAX4239AUT+TTR-ND,MAX4239AUT+TCT-ND,MAX4239AUT+TDKR-ND | MAX4239AUT+T |
| 505-AD8411AWBRZ-RLTR-ND,505-AD8411AWBRZ-RLCT-ND,505-AD8411AWBRZ-RLDKR-ND | AD8411AWBRZ-RL |
| 505-AD8410AWBRMZ-ND | AD8410AWBRMZ |
| AD8274ARZ-R7TR-ND,AD8274ARZ-R7CT-ND,AD8274ARZ-R7DKR-ND | AD8274ARZ-R7 |
| MAX4238ASA±ND | MAX4238ASA+ |
| MAX4239ASA±ND | MAX4239ASA+ |
| 296-52302-2-ND,296-52302-1-ND,296-52302-6-ND | OPA859IDSGT |
| 175-MAX4238AUT/V+TTR-ND,175-MAX4238AUT/V+TCT-ND,175-MAX4238AUT/V+TDKR-ND | MAX4238AUT/V+T |
| 505-MAX49918IATB±ND | MAX49918IATB+ |
| 296-OPA858IDSGRTR-ND,296-OPA858IDSGRCT-ND,296-OPA858IDSGRDKR-ND | OPA858IDSGR |
| AD8271ARMZ-R7TR-ND,AD8271ARMZ-R7CT-ND,AD8271ARMZ-R7DKR-ND | AD8271ARMZ-R7 |
| 296-OPA858QDSGRQ1TR-ND,296-OPA858QDSGRQ1CT-ND,296-OPA858QDSGRQ1DKR-ND | OPA858QDSGRQ1 |
| 296-52301-2-ND,296-52301-1-ND,296-52301-6-ND | OPA858IDSGT |
| 296-OPA828IDGNRTR-ND,296-OPA828IDGNRCT-ND,296-OPA828IDGNRDKR-ND | OPA828IDGNR |
| 296-7316-5-ND | TLC2652AC-8D |
| 505-ADUM3195WBRQZ-ND | ADUM3195WBRQZ |
| 505-OP221GSZ-ND | OP221GSZ |
| 296-THS3491YRTR-ND,296-THS3491YRCT-ND,296-THS3491YRDKR-ND | THS3491YR |
| 505-LT6370AHS8E#PBF-ND | LT6370AHS8E#PBF |
| 296-OPA928DTTR-ND,296-OPA928DTCT-ND,296-OPA928DTDKR-ND | OPA928DT |
| 497-11014-2-ND,497-11014-1-ND,497-11014-6-ND | LM2904AYDT |
| 497-18716-2-ND,497-18716-1-ND,497-18716-6-ND | LM2904AWYPT |
| 497-10217-2-ND,497-10217-1-ND,497-10217-6-ND | LM2904YDT |
| 497-LM2904WYDTTR-ND,497-LM2904WYDTCT-ND,497-LM2904WYDTDKR-ND | LM2904WYDT |
| 497-10219-2-ND,497-10219-1-ND,497-10219-6-ND | LM2904YST |
| 296-INA214AIRSWRTR-ND,296-INA214AIRSWRCT-ND,296-INA214AIRSWRDKR-ND,2156-INA214AIRSWR-ND | INA214AIRSWR |
| 296-48551-2-ND,296-48551-1-ND,296-48551-6-ND | INA213AIRSWR |
| 296-48134-2-ND,296-48134-1-ND,296-48134-6-ND | INA215BIDCKR |
| 296-INA210AIRSWRTR-ND,296-INA210AIRSWRCT-ND,296-INA210AIRSWRDKR-ND,2156-INA210AIRSWR-ND | INA210AIRSWR |
| 296-40128-2-ND,296-40128-1-ND,296-40128-6-ND | INA212BIDCKR |
| 296-48133-2-ND,296-48133-1-ND,296-48133-6-ND | INA212BIRSWR |
| 296-40126-2-ND,296-40126-1-ND,296-40126-6-ND | INA211BIDCKR |
| 296-51148-2-ND,296-51148-1-ND,296-51148-6-ND | INA213CQDCKRQ1 |
| 296-38957-2-ND,296-38957-1-ND,296-38957-6-ND | INA214BIDCKT |
| 296-23585-2-ND,296-23585-1-ND,296-23585-6-ND | INA211AIDCKT |
| 296-INA211BIDCKTTR-ND,296-INA211BIDCKTCT-ND,296-INA211BIDCKTDKR-ND | INA211BIDCKT |
| 296-43565-2-ND,296-43565-1-ND,296-43565-6-ND | INA210BIDCKT |
| 296-48549-2-ND,296-48549-1-ND,296-48549-6-ND | INA212CIDCKR |
| MC34072AMTTBGOSTR-ND,MC34072AMTTBGOSCT-ND,MC34072AMTTBGOSDKR-ND | MC34072AMTTBG |
| 296-48552-2-ND,296-48552-1-ND,296-48552-6-ND | INA213CIDCKT |
| LE87100NQCTTR-ND,LE87100NQCTCT-ND,LE87100NQCTDKR-ND | LE87100NQCT |
| NCV33074ADTBR2GOSTR-ND,NCV33074ADTBR2GOSCT-ND,NCV33074ADTBR2GOSDKR-ND | NCV33074ADTBR2G |
| 296-50222-2-ND,296-50222-1-ND,296-50222-6-ND | OPA521IRGWT |
| MAX4238ATT+TTR-ND,MAX4238ATT+TCT-ND,MAX4238ATT+TDKR-ND | MAX4238ATT+T |
| AD8274ARZ-ND | AD8274ARZ |
| 296-OPA859QDSGRQ1TR-ND,296-OPA859QDSGRQ1CT-ND,296-OPA859QDSGRQ1DKR-ND | OPA859QDSGRQ1 |
| AD8271ARMZ-ND | AD8271ARMZ |
| AD8271BRMZ-ND | AD8271BRMZ |
| 505-AD8270ACPZ-WP-ND | AD8270ACPZ-WP |
| 505-LT6370AIS8E#PBF-ND | LT6370AIS8E#PBF |
| 497-12004-2-ND,497-12004-1-ND,497-12004-6-ND | LM2904WYPT |
| 497-16182-2-ND,497-16182-1-ND | LM2904WDT |
| AD8274ARMZ-ND | AD8274ARMZ |
| 2156-TLC2652C-8D-ND,296-7321-5-ND | TLC2652C-8D |
| AD8270ACPZ-R7TR-ND,AD8270ACPZ-R7CT-ND,AD8270ACPZ-R7DKR-ND | AD8270ACPZ-R7 |
| 5503-TP27-SRTR-ND,5503-TP27-SRCT-ND,5503-TP27-SRDKR-ND | TP27-SR |
| 5503-TPA7252-SO1RTR-ND,5503-TPA7252-SO1RCT-ND,5503-TPA7252-SO1RDKR-ND | TPA7252-SO1R |
| 5503-TP2261-TR-ND,5503-TP2261-TRCT-ND,5503-TP2261-TRDKR-ND | TP2261-TR |
| 5503-LMV321B-CRTR-ND,5503-LMV321B-CRCT-ND,5503-LMV321B-CRDKR-ND | LMV321B-CR |
| 5503-LMV358B-SRTR-ND,5503-LMV358B-SRCT-ND,5503-LMV358B-SRDKR-ND | LMV358B-SR |
| 5503-TP2264-TR-ND,5503-TP2264-TRCT-ND,5503-TP2264-TRDKR-ND | TP2264-TR |
| 5503-LM358A-TSRTR-ND,5503-LM358A-TSRCT-ND,5503-LM358A-TSRDKR-ND | LM358A-TSR |
| 5503-TP2111-TR-ND,5503-TP2111-TRCT-ND,5503-TP2111-TRDKR-ND | TP2111-TR |
| 5503-TP2264-SRTR-ND,5503-TP2264-SRCT-ND,5503-TP2264-SRDKR-ND | TP2264-SR |
| 5503-LMV358B-TSRTR-ND,5503-LMV358B-TSRCT-ND,5503-LMV358B-TSRDKR-ND | LMV358B-TSR |
| 5503-TP2111-CRTR-ND,5503-TP2111-CRCT-ND,5503-TP2111-CRDKR-ND | TP2111-CR |
| 5503-TP1562AL1-SRTR-ND,5503-TP1562AL1-SRCT-ND,5503-TP1562AL1-SRDKR-ND | TP1562AL1-SR |
| 5503-TP1562AL1-VRTR-ND,5503-TP1562AL1-VRCT-ND,5503-TP1562AL1-VRDKR-ND | TP1562AL1-VR |
| 5503-TP6002-FRTR-ND,5503-TP6002-FRCT-ND,5503-TP6002-FRDKR-ND | TP6002-FR |
| 5503-TP1562AL1-TSRTR-ND,5503-TP1562AL1-TSRCT-ND,5503-TP1562AL1-TSRDKR-ND | TP1562AL1-TSR |
| 5503-TP2121-CRTR-ND,5503-TP2121-CRCT-ND,5503-TP2121-CRDKR-ND | TP2121-CR |
| 5503-LM358A-VRTR-ND,5503-LM358A-VRCT-ND,5503-LM358A-VRDKR-ND | LM358A-VR |
| 5503-LM2904A-SRTR-ND,5503-LM2904A-SRCT-ND,5503-LM2904A-SRDKR-ND | LM2904A-SR |
| 5503-LM2904A-VRTR-ND,5503-LM2904A-VRCT-ND,5503-LM2904A-VRDKR-ND | LM2904A-VR |
| 5503-TP2122-VRTR-ND,5503-TP2122-VRCT-ND,5503-TP2122-VRDKR-ND | TP2122-VR |
| 5503-TP2122-SRTR-ND,5503-TP2122-SRCT-ND,5503-TP2122-SRDKR-ND | TP2122-SR |
| 5503-TP1241L1-TR-ND,5503-TP1241L1-TRCT-ND,5503-TP1241L1-TRDKR-ND | TP1241L1-TR |
| 5503-LMV324B-TR-ND,5503-LMV324B-TRCT-ND,5503-LMV324B-TRDKR-ND | LMV324B-TR |
| 5503-LMV324B-SRTR-ND,5503-LMV324B-SRCT-ND,5503-LMV324B-SRDKR-ND | LMV324B-SR |
| 5503-LM358A-F1RTR-ND,5503-LM358A-F1RCT-ND,5503-LM358A-F1RDKR-ND | LM358A-F1R |
| 5503-LM324A-TR-ND,5503-LM324A-TRCT-ND,5503-LM324A-TRDKR-ND | LM324A-TR |
| 5503-TPA2644-TS2RTR-ND,5503-TPA2644-TS2RCT-ND,5503-TPA2644-TS2RDKR-ND | TPA2644-TS2R |
| 5503-TPA2644-SO2RTR-ND,5503-TPA2644-SO2RCT-ND,5503-TPA2644-SO2RDKR-ND | TPA2644-SO2R |
| 296-INA500BIDCKRTR-ND,296-INA500BIDCKRCT-ND,296-INA500BIDCKRDKR-ND | INA500BIDCKR |
| 296-INA500CIDCKRTR-ND,296-INA500CIDCKRCT-ND,296-INA500CIDCKRDKR-ND | INA500CIDCKR |
| 296-INA500BIDBVRTR-ND,296-INA500BIDBVRCT-ND,296-INA500BIDBVRDKR-ND | INA500BIDBVR |
| 296-TL103WBIDRTR-ND,296-TL103WBIDRCT-ND,296-TL103WBIDRDKR-ND | TL103WBIDR |
| 296-INA500CIDBVRTR-ND,296-INA500CIDBVRCT-ND,296-INA500CIDBVRDKR-ND | INA500CIDBVR |
| 5503-LM2904A-TS1R-STR-ND,5503-LM2904A-TS1R-SCT-ND,5503-LM2904A-TS1R-SDKR-ND | LM2904A-TS1R-S |
| 5503-TP1562AL1-VS1R-STR-ND,5503-TP1562AL1-VS1R-SCT-ND,5503-TP1562AL1-VS1R-SDKR-ND | TP1562AL1-VS1R-S |
| 5503-TPH2502-VRTR-ND,5503-TPH2502-VRCT-ND,5503-TPH2502-VRDKR-ND | TPH2502-VR |
| 296-INA181A4QDCKRQ1TR-ND,296-INA181A4QDCKRQ1CT-ND,296-INA181A4QDCKRQ1DKR-ND | INA181A4QDCKRQ1 |
| 296-INA181A1QDCKRQ1TR-ND,296-INA181A1QDCKRQ1CT-ND,296-INA181A1QDCKRQ1DKR-ND | INA181A1QDCKRQ1 |
| 296-INA181A3QDCKRQ1TR-ND,296-INA181A3QDCKRQ1CT-ND,296-INA181A3QDCKRQ1DKR-ND | INA181A3QDCKRQ1 |
| 296-INA181A2QDCKRQ1TR-ND,296-INA181A2QDCKRQ1CT-ND,296-INA181A2QDCKRQ1DKR-ND | INA181A2QDCKRQ1 |
| 5503-TP2274-SO2RTR-ND,5503-TP2274-SO2RCT-ND,5503-TP2274-SO2RDKR-ND | TP2274-SO2R |
| 5503-TP1242L1-SRTR-ND,5503-TP1242L1-SRCT-ND,5503-TP1242L1-SRDKR-ND | TP1242L1-SR |
| 5503-TP1242L1-VRTR-ND,5503-TP1242L1-VRCT-ND,5503-TP1242L1-VRDKR-ND | TP1242L1-VR |
| 296-INA350ABSIRUGRTR-ND,296-INA350ABSIRUGRCT-ND,296-INA350ABSIRUGRDKR-ND | INA350ABSIRUGR |
| 296-INA350CDSIRUGRTR-ND,296-INA350CDSIRUGRCT-ND,296-INA350CDSIRUGRDKR-ND | INA350CDSIRUGR |
| 5503-TP07A-SRTR-ND,5503-TP07A-SRCT-ND,5503-TP07A-SRDKR-ND | TP07A-SR |
| 5503-TP17-SRTR-ND,5503-TP17-SRCT-ND,5503-TP17-SRDKR-ND | TP17-SR |
| 5503-TP5531U-CRTR-ND,5503-TP5531U-CRCT-ND,5503-TP5531U-CRDKR-ND | TP5531U-CR |
| 5503-TP5531-TR-ND,5503-TP5531-TRCT-ND,5503-TP5531-TRDKR-ND | TP5531-TR |
| 5503-TP1281L1-TR-ND,5503-TP1281L1-TRCT-ND,5503-TP1281L1-TRDKR-ND | TP1281L1-TR |
| 5503-LM2904A-SO1R-STR-ND,5503-LM2904A-SO1R-SCT-ND,5503-LM2904A-SO1R-SDKR-ND | LM2904A-SO1R-S |
| 296-INA210AIDCKJTR-ND,296-INA210AIDCKJCT-ND,296-INA210AIDCKJDKR-ND | INA210AIDCKJ |
| 5503-TPA7253A-SO1RTR-ND,5503-TPA7253A-SO1RCT-ND,5503-TPA7253A-SO1RDKR-ND | TPA7253A-SO1R |
| 296-INA215CIDCKRTR-ND,296-INA215CIDCKRCT-ND,296-INA215CIDCKRDKR-ND | INA215CIDCKR |
| 296-INA214CIRSWRTR-ND,296-INA214CIRSWRCT-ND,296-INA214CIRSWRDKR-ND | INA214CIRSWR |
| 5503-TP1561AUL1-CRTR-ND,5503-TP1561AUL1-CRCT-ND,5503-TP1561AUL1-CRDKR-ND | TP1561AUL1-CR |
| 5503-TP6001U-CRTR-ND,5503-TP6001U-CRCT-ND,5503-TP6001U-CRDKR-ND | TP6001U-CR |
| 5503-TP6001R-TR-ND,5503-TP6001R-TRCT-ND,5503-TP6001R-TRDKR-ND | TP6001R-TR |
| 5503-TP6001-TR-ND,5503-TP6001-TRCT-ND,5503-TP6001-TRDKR-ND | TP6001-TR |
| 5503-TPA2681-S5TR-ND,5503-TPA2681-S5TRCT-ND,5503-TPA2681-S5TRDKR-ND | TPA2681-S5TR |
| 5503-TP6001-CRTR-ND,5503-TP6001-CRCT-ND,5503-TP6001-CRDKR-ND | TP6001-CR |
| 5503-TP2261-SRTR-ND,5503-TP2261-SRCT-ND,5503-TP2261-SRDKR-ND | TP2261-SR |
| 5503-TP2581-TR-ND,5503-TP2581-TRCT-ND,5503-TP2581-TRDKR-ND | TP2581-TR |
| 296-INA185A4QDCKRQ1TR-ND,296-INA185A4QDCKRQ1CT-ND,296-INA185A4QDCKRQ1DKR-ND | INA185A4QDCKRQ1 |
| 296-INA185A2QDCKRQ1TR-ND,296-INA185A2QDCKRQ1CT-ND,296-INA185A2QDCKRQ1DKR-ND | INA185A2QDCKRQ1 |
| 296-INA185A3QDCKRQ1TR-ND,296-INA185A3QDCKRQ1CT-ND,296-INA185A3QDCKRQ1DKR-ND | INA185A3QDCKRQ1 |
| 296-INA185A1QDCKRQ1TR-ND,296-INA185A1QDCKRQ1CT-ND,296-INA185A1QDCKRQ1DKR-ND | INA185A1QDCKRQ1 |
| 296-51144-2-ND,296-51144-1-ND,296-51144-6-ND,2156-INA211CQDCKRQ1-ND | INA211CQDCKRQ1 |
| 296-51151-2-ND,296-51151-1-ND,296-51151-6-ND | INA214CQDCKRQ1 |
| 5503-TP2582-SRTR-ND,5503-TP2582-SRCT-ND,5503-TP2582-SRDKR-ND | TP2582-SR |
| 5503-TP2582-VRTR-ND,5503-TP2582-VRCT-ND,5503-TP2582-VRDKR-ND | TP2582-VR |
| 5503-TP2582-TSRTR-ND,5503-TP2582-TSRCT-ND,5503-TP2582-TSRDKR-ND | TP2582-TSR |
| 488-NCS20162DR2GTR-ND,488-NCS20162DR2GCT-ND,488-NCS20162DR2GDKR-ND | NCS20162DR2G |
| 5503-TPA7252A-SO1RTR-ND,5503-TPA7252A-SO1RCT-ND,5503-TPA7252A-SO1RDKR-ND | TPA7252A-SO1R |
| 5503-TPA2641U-S5TR-ND,5503-TPA2641U-S5TRCT-ND,5503-TPA2641U-S5TRDKR-ND | TPA2641U-S5TR |
| 5503-TPA2641-S5TR-ND,5503-TPA2641-S5TRCT-ND,5503-TPA2641-S5TRDKR-ND | TPA2641-S5TR |
| 5503-TP2262-SRTR-ND,5503-TP2262-SRCT-ND,5503-TP2262-SRDKR-ND | TP2262-SR |
| 5503-TPA2642-VS1RTR-ND,5503-TPA2642-VS1RCT-ND,5503-TPA2642-VS1RDKR-ND | TPA2642-VS1R |
| 5503-TP2262-VRTR-ND,5503-TP2262-VRCT-ND,5503-TP2262-VRDKR-ND | TP2262-VR |
| 5503-TP2262-TSRTR-ND,5503-TP2262-TSRCT-ND,5503-TP2262-TSRDKR-ND | TP2262-TSR |
| 5503-TP2121-TR-ND,5503-TP2121-TRCT-ND,5503-TP2121-TRDKR-ND | TP2121-TR |
| 5503-TP1561AL1-TR-ND,5503-TP1561AL1-TRCT-ND,5503-TP1561AL1-TRDKR-ND | TP1561AL1-TR |
| 488-NCV20162DR2GTR-ND,488-NCV20162DR2GCT-ND,488-NCV20162DR2GDKR-ND | NCV20162DR2G |
| 296-TLV9362QPWRQ1TR-ND,296-TLV9362QPWRQ1CT-ND,296-TLV9362QPWRQ1DKR-ND | TLV9362QPWRQ1 |
| 5503-TPA2642-SO1RTR-ND,5503-TPA2642-SO1RCT-ND,5503-TPA2642-SO1RDKR-ND | TPA2642-SO1R |
| 150-MCP60711UT-E/LTYTR-ND,150-MCP60711UT-E/LTYCT-ND,150-MCP60711UT-E/LTYDKR-ND | MCP60711UT-E/LTY |
| 5503-TP2584-TR-ND,5503-TP2584-TRCT-ND,5503-TP2584-TRDKR-ND | TP2584-TR |
| 150-MCP60713T-E/CHTR-ND,150-MCP60713T-E/CHCT-ND,150-MCP60713T-E/CHDKR-ND | MCP60713T-E/CH |
| 497-TSV781ILTTR-ND,497-TSV781ILTCT-ND,497-TSV781ILTDKR-ND | TSV781ILT |
| 5503-TP6002-SRTR-ND,5503-TP6002-SRCT-ND,5503-TP6002-SRDKR-ND | TP6002-SR |
| 5503-TP6002-VRTR-ND,5503-TP6002-VRCT-ND,5503-TP6002-VRDKR-ND | TP6002-VR |
| 5503-TP2584-SRTR-ND,5503-TP2584-SRCT-ND,5503-TP2584-SRDKR-ND | TP2584-SR |
| 150-MCP60721UT-E/LTYTR-ND,150-MCP60721UT-E/LTYCT-ND,150-MCP60721UT-E/LTYDKR-ND | MCP60721UT-E/LTY |
| 150-MCP60721T-E/OTTR-ND,150-MCP60721T-E/OTCT-ND,150-MCP60721T-E/OTDKR-ND | MCP60721T-E/OT |
| 5503-TP1562AL1-FRTR-ND,5503-TP1562AL1-FRCT-ND,5503-TP1562AL1-FRDKR-ND | TP1562AL1-FR |
| 5503-TP5534-SRTR-ND,5503-TP5534-SRCT-ND,5503-TP5534-SRDKR-ND | TP5534-SR |
| 5503-TPA191A5-SC6RTR-ND,5503-TPA191A5-SC6RCT-ND,5503-TPA191A5-SC6RDKR-ND | TPA191A5-SC6R |
| 31-AS2376S-13TR-ND,31-AS2376S-13CT-ND,31-AS2376S-13DKR-ND | AS2376S-13 |
| 5503-TP2262L1-SO1R-STR-ND,5503-TP2262L1-SO1R-SCT-ND,5503-TP2262L1-SO1R-SDKR-ND | TP2262L1-SO1R-S |
| 497-TSZ151ICTTR-ND,497-TSZ151ICT-ND,497-TSZ151ICTDKR-ND | TSZ151ICT |
| 497-TSZ151ILTTR-ND,497-TSZ151ILTCT-ND,497-TSZ151ILTDKR-ND | TSZ151ILT |
| 296-OPA991QDCKRQ1TR-ND,296-OPA991QDCKRQ1CT-ND,296-OPA991QDCKRQ1DKR-ND | OPA991QDCKRQ1 |
| 846-BA83472YFVM-CTR-ND,846-BA83472YFVM-CTRCT-ND,846-BA83472YFVM-CTRDKR-ND | BA83472YFVM-CTR |
| 5503-TP2272-VS1RTR-ND,5503-TP2272-VS1RCT-ND,5503-TP2272-VS1RDKR-ND | TP2272-VS1R |
| 5503-TP1564AL1-TR-ND,5503-TP1564AL1-TRCT-ND,5503-TP1564AL1-TRDKR-ND | TP1564AL1-TR |
| 296-40133-2-ND,296-40133-1-ND,296-40133-6-ND | INA215AIDCKT |
| 488-NCS20164DR2GTR-ND,488-NCS20164DR2GCT-ND,488-NCS20164DR2GDKR-ND | NCS20164DR2G |
| 150-MCP60821T-E/OTTR-ND,150-MCP60821T-E/OTCT-ND,150-MCP60821T-E/OTDKR-ND | MCP60821T-E/OT |
| 150-MCP60821UT-E/LTYTR-ND,150-MCP60821UT-E/LTYCT-ND,150-MCP60821UT-E/LTYDKR-ND | MCP60821UT-E/LTY |
| 5503-TP1561AL1-S5TR-STR-ND,5503-TP1561AL1-S5TR-SCT-ND,5503-TP1561AL1-S5TR-SDKR-ND | TP1561AL1-S5TR-S |
| 5503-TP6004-TR-ND,5503-TP6004-TRCT-ND,5503-TP6004-TRDKR-ND | TP6004-TR |
| 5503-TPH2501-TR-ND,5503-TPH2501-TRCT-ND,5503-TPH2501-TRDKR-ND | TPH2501-TR |
| 5503-TP6004-SRTR-ND,5503-TP6004-SRCT-ND,5503-TP6004-SRDKR-ND | TP6004-SR |
| 5503-TP1564AL1-SRTR-ND,5503-TP1564AL1-SRCT-ND,5503-TP1564AL1-SRDKR-ND | TP1564AL1-SR |
| 5503-TP2112-SRTR-ND,5503-TP2112-SRCT-ND,5503-TP2112-SRDKR-ND | TP2112-SR |
| 5503-TP2112-VRTR-ND,5503-TP2112-VRCT-ND,5503-TP2112-VRDKR-ND | TP2112-VR |
| 5503-TPA2644-SO2R-STR-ND,5503-TPA2644-SO2R-SCT-ND,5503-TPA2644-SO2R-SDKR-ND | TPA2644-SO2R-S |
| 296-TLV9364QPWRQ1TR-ND,296-TLV9364QPWRQ1CT-ND,296-TLV9364QPWRQ1DKR-ND | TLV9364QPWRQ1 |
| 296-TLV9364QDRQ1TR-ND,296-TLV9364QDRQ1CT-ND,296-TLV9364QDRQ1DKR-ND | TLV9364QDRQ1 |
| 296-OPA994IDCKRTR-ND,296-OPA994IDCKRCT-ND,296-OPA994IDCKRDKR-ND | OPA994IDCKR |
| 296-OPA991SQDBVRQ1TR-ND,296-OPA991SQDBVRQ1CT-ND,296-OPA991SQDBVRQ1DKR-ND | OPA991SQDBVRQ1 |
| 296-OPA2323IDGKRTR-ND,296-OPA2323IDGKRCT-ND,296-OPA2323IDGKRDKR-ND | OPA2323IDGKR |
| 296-OPA2323IDDFRTR-ND,296-OPA2323IDDFRCT-ND,296-OPA2323IDDFRDKR-ND | OPA2323IDDFR |
| 497-4261-2-ND,497-4261-1-ND,497-4261-6-ND | LM2904WHDT |
| 488-NCV21674DMG050R2GTR-ND,488-NCV21674DMG050R2GCT-ND,488-NCV21674DMG050R2GDKR-ND | NCV21674DMG050R2G |
| 296-51139-2-ND,296-51139-1-ND,296-51139-6-ND | INA210CIDCKT |
| 497-TSZ151IYCTTR-ND,497-TSZ151IYCT-ND,497-TSZ151IYCTDKR-ND | TSZ151IYCT |
| 497-TSZ151IYLTTR-ND,497-TSZ151IYLTCT-ND,497-TSZ151IYLTDKR-ND | TSZ151IYLT |
| 488-NCV33074DR2GTR-ND,488-NCV33074DR2GCT-ND,488-NCV33074DR2GDKR-ND | NCV33074DR2G |
| 505-MAX49925XATB±ND | MAX49925XATB+ |
| 5503-TPH2503-TR-ND,5503-TPH2503-TRCT-ND,5503-TPH2503-TRDKR-ND | TPH2503-TR |
| 5503-TP5591-SRTR-ND,5503-TP5591-SRCT-ND,5503-TP5591-SRDKR-ND | TP5591-SR |
| 5503-TP1562AL1-SO1R-STR-ND,5503-TP1562AL1-SO1R-SCT-ND,5503-TP1562AL1-SO1R-SDKR-ND | TP1562AL1-SO1R-S |
| 296-TLV9162QPWRQ1TR-ND,296-TLV9162QPWRQ1CT-ND,296-TLV9162QPWRQ1DKR-ND | TLV9162QPWRQ1 |
| 5503-TP2124-TR-ND,5503-TP2124-TRCT-ND,5503-TP2124-TRDKR-ND | TP2124-TR |
| 5503-TP5591-TR-ND,5503-TP5591-TRCT-ND,5503-TP5591-TRDKR-ND | TP5591-TR |
| 5503-TP5591U-CRTR-ND,5503-TP5591U-CRCT-ND,5503-TP5591U-CRDKR-ND | TP5591U-CR |
| 5503-TP2124-SRTR-ND,5503-TP2124-SRCT-ND,5503-TP2124-SRDKR-ND | TP2124-SR |
| 497-TSB624IYPTTR-ND,497-TSB624IYPTCT-ND,497-TSB624IYPTDKR-ND | TSB624IYPT |
| 497-TSV774IPTTR-ND,497-TSV774IPTCT-ND,497-TSV774IPTDKR-ND | TSV774IPT |
| 296-TLV9162SIRUGRTR-ND,296-TLV9162SIRUGRCT-ND,296-TLV9162SIRUGRDKR-ND | TLV9162SIRUGR |
| 5503-TP2274-TS2RTR-ND,5503-TP2274-TS2RCT-ND,5503-TP2274-TS2RDKR-ND | TP2274-TS2R |
| 497-TSB182IDTTR-ND,497-TSB182IDTCT-ND,497-TSB182IDTDKR-ND | TSB182IDT |
| 5503-TP5592-SRTR-ND,5503-TP5592-SRCT-ND,5503-TP5592-SRDKR-ND | TP5592-SR |
| 5503-TPA183A2-S5TR-ND,5503-TPA183A2-S5TRCT-ND,5503-TPA183A2-S5TRDKR-ND | TPA183A2-S5TR |
| 5503-TP1564AL1-SO2R-STR-ND,5503-TP1564AL1-SO2R-SCT-ND,5503-TP1564AL1-SO2R-SDKR-ND | TP1564AL1-SO2R-S |
| 497-TSB182ISTTR-ND,497-TSB182ISTCT-ND,497-TSB182ISTDKR-ND | TSB182IST |
| 175-MAX40111ANT+TTR-ND,175-MAX40111ANT+TCT-ND,175-MAX40111ANT+TDKR-ND | MAX40111ANT+T |
| 2129-NJM8532RZ-TE2TR-ND,2129-NJM8532RZ-TE2CT-ND,2129-NJM8532RZ-TE2DKR-ND | NJM8532RZ-TE2 |
| 497-TSB952IQ2TTR-ND,497-TSB952IQ2TCT-ND,497-TSB952IQ2TDKR-ND | TSB952IQ2T |
| 5503-TP5531U-TR-ND,5503-TP5531U-TRCT-ND,5503-TP5531U-TRDKR-ND | TP5531U-TR |
| 497-TSB952IDTTR-ND,497-TSB952IDTCT-ND,497-TSB952IDTDKR-ND | TSB952IDT |
| 5503-TPA183A1-S5TR-ND,5503-TPA183A1-S5TRCT-ND,5503-TPA183A1-S5TRDKR-ND | TPA183A1-S5TR |
| 296-OPA4990QPWRQ1TR-ND,296-OPA4990QPWRQ1CT-ND,296-OPA4990QPWRQ1DKR-ND | OPA4990QPWRQ1 |
| 5503-TP5592-VRTR-ND,5503-TP5592-VRCT-ND,5503-TP5592-VRDKR-ND | TP5592-VR |
| 296-TLV9164QPWRQ1TR-ND,296-TLV9164QPWRQ1CT-ND,296-TLV9164QPWRQ1DKR-ND | TLV9164QPWRQ1 |
| 296-TLV9164QDRQ1TR-ND,296-TLV9164QDRQ1CT-ND,296-TLV9164QDRQ1DKR-ND | TLV9164QDRQ1 |
| 497-TSV774IYPTTR-ND,497-TSV774IYPTCT-ND,497-TSV774IYPTDKR-ND | TSV774IYPT |
| 2129-NL6012AFAE2DTR-ND,2129-NL6012AFAE2DCT-ND,2129-NL6012AFAE2DDKR-ND | NL6012AFAE2D |
| 497-TSC201ISTTR-ND,497-TSC201ISTCT-ND,497-TSC201ISTDKR-ND | TSC201IST |
| 488-NCS21671SQ200T2GTR-ND,488-NCS21671SQ200T2GCT-ND,488-NCS21671SQ200T2GDKR-ND | NCS21671SQ200T2G |
| 488-NCS21671SQ100T2GTR-ND,488-NCS21671SQ100T2GCT-ND,488-NCS21671SQ100T2GDKR-ND | NCS21671SQ100T2G |
| 497-TSC202IDTTR-ND,497-TSC202IDTCT-ND,497-TSC202IDTDKR-ND | TSC202IDT |
| 497-TSC201IDTTR-ND,497-TSC201IDTCT-ND,497-TSC201IDTDKR-ND | TSC201IDT |
| 488-NCS21671SQ050T2GTR-ND,488-NCS21671SQ050T2GCT-ND,488-NCS21671SQ050T2GDKR-ND | NCS21671SQ050T2G |
| 497-TSC202ISTTR-ND,497-TSC202ISTCT-ND,497-TSC202ISTDKR-ND | TSC202IST |
| 296-OPA4323IDYYRTR-ND,296-OPA4323IDYYRCT-ND,296-OPA4323IDYYRDKR-ND | OPA4323IDYYR |
| 488-NCV21671SQ200T2GTR-ND,488-NCV21671SQ200T2GCT-ND,488-NCV21671SQ200T2GDKR-ND | NCV21671SQ200T2G |
| 488-NCV21671SQ100T2GTR-ND,488-NCV21671SQ100T2GCT-ND,488-NCV21671SQ100T2GDKR-ND | NCV21671SQ100T2G |
| 488-NCV21671SQ050T2GTR-ND,488-NCV21671SQ050T2GCT-ND,488-NCV21671SQ050T2GDKR-ND | NCV21671SQ050T2G |
| 488-NCV21671SQ025T2GTR-ND,488-NCV21671SQ025T2GCT-ND,488-NCV21671SQ025T2GDKR-ND | NCV21671SQ025T2G |
| 497-TSB182IYSTTR-ND,497-TSB182IYSTCT-ND,497-TSB182IYSTDKR-ND | TSB182IYST |
| 497-TSB182IYDTTR-ND,497-TSB182IYDTCT-ND,497-TSB182IYDTDKR-ND | TSB182IYDT |
| 296-INA241B4IDGKRTR-ND,296-INA241B4IDGKRCT-ND,296-INA241B4IDGKRDKR-ND | INA241B4IDGKR |
| 296-INA241B3IDRTR-ND,296-INA241B3IDRCT-ND,296-INA241B3IDRDKR-ND | INA241B3IDR |
| 296-INA241B4QDRQ1TR-ND,296-INA241B4QDRQ1CT-ND,296-INA241B4QDRQ1DKR-ND | INA241B4QDRQ1 |
| 296-INA296B4QDRQ1TR-ND,296-INA296B4QDRQ1CT-ND,296-INA296B4QDRQ1DKR-ND | INA296B4QDRQ1 |
| 296-INA296B2IDGKRTR-ND,296-INA296B2IDGKRCT-ND,296-INA296B2IDGKRDKR-ND | INA296B2IDGKR |
| 296-INA296B1IDGKRTR-ND,296-INA296B1IDGKRCT-ND,296-INA296B1IDGKRDKR-ND | INA296B1IDGKR |
| 296-INA241B5IDGKRTR-ND,296-INA241B5IDGKRCT-ND,296-INA241B5IDGKRDKR-ND | INA241B5IDGKR |
| 296-INA296B3IDRTR-ND,296-INA296B3IDRCT-ND,296-INA296B3IDRDKR-ND | INA296B3IDR |
| 296-INA241B1IDRTR-ND,296-INA241B1IDRCT-ND,296-INA241B1IDRDKR-ND | INA241B1IDR |
| 296-INA296B5IDGKRTR-ND,296-INA296B5IDGKRCT-ND,296-INA296B5IDGKRDKR-ND | INA296B5IDGKR |
| 296-INA241B2IDRTR-ND,296-INA241B2IDRCT-ND,296-INA241B2IDRDKR-ND | INA241B2IDR |
| 296-INA241B4IDRTR-ND,296-INA241B4IDRCT-ND,296-INA241B4IDRDKR-ND | INA241B4IDR |
| 296-INA241B5IDRTR-ND,296-INA241B5IDRCT-ND,296-INA241B5IDRDKR-ND | INA241B5IDR |
| 296-INA296B2IDRTR-ND,296-INA296B2IDRCT-ND,296-INA296B2IDRDKR-ND | INA296B2IDR |
| 296-INA241B3IDGKRTR-ND,296-INA241B3IDGKRCT-ND,296-INA241B3IDGKRDKR-ND | INA241B3IDGKR |
| 296-INA296B3IDGKRTR-ND,296-INA296B3IDGKRCT-ND,296-INA296B3IDGKRDKR-ND | INA296B3IDGKR |
| 296-INA296B4IDGKRTR-ND,296-INA296B4IDGKRCT-ND,296-INA296B4IDGKRDKR-ND | INA296B4IDGKR |
| 296-INA296B4IDRTR-ND,296-INA296B4IDRCT-ND,296-INA296B4IDRDKR-ND | INA296B4IDR |
| 296-INA310B4IDGKRTR-ND,296-INA310B4IDGKRCT-ND,296-INA310B4IDGKRDKR-ND | INA310B4IDGKR |
| 296-INA241B1IDGKRTR-ND,296-INA241B1IDGKRCT-ND,296-INA241B1IDGKRDKR-ND | INA241B1IDGKR |
| 296-INA296B1IDRTR-ND,296-INA296B1IDRCT-ND,296-INA296B1IDRDKR-ND | INA296B1IDR |
| 296-INA310B5IDGKRTR-ND,296-INA310B5IDGKRCT-ND,296-INA310B5IDGKRDKR-ND | INA310B5IDGKR |
| 296-INA241B2IDGKRTR-ND,296-INA241B2IDGKRCT-ND,296-INA241B2IDGKRDKR-ND | INA241B2IDGKR |
| 296-OPA2992QPWRQ1TR-ND,296-OPA2992QPWRQ1CT-ND,296-OPA2992QPWRQ1DKR-ND | OPA2992QPWRQ1 |
| 5503-TPH2504-TR-ND,5503-TPH2504-TRCT-ND,5503-TPH2504-TRDKR-ND | TPH2504-TR |
| 488-NCS7031DM1G020R2GTR-ND,488-NCS7031DM1G020R2GCT-ND,488-NCS7031DM1G020R2GDKR-ND | NCS7031DM1G020R2G |
| 488-NCV21671DM200R2GTR-ND,488-NCV21671DM200R2GCT-ND,488-NCV21671DM200R2GDKR-ND | NCV21671DM200R2G |
| 488-NCV21671DM050R2GTR-ND,488-NCV21671DM050R2GCT-ND,488-NCV21671DM050R2GDKR-ND | NCV21671DM050R2G |
| 488-NCV21671DM100R2GTR-ND,488-NCV21671DM100R2GCT-ND,488-NCV21671DM100R2GDKR-ND | NCV21671DM100R2G |
| 497-TSB952IYQ2TTR-ND,497-TSB952IYQ2TCT-ND,497-TSB952IYQ2TDKR-ND | TSB952IYQ2T |
| 497-TSB952IYDTTR-ND,497-TSB952IYDTCT-ND,497-TSB952IYDTDKR-ND | TSB952IYDT |
| 5503-TP5594-SRTR-ND,5503-TP5594-SRCT-ND,5503-TP5594-SRDKR-ND | TP5594-SR |
| 296-OPA2992SIRUGRTR-ND,296-OPA2992SIRUGRCT-ND,296-OPA2992SIRUGRDKR-ND | OPA2992SIRUGR |
| 5503-TP5594-TR-ND,5503-TP5594-TRCT-ND,5503-TP5594-TRDKR-ND | TP5594-TR |
| 497-TSC2020ISTTR-ND,497-TSC2020ISTCT-ND,497-TSC2020ISTDKR-ND | TSC2020IST |
| 497-TSC2022ISTTR-ND,497-TSC2022ISTCT-ND,497-TSC2022ISTDKR-ND | TSC2022IST |
| 497-TSC2020IDTTR-ND,497-TSC2020IDTCT-ND,497-TSC2020IDTDKR-ND | TSC2020IDT |
| 497-TSC2021ISTTR-ND,497-TSC2021ISTCT-ND,497-TSC2021ISTDKR-ND | TSC2021IST |
| 497-TSC201IYDTTR-ND,497-TSC201IYDTCT-ND,497-TSC201IYDTDKR-ND | TSC201IYDT |
| 497-TSC202IYDTTR-ND,497-TSC202IYDTCT-ND,497-TSC202IYDTDKR-ND | TSC202IYDT |
| 497-TSC202IYSTTR-ND,497-TSC202IYSTCT-ND,497-TSC202IYSTDKR-ND | TSC202IYST |
| 497-TSC200IYDTTR-ND,497-TSC200IYDTCT-ND,497-TSC200IYDTDKR-ND | TSC200IYDT |
| 497-TSC200IYSTTR-ND,497-TSC200IYSTCT-ND,497-TSC200IYSTDKR-ND | TSC200IYST |
| 497-TSC201IYSTTR-ND,497-TSC201IYSTCT-ND,497-TSC201IYSTDKR-ND | TSC201IYST |
| 488-NCV7031D1G020R2GTR-ND,488-NCV7031D1G020R2GCT-ND,488-NCV7031D1G020R2GDKR-ND | NCV7031D1G020R2G |
| 296-INA296B5QDDFRQ1TR-ND,296-INA296B5QDDFRQ1CT-ND,296-INA296B5QDDFRQ1DKR-ND | INA296B5QDDFRQ1 |
| 296-INA241B5QDDFRQ1TR-ND,296-INA241B5QDDFRQ1CT-ND,296-INA241B5QDDFRQ1DKR-ND | INA241B5QDDFRQ1 |
| 296-INA310B4QDGKRQ1TR-ND,296-INA310B4QDGKRQ1CT-ND,296-INA310B4QDGKRQ1DKR-ND | INA310B4QDGKRQ1 |
| 296-INA296B1QDGKRQ1TR-ND,296-INA296B1QDGKRQ1CT-ND,296-INA296B1QDGKRQ1DKR-ND | INA296B1QDGKRQ1 |
| 296-INA241B5QDGKRQ1TR-ND,296-INA241B5QDGKRQ1CT-ND,296-INA241B5QDGKRQ1DKR-ND | INA241B5QDGKRQ1 |
| 296-INA241B1QDGKRQ1TR-ND,296-INA241B1QDGKRQ1CT-ND,296-INA241B1QDGKRQ1DKR-ND | INA241B1QDGKRQ1 |
| 296-INA296B3QDGKRQ1TR-ND,296-INA296B3QDGKRQ1CT-ND,296-INA296B3QDGKRQ1DKR-ND | INA296B3QDGKRQ1 |
| 296-INA296B1QDRQ1TR-ND,296-INA296B1QDRQ1CT-ND,296-INA296B1QDRQ1DKR-ND | INA296B1QDRQ1 |
| 296-INA296B5QDRQ1TR-ND,296-INA296B5QDRQ1CT-ND,296-INA296B5QDRQ1DKR-ND | INA296B5QDRQ1 |
| 296-INA296B3QDRQ1TR-ND,296-INA296B3QDRQ1CT-ND,296-INA296B3QDRQ1DKR-ND | INA296B3QDRQ1 |
| 296-INA296B2QDRQ1TR-ND,296-INA296B2QDRQ1CT-ND,296-INA296B2QDRQ1DKR-ND | INA296B2QDRQ1 |
| 296-INA296B5QDGKRQ1TR-ND,296-INA296B5QDGKRQ1CT-ND,296-INA296B5QDGKRQ1DKR-ND | INA296B5QDGKRQ1 |
| 296-INA241B3QDGKRQ1TR-ND,296-INA241B3QDGKRQ1CT-ND,296-INA241B3QDGKRQ1DKR-ND | INA241B3QDGKRQ1 |
| 296-INA296B4QDGKRQ1TR-ND,296-INA296B4QDGKRQ1CT-ND,296-INA296B4QDGKRQ1DKR-ND | INA296B4QDGKRQ1 |
| 296-INA241B4QDGKRQ1TR-ND,296-INA241B4QDGKRQ1CT-ND,296-INA241B4QDGKRQ1DKR-ND | INA241B4QDGKRQ1 |
| 296-INA241B2QDGKRQ1TR-ND,296-INA241B2QDGKRQ1CT-ND,296-INA241B2QDGKRQ1DKR-ND | INA241B2QDGKRQ1 |
| 296-INA241B4QDDFRQ1TR-ND,296-INA241B4QDDFRQ1CT-ND,296-INA241B4QDDFRQ1DKR-ND | INA241B4QDDFRQ1 |
| 296-INA296B2QDGKRQ1TR-ND,296-INA296B2QDGKRQ1CT-ND,296-INA296B2QDGKRQ1DKR-ND | INA296B2QDGKRQ1 |
| 296-INA241A5IDRTR-ND,296-INA241A5IDRCT-ND,296-INA241A5IDRDKR-ND | INA241A5IDR |
| 5503-TP5551-SRTR-ND,5503-TP5551-SRCT-ND,5503-TP5551-SRDKR-ND | TP5551-SR |
| 5503-TP5551-TR-ND,5503-TP5551-TRCT-ND,5503-TP5551-TRDKR-ND | TP5551-TR |
| 497-TSV774IQ5TTR-ND,497-TSV774IQ5TCT-ND,497-TSV774IQ5TDKR-ND | TSV774IQ5T |
| 296-INA310B3QDGKRQ1TR-ND,296-INA310B3QDGKRQ1CT-ND,296-INA310B3QDGKRQ1DKR-ND | INA310B3QDGKRQ1 |
| 296-OPA4992QPWRQ1TR-ND,296-OPA4992QPWRQ1CT-ND,296-OPA4992QPWRQ1DKR-ND | OPA4992QPWRQ1 |
| 296-INA310B5QDGKRQ1TR-ND,296-INA310B5QDGKRQ1CT-ND,296-INA310B5QDGKRQ1DKR-ND | INA310B5QDGKRQ1 |
| 296-INA296A4QDRQ1TR-ND,296-INA296A4QDRQ1CT-ND,296-INA296A4QDRQ1DKR-ND | INA296A4QDRQ1 |
| 296-INA241A4QDRQ1TR-ND,296-INA241A4QDRQ1CT-ND,296-INA241A4QDRQ1DKR-ND | INA241A4QDRQ1 |
| 296-INA310B2QDGKRQ1TR-ND,296-INA310B2QDGKRQ1CT-ND,296-INA310B2QDGKRQ1DKR-ND | INA310B2QDGKRQ1 |
| 296-INA310B1QDGKRQ1TR-ND,296-INA310B1QDGKRQ1CT-ND,296-INA310B1QDGKRQ1DKR-ND | INA310B1QDGKRQ1 |
| 5503-TPA2296F-S6TR-STR-ND,5503-TPA2296F-S6TR-SCT-ND,5503-TPA2296F-S6TR-SDKR-ND | TPA2296F-S6TR-S |
| 296-INA310A4IDGKRTR-ND,296-INA310A4IDGKRCT-ND,296-INA310A4IDGKRDKR-ND | INA310A4IDGKR |
| 846-BA83474YFV-CE2TR-ND,846-BA83474YFV-CE2CT-ND,846-BA83474YFV-CE2DKR-ND | BA83474YFV-CE2 |
| 296-INA310A5IDGKRTR-ND,296-INA310A5IDGKRCT-ND,296-INA310A5IDGKRDKR-ND | INA310A5IDGKR |
| 497-TSC2020IYDTTR-ND,497-TSC2020IYDTCT-ND,497-TSC2020IYDTDKR-ND | TSC2020IYDT |
| 497-TSC2020IYSTTR-ND,497-TSC2020IYSTCT-ND,497-TSC2020IYSTDKR-ND | TSC2020IYST |
| 497-TSZ181H1YLTTR-ND,497-TSZ181H1YLTCT-ND,497-TSZ181H1YLTDKR-ND | TSZ181H1YLT |
| 5503-TP5552-SRTR-ND,5503-TP5552-SRCT-ND,5503-TP5552-SRDKR-ND | TP5552-SR |
| 5503-TP5552-VRTR-ND,5503-TP5552-VRCT-ND,5503-TP5552-VRDKR-ND | TP5552-VR |
| 5503-TPA2296H-S6TR-STR-ND,5503-TPA2296H-S6TR-SCT-ND,5503-TPA2296H-S6TR-SDKR-ND | TPA2296H-S6TR-S |
| 5503-TPA2296H-S5TR-STR-ND,5503-TPA2296H-S5TR-SCT-ND,5503-TPA2296H-S5TR-SDKR-ND | TPA2296H-S5TR-S |
| 5503-TPA2296T-S5TR-ND,5503-TPA2296T-S5TRCT-ND,5503-TPA2296T-S5TRDKR-ND | TPA2296T-S5TR |
| 296-INA296A5IDRTR-ND,296-INA296A5IDRCT-ND,296-INA296A5IDRDKR-ND | INA296A5IDR |
| 296-INA296A1IDRTR-ND,296-INA296A1IDRCT-ND,296-INA296A1IDRDKR-ND | INA296A1IDR |
| 296-INA296A2IDRTR-ND,296-INA296A2IDRCT-ND,296-INA296A2IDRDKR-ND | INA296A2IDR |
| 296-INA296A3IDRTR-ND,296-INA296A3IDRCT-ND,296-INA296A3IDRDKR-ND | INA296A3IDR |
| 296-INA296A5IDGKRTR-ND,296-INA296A5IDGKRCT-ND,296-INA296A5IDGKRDKR-ND | INA296A5IDGKR |
| 296-INA296A1IDGKRTR-ND,296-INA296A1IDGKRCT-ND,296-INA296A1IDGKRDKR-ND | INA296A1IDGKR |
| 5503-TP5534-TR-ND,5503-TP5534-TRCT-ND,5503-TP5534-TRDKR-ND | TP5534-TR |
| 5503-TPA1861-SRTR-ND,5503-TPA1861-SRCT-ND,5503-TPA1861-SRDKR-ND | TPA1861-SR |
| 5503-TPA1861-TR-ND,5503-TPA1861-TRCT-ND,5503-TPA1861-TRDKR-ND | TPA1861-TR |
| 2129-NJU77903DL3H-TE2TR-ND,2129-NJU77903DL3H-TE2CT-ND,2129-NJU77903DL3H-TE2DKR-ND | NJU77903DL3H-TE2 |
| 497-TSV774IYQ5TTR-ND,497-TSV774IYQ5TCT-ND,497-TSV774IYQ5TDKR-ND | TSV774IYQ5T |
| 296-INA310A2QDGKRQ1TR-ND,296-INA310A2QDGKRQ1CT-ND,296-INA310A2QDGKRQ1DKR-ND | INA310A2QDGKRQ1 |
| 296-INA310A3QDGKRQ1TR-ND,296-INA310A3QDGKRQ1CT-ND,296-INA310A3QDGKRQ1DKR-ND | INA310A3QDGKRQ1 |
| 5503-TPA1882-SRTR-ND,5503-TPA1882-SRCT-ND,5503-TPA1882-SRDKR-ND | TPA1882-SR |
| 296-INA310A4QDGKRQ1TR-ND,296-INA310A4QDGKRQ1CT-ND,296-INA310A4QDGKRQ1DKR-ND | INA310A4QDGKRQ1 |
| 296-INA310A1QDGKRQ1TR-ND,296-INA310A1QDGKRQ1CT-ND,296-INA310A1QDGKRQ1DKR-ND | INA310A1QDGKRQ1 |
| 296-INA310A5QDGKRQ1TR-ND,296-INA310A5QDGKRQ1CT-ND,296-INA310A5QDGKRQ1DKR-ND | INA310A5QDGKRQ1 |
| 296-INA296A1QDDFRQ1TR-ND,296-INA296A1QDDFRQ1CT-ND,296-INA296A1QDDFRQ1DKR-ND | INA296A1QDDFRQ1 |
| 296-INA296A1QDGKRQ1TR-ND,296-INA296A1QDGKRQ1CT-ND,296-INA296A1QDGKRQ1DKR-ND | INA296A1QDGKRQ1 |
| 296-INA296A1QDRQ1TR-ND,296-INA296A1QDRQ1CT-ND,296-INA296A1QDRQ1DKR-ND | INA296A1QDRQ1 |
| 296-INA296A5QDRQ1TR-ND,296-INA296A5QDRQ1CT-ND,296-INA296A5QDRQ1DKR-ND | INA296A5QDRQ1 |
| 296-INA296A2QDRQ1TR-ND,296-INA296A2QDRQ1CT-ND,296-INA296A2QDRQ1DKR-ND | INA296A2QDRQ1 |
| 296-INA241A3QDGKRQ1TR-ND,296-INA241A3QDGKRQ1CT-ND,296-INA241A3QDGKRQ1DKR-ND | INA241A3QDGKRQ1 |
| 296-INA241A5QDGKRQ1TR-ND,296-INA241A5QDGKRQ1CT-ND,296-INA241A5QDGKRQ1DKR-ND | INA241A5QDGKRQ1 |
| 296-INA241A1QDGKRQ1TR-ND,296-INA241A1QDGKRQ1CT-ND,296-INA241A1QDGKRQ1DKR-ND | INA241A1QDGKRQ1 |
| 296-INA241A2QDGKRQ1TR-ND,296-INA241A2QDGKRQ1CT-ND,296-INA241A2QDGKRQ1DKR-ND | INA241A2QDGKRQ1 |
| 296-INA296A2QDGKRQ1TR-ND,296-INA296A2QDGKRQ1CT-ND,296-INA296A2QDGKRQ1DKR-ND | INA296A2QDGKRQ1 |
| 296-INA296A5QDGKRQ1TR-ND,296-INA296A5QDGKRQ1CT-ND,296-INA296A5QDGKRQ1DKR-ND | INA296A5QDGKRQ1 |
| 296-INA296A3QDRQ1TR-ND,296-INA296A3QDRQ1CT-ND,296-INA296A3QDRQ1DKR-ND | INA296A3QDRQ1 |
| 296-INA241A4QDGKRQ1TR-ND,296-INA241A4QDGKRQ1CT-ND,296-INA241A4QDGKRQ1DKR-ND | INA241A4QDGKRQ1 |
| 296-INA296A4QDGKRQ1TR-ND,296-INA296A4QDGKRQ1CT-ND,296-INA296A4QDGKRQ1DKR-ND | INA296A4QDGKRQ1 |
| 5503-TPA1882-VRTR-ND,5503-TPA1882-VRCT-ND,5503-TPA1882-VRDKR-ND | TPA1882-VR |
| 175-MAX49921FATA/VY+TTR-ND,175-MAX49921FATA/VY+TCT-ND,175-MAX49921FATA/VY+TDKR-ND | MAX49921FATA/VY+T |
| 5503-TPA8001-SOARTR-ND,5503-TPA8001-SOARCT-ND,5503-TPA8001-SOARDKR-ND | TPA8001-SOAR |
| 505-AD8410AWBRMZ-RLTR-ND,505-AD8410AWBRMZ-RLCT-ND,505-AD8410AWBRMZ-RLDKR-ND | AD8410AWBRMZ-RL |
| 505-AD8411AWBRZ-ND | AD8411AWBRZ |
| 296-INA254A3IPWARTR-ND,296-INA254A3IPWARCT-ND,296-INA254A3IPWARDKR-ND | INA254A3IPWAR |
| 296-INA254A2IPWARTR-ND,296-INA254A2IPWARCT-ND,296-INA254A2IPWARDKR-ND | INA254A2IPWAR |
| 296-INA254A1IPWARTR-ND,296-INA254A1IPWARCT-ND,296-INA254A1IPWARDKR-ND | INA254A1IPWAR |
| 5503-TP5554-TR-ND,5503-TP5554-TRCT-ND,5503-TP5554-TRDKR-ND | TP5554-TR |
| 505-ADA4510-2ARMZ-R7TR-ND,505-ADA4510-2ARMZ-R7CT-ND,505-ADA4510-2ARMZ-R7DKR-ND | ADA4510-2ARMZ-R7 |
| 5503-TPA1286U-SO1RTR-ND,5503-TPA1286U-SO1RCT-ND,5503-TPA1286U-SO1RDKR-ND | TPA1286U-SO1R |
| 5503-TPA1285T-VR-STR-ND,5503-TPA1285T-VR-SCT-ND,5503-TPA1285T-VR-SDKR-ND | TPA1285T-VR-S |
| 5503-TPA1286-SO1RTR-ND,5503-TPA1286-SO1RCT-ND,5503-TPA1286-SO1RDKR-ND | TPA1286-SO1R |
| 5503-TPA1286U-DF7RTR-ND,5503-TPA1286U-DF7RCT-ND,5503-TPA1286U-DF7RDKR-ND | TPA1286U-DF7R |
| 5503-TPA1286-VS1RTR-ND,5503-TPA1286-VS1RCT-ND,5503-TPA1286-VS1RDKR-ND | TPA1286-VS1R |
| 5503-TPA1286U-VS1RTR-ND,5503-TPA1286U-VS1RCT-ND,5503-TPA1286U-VS1RDKR-ND | TPA1286U-VS1R |
| 5503-TPA1295F-SO1R-STR-ND,5503-TPA1295F-SO1R-SCT-ND,5503-TPA1295F-SO1R-SDKR-ND | TPA1295F-SO1R-S |
| 296-OPA814DBVRTR-ND,296-OPA814DBVRCT-ND,296-OPA814DBVRDKR-ND | OPA814DBVR |
| 5503-TPA3530-SO1RTR-ND,5503-TPA3530-SO1RCT-ND,5503-TPA3530-SO1RDKR-ND | TPA3530-SO1R |
| 5536-LM358GN-ND | LM358GN |
| 5536-LM4558N-ND | LM4558N |
| 5399-LM321TR-ND,5399-LM321CT-ND,5399-LM321DKR-ND | LM321 |
| 4518-LMV358IPWRTR-ND,4518-LMV358IPWRCT-ND,4518-LMV358IPWRDKR-ND | LMV358IPWR |
| 2156-INA215CQDCKRQ1-296-ND | INA215CQDCKRQ1 |
| 497-10218-2-ND,497-10218-1-ND,497-10218-6-ND | LM2904YPT |
| 4518-LM124DRTR-ND,4518-LM124DRCT-ND,4518-LM124DRDKR-ND | LM124DR |
| 4518-LM324PWRTR-ND,4518-LM324PWRCT-ND,4518-LM324PWRDKR-ND | LM324PWR |
| 2156-TLC25L2ACDR-ND | TLC25L2ACDR |
| 2156-TLC25L2ACP-ND | TLC25L2ACP |
| 4518-OPA348AIDCKRTR-ND,4518-OPA348AIDCKRCT-ND,4518-OPA348AIDCKRDKR-ND | OPA348AIDCKR |
| 4518-LMV722IDRTR-ND,4518-LMV722IDRCT-ND,4518-LMV722IDRDKR-ND | LMV722IDR |
| 4518-LMV721IDBVRTR-ND,4518-LMV721IDBVRCT-ND,4518-LMV721IDBVRDKR-ND | LMV721IDBVR |
| 4518-LMV721IDCKRTR-ND,4518-LMV721IDCKRCT-ND,4518-LMV721IDCKRDKR-ND | LMV721IDCKR |
| 4518-OPA2347UATR-ND,4518-OPA2347UACT-ND,4518-OPA2347UADKR-ND | OPA2347UA |
| 4518-TL084CDRTR-ND,4518-TL084CDRCT-ND,4518-TL084CDRDKR-ND | TL084CDR |
| 296-51147-2-ND,296-51147-1-ND,296-51147-6-ND,2156-INA212CQDCKRQ1-ND | INA212CQDCKRQ1 |