This Product Selection Guide contains information to help select products in the Labels, Stickers, Decals - Preprinted category on DigiKey.com
Preprinted Labels, Stickers, and Decals are materials (Aluminum, Cardboard, Cloth, Fabric, Nylon, Paper, and many more) with a sticky backing and either words, symbols, or both preprinted on them. The filters are characterized by print type, language, application specifics, and arrangement. The arrangement being symbol and text, symbol only, or text only.
SelectionCharacteristics
Print Type: Indicates the method of printing the label is compatible with.
Language: Indicates what language(s) the labels are printed in.
Applications: Defines the use case for the product.
Application Specifics: Provides further details for the use case of the product.
Arrangement: Defines if the product uses symbols and/or text.
Legend (Text): Defines what is printed on the product.
Legend (Symbol Only): Defines what is printed on the product for symbols.
Color - Background: Indicates the background color used for the product.
Color - Legend: Indicates the color used for the print.
Length: Indicates the overall length of the product.
Width: Indicates the overall width of the product.
Diameter - Label: Indicates the diameter of the product.
Location: Indicates if the label is designed for indoor or outdoor environments.
Material - Body: Defines the material used for the body of the product.
Mounting Type: Indicates how the product is attached.
Outside Pipe Diameter (Max): indicates the maximum size of a label designed for application to pipes or plumbing, in terms of the pipe size for which the label is designed.
Outside Pipe Diameter (Min): indicates the minimum size of a label designed for application to pipes or plumbing, in terms of the pipe size for which the label is designed.
Shape: Indicates the overall shape of the product.
Features: These are different capabilities or properties of the device such as abrasion resistant or weather resistant.
Ratings: Minimum performance standards of the product, which are typically set by a third party.
ProductExamples
| MFR PART # | B6727 |
|---|---|
| DIGIKEY PART # | 2071-B6727-ND |
| MANUFACTURER | Botron Company Inc. |
| DESCRIPTION | B6727 BRIGHT YELLOW SELF ADHESIV |
| DATASHEET | Click Here |
| MFR PART # | 53079 |
|---|---|
| DIGIKEY PART # | 2267-53079-ND |
| MANUFACTURER | Brady Corporation |
| DESCRIPTION | B946 NFPA TARGET LABEL 3.5"X5" 5 |
| DATASHEET | Click Here |