Looking for this component - I belive it's a Voltage regulator?

Hi, Looking for this component, i believe it’s a 8 pin regulator, I have no schematic and the markings i can’t find anywhere. 04S 0483.

Thanks in advance
Lars

Hi lek

Unfortunately I am not able to locate this part based off the markings.

Hi @lek ,
LDOs rarely come in TSSOP8 package.
I wonder, could you provide more pictures, showing the components around and better view of the tracks (flux remover may improve the visibility).
Cheers, heke

Hi
Yes you are probably right, here is a wider picture. This circuit provides the voltage for the power transistor to the left, well that is what I think anyway.
I have a constant 4,6 volt from it but it should be varying is to the selected output power for the transmitter…. I I’m probably on deep water here :slight_smile:

Hi @lek ,
Thank you for the picture.
Hard to tell.
Guessing that the product is a some sort of UHF transceiver?
The chip may be doing active power amplifier biasing. Actually the chip on right interests (can see only a fraction of it at the edge of the picture, northeast from the screw). Can you provide another pic showing the stuff to the right?
Cheers, heke