Looking for equivalent or better IC chip with Marking code: V3605 and below that with GF88GG.
Researching around SMD marking code sites and a Google search leads me to believe it is the following: Magnachip MDV3605 Single P-Channel Trench MOSFET, -30A, -20A, 18 mOhms.
A little background on the application for the chip in question. The chip was burnt out on one GPU during testing and I have another GPU of the same kind with the same circuitry, which is how I got the marking codes for the IC. I am replacing the one 7002K, two K72 and few caps for good measure.
Mouser electronics leads me to the following IC chip if I search for the package type: PDFN33-8.
Taiwan Semiconductor TSM085P03CV RGG Mouser Taiwan Semiconductor V3605 equivalent
Attached are the best pictures taken of the known good circuitry and with the PDF I’ve found of the MDV3605.
MDV3605.PDF (1.1 MB)