I wouldn’t do that hack. It would be only tied to your user login.
I would do it like this: Yocto/Wireless – Gateworks
Regards,
I wouldn’t do that hack. It would be only tied to your user login.
I would do it like this: Yocto/Wireless – Gateworks
Regards,
@RobertCNelson https://community.nxp.com/thread/453629
mii info
I don’t know if this will help me to have ethernet eth0, but I did it!
result for ls -la /boot/ in my board with 2018-u-boot.imx. I can see extlinux. What about this?
root@imx7d-pico:~# ls -la /boot/
drwxr-xr-x 3 root root 1024 Oct 3 2019 .
drwxr-xr-x 20 root root 1024 Oct 3 2019 ..
lrwxrwxrwx 1 root root 85 Oct 3 2019 SPL -> SPL-imx7d-pico-v2018.11+gitAUTOINC+6e25ce6f3c-r0-pi-v2018.11+gitAUTOINC+6e25ce6f3c-r0
-rw-r--r-- 1 root root 60416 Oct 3 2019 SPL-imx7d-pico-v2018.11+gitAUTOINC+6e25ce6f3c-r0-pi-v2018.11+gitAUTOINC+6e25ce6f3c-r0
lrwxrwxrwx 1 root root 85 Oct 3 2019 SPL-pi -> SPL-imx7d-pico-v2018.11+gitAUTOINC+6e25ce6f3c-r0-pi-v2018.11+gitAUTOINC+6e25ce6f3c-r0
drwxr-xr-x 2 root root 1024 Oct 3 2019 extlinux
-rw-r--r-- 1 root root 32859 Oct 3 2019 imx7d-pico-pi.dtb
-rw-r--r-- 1 root root 483472 Oct 3 2019 u-boot-pi-v2018.11+gitAUTOINC+6e25ce6f3c-r0.img
lrwxrwxrwx 1 root root 47 Oct 3 2019 u-boot.img -> u-boot-pi-v2018.11+gitAUTOINC+6e25ce6f3c-r0.img
lrwxrwxrwx 1 root root 47 Oct 3 2019 u-boot.img-pi -> u-boot-pi-v2018.11+gitAUTOINC+6e25ce6f3c-r0.img
lrwxrwxrwx 1 root root 36 Oct 3 2019 zImage -> zImage-4.20.0-rc6-fslc+gbf414f71d713
-rw-r--r-- 1 root root 8527288 Oct 3 2019 zImage-4.20.0-rc6-fslc+gbf414f71d713
root@imx7d-pico:~#
Well, that will allow you to fill in a little more details:
/boot/extlinux/extlinux.conf
label Linux 4.20.0-rc6-fslc+gbf414f71d713
kernel /boot/zImage-4.20.0-rc6-fslc+gbf414f71d713
fdtdir /boot/
But you’ll still need to figure out:
append root=/dev/mmcblk2p1 ro rootfstype=ext4 rootwait quiet
it’s either:
append root=/dev/mmcblk2p2 ro rootfstype=ext4 rootwait quiet
or:
append root=/dev/mmcblk2p3 ro rootfstype=ext4 rootwait quiet
Regards,
@RobertCNelson
I’m trying to get your ubuntu version on another imx7d-pico. In it I will try wifi (I saw previous messages from you and someone else there) and I will need x11/chromium because I will use (5 INCH 800 x 480 PCAP MULTI TOUCH LCD PANEL INCLUDING TOUCH CABLE
TechNexion TDP-0500-T800480-PCAP) and I will have to have an application (probably in node or python) to exchange photos (jpg/png) in full screen with my fingers
I will keep you informed and thank you
I have a question: How kernel version I can put in ubuntu/pico-imx7d-pico to not have issues with wifi configuration in the future?
@RobertCNelson issue (file not found) with `
sudo tar xfvp .
/---armhf-/armhf-rootfs-*.tar -C /media/rootfs/`
command:
~/imx_usb_loader/u-boot/armv7-lpae-multiplatform/
In the directions, i’ve tried really hard to direct user to not do that ^…
user@localhost:~/u-boot$
Every git repo should be from ~/ and not cloned on top of each other…
Sorry i had to use Google Translate for:
Funcao open falhou: Arquivo ou directorio inexistente -> Open function failed: File or directory does not exist
Your version of Ubuntu auto-mounted the drive as “/media/neuberfran/rootfs/” while my command had you mount it as “/media/rootfs” So just change it.

sudo tar xfvp ./*-*-*-armhf-*/armhf-rootfs-*.tar -C /media/neuberfran/rootfs/
sync
sudo chown root:root /media/neuberfran/rootfs/
sudo chmod 755 /media/neuberfran/rootfs/
Regards,
@RobertCNelson I reset my board with mfgtools2, but not solved yet
(I do this command before everything sudo chmod 777 ubuntu.tar and sudo chmod 777 rootfs.tar)
I don’t know if this has to do with the current error:
The command:
sudo tar xfvp ./*-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
Assumes, you’ve picked either Ubuntu or Debian, not both. As the “---armhf-/” will encode to both in your case and fail:
The easy fix is just to rewrite it as:
For Debian:
sudo tar xfvp ./debian-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/
For Ubuntu:
sudo tar xfvp ./ubuntu-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/
Regards,
@RobertCNelson Issue after instalation
@RobertCNelson I need wifi
@RobertCNelson Pls, How can I get x11, apt-get (python or nodejs) and wifi in my ubuntu?
ubuntu@arm:~$ uname -a
Linux arm 5.4.58-armv7-lpae-x33 #1 SMP PREEMPT Mon Aug 24 12:36:57 -03 2020 armv7l armv7l armv7l GNU/Linux
I can’t change /etc/network/interfaces with sudo vi interfaces
(readonly file issue is problem
apt is already installed, just use it normally:
sudo apt update
sudo apt install pkg_name
WiFi was documented in the other PICO-PI-IMX7 thread in this forum, as only working in v5.1.x branch.
Why is it Read Only?
Please dump:
cat /proc/cmdline
cat /etc/fstab
Regards,
@RobertCNelson cat results. I will display photos jpg/png in (5 INCH 800 x 480 PCAP MULTI TOUCH LCD PANEL INCLUDING TOUCH CABLE TechNexion TDP-0500-T800480-PCAP).
Okay, no idea why it was RO, everything else looks correct.
This will install nodejs
sudo apt update
sudo apt install nodejs
Just photo’s? There is no reason for x11/wayland overhead then. ![]()
Just use “fbi” Linux frame buffer image viewer
Regards,
@RobertCNelson I currently don’t see anything that ubuntu (on imx7d-pico) is doing / happening on the screen. Using fbida will I be able to set the photos (in emmc root paste, for example) I want to see on the screen? I will can change to next photo using touch screen (the monitor is compatible)?
The lcd was enabled in v5.6.0-rc1: kernel/git/torvalds/linux.git - Linux kernel source tree
Can you access it thru nano?
sudo nano /etc/network/interfaces
Please run:
dmesg | grep mmc
So we can see why the mmc might in Read Only mode…
Edit: got video working in v5.6.x
Regards,
@RobertCNelson result command-
That’s odd, you have an orphan block on a new file system.
I’d run fsck on the drive locally, you need to go into u-boot and export the drive with
ums 0 mmc 0
Then run:
sudo fsck -a /dev/...
On it from your host…
Regards,
@RobertCNelson sudo fsck -a /dev/… Not work yet.
ubuntu@arm:/etc/network$ ls -ln
total 24
drwxr-xr-x 2 0 0 4096 May 10 20:21 if-down.d
drwxr-xr-x 2 0 0 4096 May 10 20:21 if-post-down.d
drwxr-xr-x 2 0 0 4096 May 10 20:21 if-pre-up.d
drwxr-xr-x 2 0 0 4096 May 10 20:21 if-up.d
**-rw-r--r-- 1 0 0 142 May 10 20:23 interfaces**
drwxr-xr-x 2 0 0 4096 May 3 2019 interfaces.d
ubuntu@arm:/etc/network$ pwd
/etc/network
sudo sfdisk ${DISK} <<-__EOF__ (in your tutorial) command only workd when I do with --force, type: sudo sfdisk --force ${DISK} <<-__EOF__
3.2 I can’t edit interfaces files using root too
3.3 -rw-r–r-- 1 0 0 142 May 10 20:23 interfaces is 644 number