Please help finding replacement for this micro switch

I’m looking for replacement for this micro switch. The best match I found is V15T16-CP200 but the inducive amperage is different, 16(4)A instead of 16(6)A.

![IMG_5307|375x500](upload://44BxNlkueta9RK7pc2eXUA50jBz.jpeg)

Add images

Hello huyen210 and welcome to the DigiKey TechForum.

I was able to find the options linked HERE that do have a higher amperage rating that may work for you.

Thank you so much, Nick. I’m worried that your suggestions are too high amperage. My switch has this notation 16(6)A 250VAC. Can I replace it with one with this notation 16(4)A 250VAC? Thanks

Matching mechanical fit is the first concern.

A single switch may have several different contact ratings depending on test conditions. Equal or greater contact current ratings for similar test conditions are recommended if no other information is available, but the thing that matters is that the actual use conditions are within the ratings of any replacement chosen.

Maybe. The number in parentheses is an inductive load rating. If the load is not inductive, or is an inductive load below 4A, it could be considered an acceptable replacement.