Questions About Air pump and Vacuum

Hello, I was recently working on a project that required small airpumps, one for pumping air at around 1.8-3 L/min, and one for vacuuming at approximately the same rate. Both pumps will be placed in a housing with approximate dimensions of 90 mm x 38 mm x 34 mm. I was wondering if there are pumps that can work as both inflation and deflation, and fit in the given dimensions, or if there are inflation and deflation pumps that perform accordingly. I was also wondering if the pump 4700, given by Adafruit Industries LLC, meets those requirements.

If such pumps exist, what are the SolidWorks model and dimensions for them?

Thank you!!!

@nikmehr33

The below are the options I had found for each type. I am not seeing that we list these based on air flow.

Pressure pumps.
Valves and Control | Pneumatics, Hydraulics | Electronic Components Distributor DigiKey

Vacuum pumps
Valves and Control | Pneumatics, Hydraulics | Electronic Components Distributor DigiKey