Release highlight of Libero® software suite for PolarFire® FPGAs from Microchip

Release highlight of Libero® software suite for PolarFire® FPGAs from Microchip

Libero v2025.2 Programming SARs and Features

MT25QL128ABA1ESE-0SIT as IC FLASH 128Mbit SPI 133MHz in 8SO from Micron Technology Inc.
W25Q64JVSSIQ as IC FLASH 64Mbit SPI/QUAD in 8SOIC from Winbond Electronics

Full SPI-Flash Memory Utilization for Data Storage Clients

Feature
If the SPI bitstream client is not present, you can create SPI data storage clients at any address, including those below 0x400

Description
In previous releases, the first 1024 Bytes of the target SPI-Flash memory device are reserved to store the addresses of programmed bitstreams whether they exist or not
In v2025.2 release, this restriction is removed for data storage clients only

Key Mode Column

Feature
Inserted a Key Mode column to the SPI Flash Clients Table showing which key (Default Key/UEK1/UEK2) was used for encrypting SPI bitstream file.

Purpose
In v2025.2 release, a “Key Mode” column is added to explicitly show what encryption key was used to generate a bitstream

SPI-Flash STAPL Support

Purpose
The purpose of this feature is to allow any STAPL player from different vendors to program SPI-Flash memory devices through PF and PFSoC devices including FPExpress

STAPL File Generation
This feature was added in v2025.1 release for Micron MT25QL01GBBB8ESF-0SIT TR and MT25QU01GBBB8E12-0AAT and MT25QU02GCBB8E12-0SIT and MT25QL02GCBB8E12-0AAT devices
In v2025.2, we have added Support for Winbond 25Q64JVSSIQ and Micron MT25QL128ABA1ESE-0SIT

FP6 SPI-Flash Support

In v2025.2 release, support for Winbond W25Q64JV SPI – Flash device was added

1 Like