Sensor T9602-5-A-1 communication reference number T4585647

A) how can we connect the sensor with our tracker ?

B) how will we get the output data ( Bluetooth , wire)? and do you have same sensors but Bluetooth

3) should I have a specific tracker to use this type of sensors?

Hi mlf.live2023,

Welcome to the Tech Forum.

Before we can answer your questions, to what “tracker” are you referring?

The T9602-5-A-1 gives a “pulse-density modulation” output which can be converted to an analog voltage with an external RC filter. After filtering, the voltage will vary, corresponding to the relative humidity and temperature (two separate signals) it measures. So you would need a device that can measure an analog voltage to determine the corresponding humidity and temperature.

It has a 1 meter cable and requires a 5V power supply for operation. The mating connector for it is the JST “EH” series - either the B4B-EH-A(LF)(SN) or the S4B-EH(LF)(SN). Unfortunately, at the time of this posting, both are on back-order. However, it does appear that the Adam Tech 25SH-C-04-TS is a probable alternative for the B4B-EH-A(LF)(SN).