T164110U controller

Are you still manufacturing this temp controller and if not is there a substitute with 2 input relays and a rtd 0-10 vdc signal?

Hi Mike,

Thank you for your first post on our TechForum. The following link is what we have to offer with the given specifications - https://www.digikey.com/short/zb0b29. These are the closest options we have to offer based on this information. Unfortunately, the product you are looking for is obsolete in our system - T1641100.

Thank you.

my input voltage is 115 vac and it allows temp to get to two different levels depending if i select “bake” or “spray” in the paint booth it operates. I can program the temp in either setting and if i select that setting (Bake or Spray) that is the temp level the inside of the paint booth gets.

Seems like Red Lion “RLC662-ND” might be my best option. Do you agree?

Mike B.

Hi Mike,

Yes, I do believe this would be the best option for an alternative solution. The input voltage that you are using fits in the parameters of the voltage on this product.

Thank you.