The core advantage of using a Digital Signal Processor (DSP) (e.g., Microchip dsPIC33FJ32MC204) to control a three-phase permanent magnet synchronous motor (PMSM) lies in the deep integration of hardware and algorithms, which can accurately meet the PMSM’s requirements for real-time performance, precision, and reliability.
System Block Diagram of a Three-Phase PMSM Controlled by a Signal Processor
(Image source: Microchip)
The specific manifestations are as follows:
1. Hardware Peripherals Customized for Motor Control
The dsPIC33 series Digital Signal Controllers (DSCs) integrate the core peripherals necessary for PMSM control, enabling the construction of a complete control system without the need for a large number of external circuits:
- Multi-Channel PWM Module: As shown in the diagram, the dsPIC33FJ32MC204 provides 6 PWM channels (PWM1H/L to PWM3H/L), which can directly drive the 6 power transistors of a three-phase inverter to generate precise voltage vectors (e.g., Space Vector PWM, SVPWM).
- High-Speed ADC and Current Detection: Current feedback (Ia, Ib) is connected via the AN0 and AN1 interfaces. Combined with a 12-bit ADC (with a sampling rate of up to 1 Msps), real-time current sampling is achieved, supporting low-cost detection solutions such as “three-phase current reconstruction using a single shunt resistor”.
- Fault Protection and Interface Expandability: The RB8 pin can be connected to an “Over Current” signal to implement hardware-level protection; interfaces such as AN8 and RA8 can be expanded for user interaction (e.g., potentiometer-based speed control, start/stop buttons).
The figure below shows the core power stage circuit of the dsPIC33FJ32MC204 Digital Signal Controller driving a three-phase permanent magnet synchronous motor (PMSM), adopting a minimalist topology with three-phase current detection using a single shunt resistor.
Three-Phase Inverter Topology (3-PHASE TOPOLOGY)
(Image source: Microchip)
Power Stage: Three-Phase Full-Bridge Inverter
-
It consists of 6 power switches (3 in the upper bridge arm and 3 in the lower bridge arm) forming a classic three-phase full bridge. Its output terminal is directly connected to the three-phase stator windings (U, V, W) of the PMSM.
-
Each power switch is driven by the PWM module of the dsPIC33 (6 PWM signals in total: PWM1H/L to PWM3H/L as shown in the diagram), which can generate Space Vector PWM (SVPWM) or square-wave control signals to adjust the motor voltage/current.
Current Detection: Single Shunt Resistor Solution
-
A sampling resistor (the grounded resistor in the diagram) is connected in series at the common terminal of the inverter’s lower bridge arm. Using Kirchhoff’s Current Law (Ia + Ib + Ic = 0), the three-phase currents can be reconstructed by detecting the voltage across this resistor.
-
Working Principle: During the PWM cycle, through time-division sampling (combined with the switching state of the power transistors), any two phases among Ia, Ib, and Ic can be calculated from the voltage of the single sampling resistor. The third phase is derived from the relationship that the sum of the three currents is zero.
Integration of Control and Protection
-
The ADC module of the dsPIC33 (e.g., channels AN0 and AN1) collects the voltage signal of the sampling resistor, converts it into current feedback, and uses it for closed-loop control (e.g., Field-Oriented Control, FOC).
-
If hardware protection (e.g., overcurrent protection) is required, a fault signal can be connected via the digital I/O of the dsPIC33 (e.g., RB8) to achieve rapid shutdown.
2. Real-Time Computing Capability Supports Complex Control Algorithms
PMSMs rely on vector algorithms such as Field-Oriented Control (FOC) to achieve stable torque output, and the DSP architecture of the dsPIC can efficiently execute such high-complexity calculations:
- Single-Cycle DSP Instructions: Supports multiply-accumulate (MAC) and floating-point operations. It can complete core operations in FOC (such as Clarke transformation, Park transformation, and PI regulation) within a single cycle, ensuring the real-time performance of the algorithm (e.g., a control frequency of over 10 kHz).
- Sensorless Algorithm Compatibility: If an encoder needs to be omitted, the dsPIC can estimate the rotor position through the high-frequency injection method or the back-EMF method, further reducing overall system cost.
Related Products
Related Application Notes
More Content Related to FOC
- Why Use a DSP to Control a Three-Phase Permanent Magnet Synchronous Motor (PMSM)?
- 3 Motor Control Techs Comparison: FOC, V/f Control, Trapezoidal Six-Step Control (BLDC)
- Why Use the Field-Oriented Control (FOC) Algorithm?
- What is the Clarke Transformation in the Field-Oriented Control (FOC) Algorithm?
- What is the Park Transformation in the Field-Oriented Control (FOC) Algorithm?
- Why Can PLL (Phase-Locked Loop) Ensure Anti-Interference and Accuracy in Multi-Level Speed Sampling?